Use the drop down button to select Burst or External. An external trigger source at the input of the Test Set's Trigger In connector is also required if you want to use the External setting.
Default: Burst.
Save Settings: The value is saved as part of the configuration (.gma) file.
You cannot configure this setting unless the Bluetooth demodulator is enabled. |