The IF Bandwidth specifies the Test Set receiver IF bandwidth to be used for the measurement.
When the wider IF filter settings are used the test results include the effects of spurious out-of-channel or inter-modulation products. This can be useful when evaluating the performance of devices during the development phase or test system development.
Range: 1.3 MHz, 3.0 MHz, and 5.0 MHz.
Default: 3.0 MHz.
Save Settings: The value is saved as part of the configuration (.gma) file.