Last Updated: June 19, 2009
These commands provide test set specific settings for the Center Frequency Leakage (CFL) measurement.
This measurement is only applicable to signals modulated using orthogonal frequency-division multiplexing (OFDM). The modulation format is set using [SENSe:]RADIo:STANdard[:SELect]:WLAN[?].
Sets/queries whether or not averaging is performed on the Center Frequency Leakage measurement.
The number of averages is set using [SENSe:]CFLeakage:AVERage:COUNt[?].
Setting Range: 0 | OFF | 1 | ON
Query Range: 0 | 1
*RST Setting: 0 | OFF
Test Set Requirements: N8300A Wireless Networking Test Set Version A.02 and above
Example:
CFLeakage:AVERage ON
Turns averaging on for the Center Frequency Leakage measurement.
Sets/queries the number of averages to be made for the Center Frequency Leakage measurement.
Averaging can be switched on or off using [SENSe:]CFLeakage:AVERage[:STATe][?].
Setting Range: 1 to 10,000
Query Range: 1 to 10,000
Resolution: 1
*RST Setting: 10
Test Set Requirements: N8300A Wireless Networking Test Set Version A.02 and above
Example:
CFLeakage:AVERage:COUNt 5
Sets the average count to 5 for the Center Frequency Leakage measurement.
Sets/queries the type of trigger source for the Center Frequency Leakage measurement.
Refer to TRIGger for more information on configuring the trigger.
Setting Range: EXTernal | IMMediate | RFBurst
Query Range: EXT | IMM | RFB
*RST Setting: IMMediate
Test Set Requirements: N8300A Wireless Networking Test Set Version A.02 and above
Example:
CFLeakage:TRIGger:SOURce RFBurst
Sets the RFBurst triggering source for the Center Frequency Leakage measurement.