Last updated: December 2, 2008
The test set provides the following time and date settings:
This field provides entry of the local time in hours and minutes.
The
Universal Coordinated Time
field will track changes made to the
Time
field.
Also known as Zulu, Greenwich Mean Time, or UCT, this field provides entry of universal time in hours and minutes.
The
Time
field will track changes made to the
Universal Coordinated Time (UTC)
field.
The
Time Zone
field provides entry of a time offset to the universal coordinated time (UTC). Based on each new time zone setting and the current UTC, a new local time value is calculated and automatically entered into the Time field.
These features are accessed by pressing the
SYSTEM CONFIG
hardkey followed by the
Instrument Setup
(
F1
) softkey.