Last updated: December 3, 2008
This section is only applicable to the lab applications.
The test set provide Network Identity and Time Zone (NITZ) information in the MM and GMM Information messages such that the mobile can store and use the information. The NITZ information including universal time (UT), daylight saving time (DST), and local time zone (LTZ).
See 3GPP TS 24.008 V7.2.0 for more information about MM and GMM Information messages.
The test set sends the NITZ information in each of the following conditions:
You can configure the NITZ parameters in the test set to control in which conditions the NITZ information is sent. The following table lists all the NITZ parameters that are configurable in the test set.
NITZ Universal Time-Date | |
NITZ Universal Time-Time | |
NITZ Local Time Zone | |
NITZ Daylight Saving Time Coupled | |
NITZ Daylight Saving Time Value | |
NITZ Daylight Saving Time State | |
NITZ Send on GPRS Registration |
CALL[:CELL]:NITZone:SEND:GMM:REGistration[:STATe][:SELected] |
NITZ Send on GPRS Call Origination |
CALL[:CELL]:NITZone:SEND:DATA:ORIGination[:STATe][:SELected] |
NITZ Send on GSM Registration | |
NITZ Send on GSM Call Origination |
CALL[:CELL]:NITZone:SEND:VOICe:ORIGination[:STATe][:SELected] |
NITZ Transportation in DTM | |
NITZ Send Immediate | |
Set NITZ Universal Time/Date to UniversalCoordinated Time/Date |
The following procedure details how to access and use the NITZ feature.
The NITZ functionality is only available in the
Active Cell
operating mode.
NOTE |
ON
.