Last updated: December 3, 2008
This command is not applicable to the GSM Test Application. | ||
This command is not applicable to the GPRS Test Application. | ||
This command is not applicable to the EGPRS Test Application. | ||
GSM/GPRS LA |
This command sets/queries up to 16 channels in the Cell Allocated (CA) Table. The Operating Mode must be in Cell Off to configure the CA Table. The command to set the test set's Operating Mode is CALL:OPERating:MODE . See Frequency Hopping for more information. | |
Setting |
Range: 0-124, 128-251, 259-293, 306-340, 350-425, 438-885, 955-1023 |
|
Query |
Range: 0-124, 128-251, 259-293, 306-340, 350-425, 438-885, 955-1023 |
|
*RST setting |
The default CA Table contains the following ARFCNs: 1, 124, 128, 251, 259, 293, 306, 340, 438, 511, 520, 661, 810, 885, 955, 975. The following list shows which bands in the default CA Table are represented for each channel.
|
|
Requirements | GSM/GPRS/ EGPRS LA | |
OUTPUT 714;"CALL:OPERating:MODE OFF" ! Sets the test set's operating mode to Cell Off. OUTPUT 714;"CALL:CA:TABLe 1,124,128,251,259,293,306,340,350,425,438,511,520,661,810,885,955" ! Sets the CA Table to the specified values. |