Last updated: January 18, 2010
This command sets/queries the type of connection. This is always set to AUTO for the GSM test application. |
||
This command sets/queries the type of connection that is used when you use the command CALL:FUNCtion:DATA:START to start a data connection. If you set this parameter to ETSI Type A, no packet data traffic channel (PDTCH) bursts will be transmitted on the downlink. Setting this parameter to ETSI Type B (unacknowledged) ensures that one or more downlink (PDTCH) bursts are present, which can be used to loopback data through the uplink. The number of downlink bursts is determined by the setting of the command CALL:(PDTCH|PDTChannel):MSLot:CONFig . The ETSI Type B Acknowledged connection type (ACKB) is almost identical to the ETSI Type B (Unacknowledged) connection type, except that it features an acknowledged downlink. The acknowledged downlink ensures maximum compatibility with different mobile station types. ETSI Type B (Unacknowledged) or ETSI Type B (Acknowledged) is required if you want to perform BER measurements in active cell mode. Setting this parameter to BLER ensures that an Agilent proprietary data connection type is used which allows the test set to obtain BLock Error Rate (BLER) measurement reports from the mobile station (see Block Error Rate (BLER) Reports Description ). In addition, the BLER data connection type allows you to perform other GPRS measurements at the same time (except BER and ORFS due to Modulation). It is recommended you always end the data connection (using CALL:FUNCtion:DATA:STOP ) before changing the data connection type. If you change this parameter while the data connection status is transferring, the data connection will be dropped (changing the data connection status to attached), and an error message will be generated. |
||
In addition to the functions of the GPRS TA (above), the GSM/GPRS lab application has the following effects: |
||
This command sets/queries the type of connection that is used when you use the command CALL:FUNCtion:DATA:START to start a data connection. If you set this parameter to ETSI Type A, no packet data traffic channel (PDTCH) bursts will be transmitted on the downlink. Setting this parameter to ETSI Type B (unacknowledged) ensures that one or more downlink (PDTCH) bursts are present, which can be used to loopback data through the uplink. The number of downlink bursts is determined by the setting of the command CALL:(PDTCH|PDTChannel):MSLot:CONFig . The ETSI Type B Acknowledged connection type (ACKB) is almost identical to the ETSI Type B (Unacknowledged) connection type, except that it features an acknowledged downlink. The acknowledged downlink ensures maximum compatibility with different mobile station types.ETSI Type B (unacknowledged) or ETSI Type B Acknowledged is required if you want to perform BER measurements in active cell mode. Each of the ETSI test modes are extended with EGPRS header information. Setting this parameter to BLER ensures that an Agilent proprietary data connection type is used which allows the test set to obtain BLock Error Rate (BLER) measurement reports from the mobile station (see Block Error Rate (BLER) Reports Description ). In addition, the BLER data connection type allows you to perform other GMSK modulated EGPRS measurements at the same time (except Bit Error Rate and ORFS due to Modulation). Setting this parameter to SRBL ensures that the Switched Radio Block (SRB) Loopback mode is used for the data connection. This connection type is only available in Active Cell operating mode. It is recommended you always end the data connection (using CALL:FUNCtion:DATA:STOP ) before changing the data connection type. If you change this parameter while the data connection status is transferring, the data connection will be dropped (changing the data connection status to attached), and an error message will be generated. When the data connection type is AUTO (formerly known as IP Data), BER measurements will not be accurate due to synchronization problems. However, BLER measurements are not affected. |
||
GSM TA | ||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:FUNCTION:CONNECTION:TYPE B" ! Sets the connection type to ETSI Type B |
This command sets/queries whether or not the Logical Link Control (LLC) Frame Check Sequence (FCS) is corrupted in order to establish a BLER mode data connection. Setting this parameter to VALid ensures that the cyclic redundancy check code within the FCS is valid. Setting this parameter to CORRupt causes the test set to transmit an invalid FCS to the mobile. This setting may enable some mobiles to establish a BLER mode data connection which would not otherwise be possible with a valid FCS. This parameter is only applicable when the data connection type is set to BLER using CALL:FUNCtion:CONNection:TYPE BLER. If you change this parameter while the data connection type is any type other than BLER, the setting has no effect until a new BLER mode data connection is established. This command along with CALL:FUNCtion:DATA:BLER:POLLing:INTerval provides you with additional control over BLER data connection type settings. This may enable the test set to establish a BLER mode data connection with mobiles which cannot connect under normal conditions. |
||
VALid | ||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:FUNCTION:DATA:BLER:LLC:FCSEQUENCE CORRUPT" ! Sets the test set to transmit an invalid FCS to the mobile. |
This command is not applicable to GSM. | ||
Use the command CALL:FUNCtion:DATA:BLOCk:POLLing:INTerval[:SELected] instead. This command sets/queries the Block Polling Parameters for the currently selected connection type. This command is only applicable when the currently selected connection type is Auto, BLER or ETSI Type B (Ack). The command to configure the connection type is CALL:FUNCtion:CONNection:TYPE . If you change this parameter while the connection type is not applicable to the block poll interval, the setting request is ignored, and the query will return zero. |
||
Setting |
Range: 1 to 256, or 0 if the connection type is not applicable to the block polling interval. Resolution: 1 |
|
Query |
Range: 1 to 256 Resolution: 1 |
|
*RST setting | 1 | |
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:FUNCTION:DATA:BLER:POLLING:INTERVAL 8" ! Sets block polling interval to 8. |
This command is not applicable to GSM. | ||
This command sets/queries the Block Polling Parameters for the currently selected connection type. This command is only applicable when the currently selected connection type is Auto, BLER or ETSI Type B (Ack). The command to configure the connection type is CALL:FUNCtion:CONNection:TYPE . If you change this parameter while the connection type is not applicable to the block poll interval, the setting request is ignored, and the query will return zero. |
||
Setting |
Range: 1 to 256 Resolution: 1 |
|
Query |
Range: 1 to 256, or 0 if the connection type is not applicable to the block polling interval. Resolution: 1 |
|
*RST setting |
Depends on the test set application and licenses: Test application with GPRS and/or EGPRS license: 1 Test application with GSM license in addition to a GPRS and/or EGPRS license: 0 (Not Applicable to when the Connection Type is Auto in the Test application) |
|
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:FUNCtion:DATA:BLOCk:POLLing:INTerval 8" ! The block polling interval is 8 for the test set's currently selected connection. |
This command is not applicable to GSM. | ||
This command sets/queries the Block Polling Interval for when the connection type is set to ETSI Type B (Ack). The command to configure the connection type is CALL:FUNCtion:CONNection:TYPE . For more information see Block Polling Parameters . |
||
Setting |
Range: 1 to 256 Resolution: 1 |
|
Query |
Range: 1 to 256 Resolution: 1 |
|
*RST setting | 32 | |
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:FUNCtion:DATA:BLOCk:POLLing:INTerval:ACKB 64" ! The block polling interval is 64 when the test set's connection type is ETSI Type B. |
This command is not applicable to the GSM test application. | ||
This command sets/queries the Block Polling Interval for when the connection type is set to Auto. The command to configure the connection type is CALL:FUNCtion:CONNection:TYPE . For more information see Block Polling Parameters . |
||
Setting |
Range: 1 to 256 Resolution: 1 |
|
Query |
Range: 1 to 256 Resolution: 1 |
|
*RST setting | 32 | |
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:FUNCtion:DATA:BLOCk:POLLing:INTerval:AUTO 64" ! The block polling interval is 64 when the test set's connection type is Auto. |
This command is not applicable to GSM. | ||
This command sets/queries the Block Polling Interval for when the connection type is set to BLER. The command to configure the connection type is CALL:FUNCtion:CONNection:TYPE . For more information see Block Polling Parameters . |
||
Setting |
Range: 1 to 256 Resolution: 1 |
|
Query |
Range: 1 to 256 Resolution: 1 |
|
*RST setting | 1 | |
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:FUNCtion:DATA:BLOCk:POLLing:INTerval:BLER 4" ! The block polling interval is 4 when the test set's connection type is BLER. |
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:FUNCTION:DATA:DETACH" ! Detaches the mobile from the test set. |
This command sets/queries the number of Protocol Data Units (PDUs) sent from the test set to the mobile station. When the PDU count is set to zero, the test set commands the mobile station to transmit continually as long as there is a connection between the mobile station. When the PDU count is set to 4095 the test set commands the mobile station to send 4095 PDUs on the uplink TBF before the mobile station terminates the connection between the mobile station and the test set. See Protocol Data Unit Count for more information on which connection types are valid when setting the PDU count. This setting only affects the ETSI Type A operating mode, see CALL:OPERating:MODE . |
||
0|4095 | ||
4095 | ||
Requirements | ||
GSM/GPRS/ |
Revision: D.01 an d above | |
OUTPUT 714;"CALL:FUNCtion:DATA:ETSIA:PDU:COUNt 0" ! The test set commands the mobile station to continuously transmit PDUs as long as ! there is a connection between the test set and the mobile station. |
This command sets/queries the type of frame numbering scheme to be used when establishing a data connection. Changing the frame numbering scheme may enable the test set to establish a data connection with mobiles which cannot connect under normal conditions.
It is recommended that you should not change this parameter while the data connection status is Starting, as there is no guarantee whether the new setting or the previous setting will be used for the current data connection. If the type of data connection you want to establish is BLER, the commands CALL:FUNCtion:DATA:BLER:LLC:FCSequence and CALL:FUNCtion:DATA:BLER:POLLing:INTerval may also be helpful in enabling the test set to establish a data connection with mobiles which cannot establish a BLER data connection under normal conditions. |
||
REL | ||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:FUNCTION:DATA:FRAME:START ABSOLUTE" ! Sets the frame number type to Absolute. |
This command sets/queries the type of downlink payload pattern to be used when the test set's operating mode is set to a valid connection type. See CALL:FUNCtion:CONNection:TYPE for the GPIB command to set the connection type. Changes to the payload pattern setting become effective immediately. See Payload Pattern (OTHER) for more information on the payload pattern parameters available and the valid connection types for this command. |
||
EGPRS LA | ||
Range: ZERos | ONES | ABITs | APAirs | AQUads | PRBS15 | PRBS9 | FIXED2B |CUSTom |
||
Range: ZER | ONES | ABIT | APA | AQU | PRBS15 | PRBS9 | FIXED2B |CUST |
||
PRBS15 | ||
Requirements |
GSM/GPRS/ EGPRS TA |
Revision: A.01 and above |
GSM/GPRS/ EGPRS LA |
Revision: C.01 and above |
|
OUTPUT 714;"CALL:FUNCTION:DATA:PAYLoad:PATTern:ETSIB AQUADS" ! Sets the payload pattern to be Alternate Quads. |
GSM/GPRS LA |
||
EGPRS TA |
This command sets/queries the type of downlink payload pattern to be used when the test set's operating mode is set to a valid connection types. See Multi Source Payload Pattern (OTHER) for more information. |
|
EGPRS LA | ||
Range: ZERos | ONES | ABITs | APAirs | AQUads | PRBS9 | PRBS15 | FIXED2B |CUSTom |
||
Range: ZERO | ONES | ABIT | APA | AQU | PRBS9 | PRBS15 | FIXED2B |CUST |
||
PRBS15 | ||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:FUNCtion:DATA:PAYLoad:PATTern:MSOurce:BURSt2 AQUads" ! Sets the payload pattern to be Alternate Quads. |
This command sets/queries the type of downlink payload pattern to be sent to the mobile when the connection type is set to BLER (see CALL:FUNCtion:CONNection:TYPE ) in Active Cell operating mode, and the LLC Frame Check Sequence parameter is set to CORRupt (see CALL:FUNCtion:DATA:BLER:LLC:FCSequence ). Changes to the payload pattern setting become effective immediately. See Payload Pattern (BLER) for more information on the payload pattern parameters available for this command. If this command is set to any value other than GMMinfo, and you want to change the setting of the LLC Frame Check Sequence parameter from CORRupt to VALid, it is strongly recommended that you end the data connection before making this change. After the LLC Frame Check Sequence parameter has been set to VALid, the data connection can be restarted using CALL:FUNCtion:DATA:START . |
||
Range: GMMinfo | ZEROs | ONES | ABITs | APAirs | AQUads | PRBS9 | PRBS15 | FIXED2B |CUSTom |
||
Range: GMM | ZERO | ONES | ABIT | APA | AQU | PRBS9 | PRBS15 | FIXED2B | CUST |
||
GMM | ||
Requirements |
GSM/GPRS/ EGPRS TA |
Revision: A.01 and above |
GSM/GPRS/ EGPRS LA |
Revision: C.01 and above |
|
OUTPUT 714;"CALL:FUNCTION:DATA:PAYLoad:PATTern:BLER ONES" ! Sets the payload pattern to be All Ones. |
THIS COMMAND IS OBSOLETE. Please use the CALL:FUNCtion:DATA:PAYLoad:PATTern[:OTHer] command to perform the function of this command. This command sets/queries the type of downlink payload pattern to be used when the test set's operating mode is set to either BCH+PDTCH Test Mode, or Active CALL operating mode with the data connection type set to ETSI Type B (see CALL:FUNCtion:CONNection:TYPE ). Changes to the payload pattern setting become effective immediately. See Payload Pattern (BLER) for more information on the payload pattern parameters available for this command. |
||
EGPRS LA | ||
Range: ZERos | ONES | ABITs | APAirs | AQUads | PRBS9 | PRBS15 | FIXED2B | CUSTom |
||
Range: ZER | ONES | ABIT | APA | AQU | PRBS9 | PRBS15 | FIXED2B | CUST |
||
PRBS15 | ||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:FUNCTION:DATA:PAYLoad:PATTern:ETSIB AQUADS" ! Sets the payload pattern to be Alternate Quads. |
This command is not applicable to GPRS Test Application. | ||
This command is not applicable to EGPRS Test Application. | ||
Sets/Queries the "Packet Uplink Ack/Nack Interval (EGPRS)". See Packet Uplink Ack/Nack Interval . | ||
EGPRS LA | ||
Resolution: 1 |
||
9 | ||
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:FUNCTION:DATA:PUPLink:ACKNack:INTerval:EGPRs 8" ! Set the Packet Uplink !Ack/Nack Interval(EGPRS) to 8. |
This command is not applicable to GPRS Test Application. | ||
This command is not applicable to EGPRS Test Application. | ||
Sets/Queries the "Packet Uplink Ack/Nack Interval (GPRS)". See Packet Uplink Ack/Nack Interval . | ||
EGPRS LA | ||
9 | ||
Requirements | GSM/GPRS/ EGPRS LA | |
OUTPUT 714;"CALL:FUNCTION:DATA:PUPLink:ACKNack:INTerval:GPRS 8" ! Set the Packet Uplink !Ack/Nack Interval(GPRS) to 8. |
This command attempts to start the data connection. See Data Connection Processing Event Synchronization . Additional commands can be appended to aid in controller/mobile station synchronization. See Call Processing Subsystem Overlapped Command Synchronization Commands for examples. If you have trouble getting the data connection to start, see GPRS Data Connection Troubleshooting . |
||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:FUNCTION:DATA:START" ! Starts data connection. |
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:FUNCTION:DATA:STOP" ! Ends data connection. |
This command sets/queries the availability of BTE measurement in test mode. This setting controls the test set to determine whether real-time demodulation is needed and decide whether Demod Type is used. When the setting is ON, the Demod Type is changed to Normal. In order to keep backward-compatibility, when the setting is set to OFF in operating modes other than EGPRS test modes, the Demod Type is always Normal. But the BTE report is still not available to reduce the message exchange between processors of the test set. When the setting becomes OFF in EGPRS test modes and BER, BLER or SRB BER measurement is not running, the EGPRS Demod Type Setting reverts to Reduced and EGPRS demodulation is applied only occasionally. See Test Mode Burst Timing Error Measurement for more information. |
||
OFF | ||
Requirements |
GSM/GPRS/ EGPRS TA |
|
OUTPUT 714;"CALL:FUNCtion:TBTerror ON" ! Sets the BTE measurement in test mode. |