Last updated: December 3, 2008
This command sets/queries the Cell Power for the active (that is the selected) format and turns the state to ON. This is a complex command combining the cell power state and amplitude commands. The cell power state is automatically set to ON when this command is used. The Cell Power is affected when there is an amplitude offset (see Amplitude Offset ).
The power level of the TCH is also affected by the setting of this command. |
||
This command sets/queries the Cell Power for the active (that is the selected) format and turns the state to ON. This is a complex command combining the cell power state and amplitude commands. The cell power state is automatically set to ON when this command is used. The power level of the PDTCH is also affected by the setting of this command. However, the PDTCH level is also affected by other settings (see Configuring the Packet Data Traffic Channel (PDTCH) ). The Cell Power is affected when there is an amplitude offset (see Amplitude Offset ). |
||
This command sets/queries the Cell Power for the active (that is the selected) format and turns the state to ON. This is a complex command combining the cell power state and amplitude commands. The cell power state is automatically set to ON when this command is used. The Cell Power is affected when there is an amplitude offset (see Amplitude Offset ).
The power level of the TCH is also affected by the setting of this command. The power level of the PDTCH is also affected by the setting of this command. However, the PDTCH level is also affected by other settings (see Configuring the Packet Data Traffic Channel (PDTCH) ). |
||
The *RST value of this command depends on the format that is currently active. For example, if the GSM format is currently active, the *RST value for this command is the same value as the equivalent command containing the :GSM format identifier. |
||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:CELL:POWer:SAMPlitude:SELected -50dBm" ! Sets the value to -50dBm and the state to ON. |
This command sets/queries the Cell Power for a continuous wave format whether or not that format is active. This is a complex command combining the cell power state and amplitude commands. The cell power state is automatically set to ON when this command is used. The Cell Power is affected when there is an amplitude offset (see Amplitude Offset ). |
||
GSM/GPRS LA |
||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:CELL:POWer:SAMPlitude:CW -50dBm" ! Sets the value to -50dBm and the state to ON. |
This command sets/queries the Cell Power for the GSM format whether or not that format is active. This is a complex command combining the cell power state and amplitude commands. The cell power state is automatically set to ON when this command is used. The Cell Power is affected when there is an amplitude offset (see Amplitude Offset ).
The power level of the TCH is also affected by the setting of this command. |
||
GPRS TA |
||
EGPRS LA |
||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:CELL:POWer:SAMPlitude:GSM -50dBm" ! Sets the value to -50dBm and the state to ON. |
This command sets/queries the Cell Power for the active (that is the selected) format. The Cell Power is affected when there is an amplitude offset (see Amplitude Offset ).
The power level of the TCH is also affected by the setting of this command. |
||
This command sets/queries the Cell Power (BCH) for the active (that is the selected) format. The power level of the PDTCH is also affected by the setting of this command. However, the PDTCH level is also affected by other settings (see Configuring the Packet Data Traffic Channel (PDTCH) ). The Cell Power is affected when there is an amplitude offset (see Amplitude Offset ). |
||
GSM/GPRS LA |
This command sets/queries the Cell Power for the active (that is the selected) format and turns the state to ON. This is a complex command combining the cell power state and amplitude commands. The cell power state is automatically set to ON when this command is used. The Cell Power is affected when there is an amplitude offset (see Amplitude Offset ).
The power level of the TCH is also affected by the setting of this command. The power level of the PDTCH is also affected by the setting of this command. However, the PDTCH level is also affected by other settings (see Configuring the Packet Data Traffic Channel (PDTCH) ). |
|
EGPRS LA |
||
The *RST value of this command depends on the format that is currently active. For example, if the GSM format is currently active, the *RST value for this command is the same value as the equivalent command containing the :GSM format identifier. |
||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:CELL:POWer:AMPLitude:SELected -50dBm" ! Set the cell power from test set to -50dBm. |
This command sets/queries the Cell Power for a continuous wave format whether or not that format is active. The Cell Power is affected when there is an amplitude offset (see Amplitude Offset ). |
||
GSM/GPRS LA |
||
EGPRS LA |
||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:CELL:POWer:AMPLitude:CW -50dBm" ! Set the cell power from test set to -50dBm. |
This command sets/queries the Cell Power for the GSM format whether or not that format is active. The Cell Power is affected when there is an amplitude offset (see Amplitude Offset ).
The power level of the TCH is also affected by the setting of this command. |
||
EGPRS TA |
||
GPRS TA |
||
EGPRS LA |
||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:CELL:POWer:AMPLitude:GSM -50dBm" ! Set the cell power from test set to -50dBm. |