Last updated: January 16, 2009
This command is not applicable to the GSM Test Application. | ||
GPRS TA |
This command is not applicable to the GPRS Test Application. |
|
EGPRS TA |
This command is not applicable to the EGPRS Test Application. |
|
GSM/GPRS LA |
Sets the TBF Release Timer value. See Configurable Timers . |
|
EGPRS LA | ||
Setting |
Range: MS500 | MS1000 | MS1500 | MS0 | MS80 | MS120 | MS160 | MS200 |
|
Range: MS500 | MS1000 | MS1500 | MS0 | MS80 | MS120 | MS160 | MS200 |
||
MS500 | ||
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:CELL:TBFLOW:T3192 MS1000" ! Set the expire time of T3192 to 1000ms. |
This command is not applicable to the GSM Test Application. | ||
This command is not applicable to the GPRS Test Application. | ||
This command is not applicable to the EGPRS Test Application. | ||
Sets/Queries the Extended Uplink TBF State. The command to set the duration of the extended uplink TBF is CALL:(PDTCH|PDTChannel):TBFLow:UPLink:EXTended:DURation . |
||
Setting | Range: 0 | OFF | 1 | ON | |
Query | Range: 0 | 1 | |
*RST setting | 0 | |
Requirements | GSM/GPRS/ EGPRS LA | |
OUTPUT 714;"CALL:TBFLow:UPLink:EXTended ON" ! Enables the extended uplink TBF. |
This command is not applicable to the GSM Test Application. | ||
This command is not applicable to the GPRS Test Application. | ||
This command is not applicable to the EGPRS Test Application. | ||
Sets/Queries the Extended Uplink TBF No Data State which indicates whether the mobile station during extended uplink TBF mode may refrain from sending PACKET UPLINK DUMMY CONTROL BLOCK messages when there is no other RLC/MAC block ready to send. See Extended Uplink TBF for more information. The command to set the state of the extended uplink TBF is CALL[:CELL]:TBFLow:UPLink:EXTended[:STATe] . |
||
Setting | Range: 0 | OFF | 1 | ON | |
Query | Range: 0 | 1 | |
*RST setting | 0 | |
Requirements | GSM/GPRS/ EGPRS LA | |
OUTPUT 714;"CALL:TBFLow:UPLink:EXTended:NOData ON" ! Enables the extended uplink TBF no data state. |