Last updated: December 3, 2008
The 8960 Series 10 is compliant with 3GPP 51.010 (formerly ETSI GSM 11.10).
The method of test implemented by the test set's Phase and Frequency Error measurement conforms to the measurement method defined in 3GPP 51.010, section 13.1. For GPRS mobiles which support a single uplink timeslot or two adjacent uplink timeslots, the Phase and Frequency Error measurement conforms to 3GPP 51.010, section 13.16.1. For EGPRS mobiles which support a single uplink timeslot or two adjacent uplink timeslots, the Phase and Frequency Error measurement conforms to 3GPP 51.010, section 13.16.1.
Phase and Frequency Error Measurement Description
Programming a Phase and Frequency Error Measurement for GSM
Programming a Phase and Frequency Error Measurement for GPRS and EGPRS
To make a transmitter output power measurement that conforms to 3GPP 51.010 standards, perform a Power versus Time measurement. An ETSI compliant, transmitter output power (TXPower) result is available as a result of this measurement. Pass/fail checking of the Power versus Time mask is also available by using the Power versus Time measurement. The Burst Timing Error result is available for GSM, GPRS and EGPRS on the Call Setup screen and by sending a query to the CALL subsystem ( CALL:STATus:TCHannel:TERRor? for GSM, CALL:STATus:(PDTCH|PDTChannel):TERRor? for GPRS and EGPRS).
For GPRS mobiles which support a single uplink timeslot or two adjacent uplink timeslots, the transmitter output power result conforms to 3GPP 51.010, section 13.16.2. When measuring two adjacent uplinks, each of these can have different power levels.
For EGPRS mobiles which support a single uplink timeslot or two adjacent uplink timeslots, the 8PSK burst power measurement (with averaging turned on) conforms to 3GPP 51.010, section 13.17.3. The 8PSK Estimated Carrier Power measurement meets the accuracy requirements for an estimation technique of long term average power as defined in 3GPP 51.010, annex 5.
An alternative method for testing the transmitter output power is using the Transmit Power measurement in the test set.
When the
Burst Capture Range
is set to
single
, the Transmit Power measurement implemented in the test set varies from the ETSI recommended method for measuring carrier power in terms of synchronization. This measurement synchronizes using RF amplitude synchronization instead of midamble synchronization. This was intentionally done to speed up the measurement, as this is one of the most common measurements performed in manufacturing. This alternative measurement technique is approximately four times faster than the synchronized method with the same accuracy. If the input signal meets the GSM Power versus Time characteristics, the TX Power measurement provides the same results as the Power versus Time - TX Power result (which is midamble synchronized and ETSI compliant).
NOTE |
single
, the serving cell must be either GSM or GPRS for the GSM/GPRS TX Power measurement to be used. When the serving cell is EGPRS, this measurement is not available. See
Serving Cell
for information about setting the serving cell.
When the
Burst Capture Range
is set to
All
,
Note that the output RF spectrum measurement makes the TX Power measurement as part of its measurement process.
Transmit Power Measurement Description
Programming a Transmit Power Measurement for GSM
Programming a Transmit Power Measurement for GPRS/EGPRS
Programming a EGPRS Transmit Power Measurement
Power versus Time Measurement Description
Programming a Power versus Time Measurement for GSM
Programming a Power versus Time Measurement for GPRS and EGPRS
The Output RF Spectrum due to Switching method of test conforms to ETSI GSM 11.10, section 13.4 at offsets < 1800 kHz. For GPRS mobiles which support a single uplink timeslot or two adjacent uplink timeslots, the measurement conforms to ETSI GSM 11.10, section 13.16.3 at offsets < 1800 kHz.
The Output RF Spectrum due to Modulation method of test conforms to 3GPP 51.010, section 13.4 at offsets < 1800 kHz.
For GPRS or EGPRS mobiles which support a single uplink timeslot or two adjacent uplink timeslots, the measurement conforms to 3GPP 51.010, section 13.16.3 at offsets < 1800 kHz (when the Multi-Measurement Count - Modulation parameter is set to Off using SETup:ORFSpectrum:COUNt:STATe ).
When Multi-Measurement Count (Modulation) is greater than 1, the measurement is performed over 40 or more bits in each of the regions from bit 15 to 60 and bit 87 to 132 of the burst. In 3GPP 51.010, the measurement is only specified on the latter section of the burst.
Measuring on both the front and back of the burst has two advantages. First, this method provides two modulation measurements per burst, effectively doubling measurement speed. Secondly, it provides additional information regarding the spurious performance of the mobile.
The method of test in 3GPP 51.010 is based upon time-gated spectrum analysis; this technique only allows one measurement per burst. Modern DSP techniques employed in the test set makes it possible to measure more of the burst while still excluding the unwanted effects of the midamble and switching transients generated by burst modulation.
The result of the Output RF Spectrum measurement relies on pseudo random data being present in the data field of the RF burst. When using the BLER data connection type, these data fields do not contain pseudo random data, therefore the results may not be representative.
GSM Output RF Spectrum Measurement
GPRS and EGPRS Output RF Spectrum Measurement
Programming an Output RF Spectrum Measurement for GSM
Programming an Output RF Spectrum Measurement for GPRS and EGPRS
The method of test implemented by the test set's Bit Error measurement conforms to the measurement method defined in 3GPP 51.010, section 14.2. The Bit Error measurement is available for GSM, GPRS, and EGPRS.
An alternative method of test for making a Reference Sensitivity measurement is to use the Fast Bit Error (FBER) measurement in the test set. The FBER measurement is five times faster than the normal BER measurement.
The Fast Bit Error measurement is not applicable to GPRS or EGPRS.
The Block Error (BLER) measurement which the test set provides is based on GPRS receiver tests defined in 3GPP 51.010, section 14.16 (GPRS) and section 14.18.1 (EGPRS).
The method of test implemented by the test set's Frame Erasure Rate measurement conforms to steps b) - d) of the measurement procedure defined in 3GPP 51.010 section 14.2.3.4.2 and 14.2.4.4.2 The test set does not provide a fading function as required in step a).
The In-Band Frame Error Rate (IFER) measurement provides the reference sensitivity of the speech traffic channel. IFER is defined in 3GPP 51.010, section 14.2.19 (Reference sensitivity - TCH/AFS-INB), section 14.2.20 (Reference sensitivity - TCH/AHS-INB), and 3GPP 44.010, section 5.1.7a (TCH loop without signalling of erased frames for in-band channel rate error).
Programming a Bit Error Measurement for GSM
Programming a Bit Error Measurement for GPRS
Fast Bit Error Measurement Description
Programming a Fast Bit Error Measurement
Programming a Block Error Measurement
GSM Frame Erasure Rate (FER) Measurement Description
Frequency Stability measures the absolute frequency and frequency error of an analog RF signal. The signal may be modulated by SAT and/or additional FM. Refer to IS-137A section 3.1.1.2, Analog Frequency Stability, for more information on making this measurement. Measurement resolution is 1.0 Hz, meeting the requirements in IS-137A section 6.6.1.1, Analog General Equipment, Radio frequency.
The EDGE Dynamic Power (EDP) measurement is not an ETSI specified measurement.
The Analog Audio measurements are not ETSI specified measurements.
The Analog Audio measurements are not applicable to GPRS.
The Spectrum Monitor measurement is not an ETSI specified measurement.
The method of test implemented for the Modulation Accuracy measurement conforms to the measurement method defined in 3GPP 51.010 section 13.17.1. This measurement is only applicable to EGPRS.
Modulation Accuracy Measurement Description
With proper test set configuration, the method of test implemented for the GSM Bad Frame Indication conforms to the measurement method defined in 3GPP 51.010 section 14.1.1, 14.1.2, 14.1.5 and 14.1.6. This measurement is only applicable to GSM.
GSM Bad Frame Indication (BFI) Measurement Description