Last updated: November 25, 2010
This section is only applicable to EGPRS when the test set's operating mode is EGPRS BCH, EGPRS BCH + PDTCH or EGPRS BCH + PDTCH + TCH.
Different modulation coding scheme / puncturing scheme (MCS/PS) values can be assigned to each downlink of a multislot burst if the operating mode is set to EGPRS BCH, EGPRS BCH+PDTCH or EGPRS BCH + PDTCH + TCH.
The MCSs are grouped by modulation type. MCS-1 through MCS-4 use GMSK modulation, MCS-5 through MCS-9 use 8PSK modulation, DAS-5 through DAS-9 use 16QAM modulation, while
DAS-10 through DAS-12 use 32QAM modulation. The differences in data rates within these groups of MCSs is affected by the different modulation types in conjunction with puncturing and coding schemes. You may specify a MCS/PS for each downlink burst in a multislot configuration. The following list contains all the MCS/PS available. The GPIB commands to assign separate MCS/PS to individual bursts are CALL:(PDTCH|PDTChannel):MCSCheme:EBPTest[:BURSt1] and CALL:(PDTCH|PDTChannel):MCSCheme:EBPTest:BURSt<2|3|4|5> .GMSK /8PSK /16QAM /32QAM Options
The set of puncturing schemes available is different across different modulation coding schemes. see the table below.
MCS 1 | 8.8 | Yes | Yes | No |
MCS 2 | 11.2 | Yes | Yes | No |
14.8 | Yes | Yes | Yes | |
MCS 4 | 17.6 | Yes | Yes | Yes |
MCS 5 | 22.4 | Yes | Yes | No |
MCS 6 | 29.6 | Yes | Yes | No |
MCS 7 | 44.8 | Yes | Yes | Yes |
MCS 8 | 54.4 | Yes | Yes | Yes |
MCS 9 | 59.2 | Yes | Yes | Yes |
Yes | Yes | No | ||
Yes | Yes | No | ||
Yes | Yes | No | ||
Yes | Yes | No | ||
Yes | Yes | Yes | ||
Yes | Yes | No | ||
Yes | Yes | Yes | ||
Yes | Yes | Yes |
8PSK ClearCoded
When 8PSK ClearCoded is selected, no encoding is performed on the downlink. The GPIB command mnemonic for 8PSK ClearCloded is EPSKCLEAR.
16QAM ClearCoded
When 16QAM ClearCoded is selected, no encoding is performed on the downlink. The GPIB command mnemonic for 16QAM ClearCloded is QAM16CLEAR.
32QAM ClearCoded
When 32QAM ClearCoded is selected, no encoding is performed on the downlink. The GPIB command mnemonic for 32QAM ClearCloded is QAM32CLEAR.
As Burst 1
The As Burst 1 setting of this parameter uses the modulation coding scheme and puncturing scheme is assigned to the first burst of the multislot downlink. The As Burst 1 setting cannot be assigned to burst 1 of the multislot downlink.
In order to assign different modulation coding schemes and puncturing schemes to each burst in a multislot downlink, the operating mode must be set to EGPRS BCH, EGPRS BCH+PDTCH or EGPRS BCT+PDTCH+TCH.
CALL:(PDTCH|PDTChannel):MCSCheme:EBPTest[:BURSt1]
CALL:(PDTCH|PDTChannel):MCSCheme:EBPTest:BURSt<2|3|4|5>