Last updated: December 2, 2008
Function |
This command sets/queries the speech frame delay to be used by the bad frame indication measurement. This is the delay expressed in frames from sending data on the downlink to it being looped back on the uplink by the mobile station. For more information on this parameter, please see Speech Frame Delay . |
|
EGPRS LA | ||
GSM TA | ||
This command is not applicable to GPRS. | ||
This command is not applicable to EGPRS. | ||
Setting | ||
*RST Setting | ||
Requirements | GSM/GPRS/ EGPRS LA | |
OUTPUT 714;"SETup:BFI:SFDelay 4" ! Sets the speech frame delay to 4 frames. |