Last updated: December 2, 2008
This section is only applicable to the lab applications.
The following procedure assumes that an active link is established between the test set and the mobile station. See Establishing an Active GSM Link with the Mobile Station .
10 OUTPUT 714;"SET:FFER:TIM 3000" !Set measurement timeout 20 OUTPUT 714;"SET:FFER:CONT OFF" !Set trigger to single 30 ! Set the cell power to the reference sensitivity level 40 OUTPUT 714;"CALL:POW -102" 50 OUTPUT 714;"INIT:FFER" !Initiate the measurement 60 OUTPUT 714;"FETC:FFER?"!Fetch the measurement results 70 ENTER 714;Integrity,Samples,Fer,Retx_count 80 END
The measurements returned by this program are:
Integrity
returns the
Integrity Indicator
(0 means a successful measurement with no errors).
Samples
returns the number of samples counted.
Fer
returns the ratio of frame erasures to total frames tested.
Retx_count
returns the number of retransmitted frames.