The block polling parameters allow you to specify the block polling interval the test set uses to sample blocks sent or received by the mobile station for applicable connection types. There are three connection types the test set offers that apply to block polling interval parameters:
Auto
,
BLER
, and
ETSI Type B (Ack)
. Additionally, there is a separate block polling interval field that you can set that applies to the currently selected connection type. Therefore, there are four block polling interval configurable parameters:
This parameter is only applicable when the test set's connection type is Auto, BLER or ETSI Type B.
The command to set this parameter is CALL:FUNCtion:DATA:BLOCk:POLLing:INTerval[:SELected] .
This parameter is only applicable to the lab applications.
The command to set this parameter is CALL:FUNCtion:DATA:BLOCk:POLLing:INTerval:AUTO .
The command to set this parameter is CALL:FUNCtion:DATA:BLOCk:POLLing:INTerva:BLER .
The command to set this parameter is CALL:FUNCtion:DATA:BLOCk:POLLing:INTerval:ACKB .
You can configure the block polling interval for the valid connection types at any time with the exception of Block Polling Interval (Current). The test set does not allow you to set the block polling interval for the currently selected connection type if the connection type is not applicable to the block polling interval parameters.
The command to set the connection type is CALL:FUNCtion:CONNection:TYPE .
Control
menu (
2 of 3
) appears.
Protocol Control
(
F4
).
RLC/MAC
(
F2
).
Block Polling Parameters
(
F4
). This opens the
Block Polling Parameter
menu in the center of the screen.