Last updated: January 18, 2010
The following table lists the GPIB Commands to set the
Cell Identification
parameters. Please click the parameter's corresponding GPIB command link for more information on a specific parameter. The GPIB Command tables give a description of the parameter, as well as valid settings and firmware requirements.
All of the parameters listed below are located in the
Cell Identification
menu of the test set's front panel. See
How Do I Change Cell Identification Parameters?
for the procedure to configure the cell parameters. Refer to the
Operating Considerations
below before attempting to configure the cell parameters.
CALL:G850MNCode | |
CALL:G900MNCode | |
CALL[:CELL]:BCHannel:CIDentity | |
Location Area Code | |
* Only applicable to the lab application. |
Parameters can be queried from the test set regardless of the state of the test set.
Parameter MNC, MCC, LAC, RAC, NCC, BCC, and Persistent Attach can not be set unless the Operating Mode is Cell Off. See CALL:OPERating:MODE .
If the test set is in a test mode (see Test Mode Operating Modes ) operating mode, any BCH parameter can be set at any time.
The 3 Digit MNC for PCS1900 parameter defines if the PCS BCCH should be configured using the standard 2-digit MNC (J-STD-007 coding), or the PCS 3-digit MNC (J-STD-007A coding, section 2.10.5.1.3). The PCS 3-digit MNC is used on the PCS BCCH instead of the 2-digit MNC only when the current cell band is PCS and the 3 Digit MNC for PCS parameter is set to
on
. 3 Digit MNC for PCS1900 can not be set unless the Operating Mode is Cell off and Cell Band is PCS1900.
The 3 Digit MNC for GSM850 parameter defines if the BCCH should be configured using the standard 2-digit MNC (J-STD-007 coding), or the 3-digit MNC (J-STD-007A coding, section 2.10.5.1.3). The 3-digit MNC for GSM850 is used on the BCCH instead of the 2-digit MNC only when the current cell band is GSM850 and the 3 Digit MNC for GSM850 parameter is set to
on
. 3 Digit MNC for GSM850 can not be set unless the Operating Mode is Cell off and Cell Band is GSM850.