Last updated: December 2, 2008
This section is only applicable to GPRS and EGPRS.
For the procedure to access the Control Channel Parameters, see How Do I Configure the Control Channel Parameters? .
You can configure the test set to control if and when the Packet Associated Control Channel (PACCH) Packet System Information (PSI) messages are sent.
The GPIB command to set this parameter is CALL:(PACCH|PACChannel):PSInfo .
The Periodic PSI List setting allows you to select the manner that the PSI messages will be transmitted periodically on the PACCH when a packet-switched connection is available. The two manners are:
In the standard manner, the PSI messages are sent in a fixed interval which is determined by the Periodic (P)SI repetition time , and in the following decision:
See Packet Broadcast Control Channel (PBCCH) for instructions on how to configure the PBCCH.
In the custom manner, the PSI messages are sent in a fixed interval which is determined by the Periodic (P)SI repetition time . The test set transmits a customizable set of PSI messages defined by the Custom PSI List on the PACCH. The test sets also transmits a customizable set of encapsulated SI messages defined by the separated Send encapsulated SI on PACCH .
The Periodic (P)SI repetition time setting allows you to modify the repetition rate of periodic PSI and/or SI messages which are transmitted on the PACCH when the periodic SI and/or PSI transmission is enabled.
The Packet (P)SI Status Indication Response setting allows you to modify the behavior of the test set in response to a Packet SI Status Indication or Packet PSI Status Indication message received from the DUT.
The test set response the Packet SI Status Indication or Packet PSI Status Indication message in a manner determined by the message content supplied by the DUT.
The test set response the Packet SI Status Indication or Packet PSI Status Indication message in the following decision:
The Send encapsulated SI on PACCH setting allows you to configure whether the SI messages encapsulated in Packet Serving Cell SI messages are transmitted periodically on the PACCH.
The Custom SI List Setting allows you to configure a specific set of SI messages to be transmitted on the PACCH. You can enable the transmission of SI 1, SI 2, SI 2bis, SI 2ter, SI 2quater, SI 3, SI 4 or SI 13 by setting the Custom SI List. The customizable set of SI messages will be transmit:
ON
and the
Periodic PSI List
is set to
custom
.The Custom PSI List Setting allows you to configure a specific set of PSI messages to be transmitted on PACCH. You can enable the transmission of PSI 1, PSI 2, PSI 3, SI 3bis, SI 3quater, SI 5, SI 8, SI 13 or SI 14 by setting the Custom PSI List. The customizable set of PSI messages will be transmit:
ON
and the
Periodic PSI List
is set to
custom
.
The control channel parameters can be changed in any
Operating Mode
, however the settings is only applicable when the test set is in
Active Cell Operating Mode
.
Refer to the 3GPP TS 45.002 Version 6.8.0 Section 6.3 for more details on PSI messages.