This section is only applicable to the GPRS/EGPRS lab applications.
The flexible timeslot function allows you to position timeslots within the TDMA frame as much flexibility as possible. You can use the GPIB command
CALL:(PDTCH|PDTChannel):MSLot:CONFig
to set the multislot configuration to
`Custom'
, then use the GPIB command
CALL:(PDTCH|PDTChannel):MSLot:CONFig:CUSTom:TSLots
to customize the multislot combination as your requirement.
When using the Flexible Timeslot Multislot Configuration, the following overriding restrictions apply:
The following procedure details how to access and configure the Flexible Timeslot Multislot Configuration.
PDTCH parms
(
F9
)
PDTCH parms (2 of 3).
Multislot Configuration
(
F7
).
Custom Multislot Cfg
(
F8
), Use the knob to turn on/off the downlink and uplink timeslots as you need.
Apply Changes
(
F5
) and check the custom timeslot settings on the screen. The flexible timeslot is only available in the following operating modes: Active Cell, GPRS BCH+PDTCH, EGPRS BCH+PDTCH, GPRS BCH+TCH+PDTCH and EGPRS BCH+TCH+PDTCH.
The `Burst to Measure' setting is apply to the relative uplink burst. For example, if uplink timeslots 2 and 5 have active bursts, value `1' of `Burst to Measure' refers to uplink timeslot 2 and value `2' of `Burst to Measure' refers to the uplink timeslot 5
The following measurements do not support non contiguous uplink timeslots:
The following measurements do not support non overlapped timeslots: