Last updated: December 2, 2008
The test set is capable of accepting several different preset commands.
At no time during a preset operation, does transmit power exceed the last user setting of the transmit power. The input power is not set to any value lower than the last user setting of the input power. This is to avoid power spikes on the output and possible receiver damage on the input during transitions associated with preset operations.
Partial preset saves setup time because measurement setup parameters remain unchanged. This is the recommended way to place the test set in a known condition.
When you fast switch between formats in a fast switching test application the test set behaves as if a partial preset has occurred. The table below lists some key partial preset results.
OUTPUT 714;"SYSTEM:PRESET3" !Command for a partial preset when user in !remote operation.
SYSTEM:PRESET3 is the recommended command for a partial preset operation. The SYSTEM:PRESET[1] command is not recommended for use at this time.
Press the green Preset key on the front panel to perform a partial preset.
Function | Partial Preset Result |
---|---|
Trigger Arm | no change |
Measurement parameters | no change |
no change | |
Enable registers | no change |
Positive Transition Filter registers | no change |
Negative Transition Filter registers | no change |
Contents of RAM | no change |
no change | |
Contents of error queue | no change |
Operating Mode | Active Cell |
aborted and inactivated | |
Measurement results | NAN |
1 = no result available | |
ON | |
Cell Activated State | ON |
Call in progress | aborted |
Idle | |
Call Counters | cleared |
Pending Service request | not cleared |
A full preset requires you to select new measurements and configure their parameters. If measurement parameters do not need to be changed, use a partial preset to save time.
OUTPUT 714;"*RST" !Recommended command for a full preset, sets trigger arm to single.
OUTPUT 714;"SYSTEM:PRESET2" !Command for a full preset, sets trigger arm to continuous.
The *RST common command is the recommended command for a full preset operation.
Function | Full Preset Result |
---|---|
Continuous (manual operation full preset or SYSTEM:PRESET2 command) |
|