Function | ||
GPRS TA | This command is not applicable to the GPRS test application. | |
EGPRS TA |
This command is not applicable to the EGPRS Test Application. |
|
Arm External Sync. This command will hang the GPIB bus until a successful ext sync is detected or the operation times out. See External Frame Synchronization . | ||
Requirements | GSM/GPRS/EGPRS LA | |
OUTPUT 714;"CALL:TRIG:INP:FRAM:ARM" ! Arm External Sync |
Function | ||
GPRS TA | This command is not applicable to the GPRS test application. | |
EGPRS TA |
This command is not applicable to the EGPRS Test Application. |
|
Sets/queries the External Sync to GSM frame number. The command should be set before the CALL:TRIGger:INPut:FRAMe:ARM . See External Frame Synchronization |
||
Range: 0 to 2715647 Resolution: 1 |
||
Range: 0 to 2715647 Resolution: 1 |
||
0 | ||
Requirements | GSM/GPRS LA | |
OUTPUT 714;"CALL:TRIG:INP:FRAM:FNUM 5" ! Set the External Sync to GSM frame number to be 5 |
Function | ||
GPRS TA | ||
0 | OFF | 1 | ON | ||
0 | 1 | ||
0 | ||
GSM/GPRS TA | Revision: A.01 and above | |
GSM/GPRS LA |
Function | ||
GPRS TA | ||
Range: 0 to 1250 | ||
Range: 0 to 1250 | ||
0 | ||
GSM/GPRS TA | Revision: A.01 and above | |
GSM/GPRS LA |
Function | ||
GPRS TA | ||
Range: 0 to 7 | ||
Range: 0 to 7 | ||
0 | ||
GSM/GPRS TA | Revision: A.01 and above | |
GSM/GPRS LA | ||
OUTPUT 714;"CALL:TRIGger:FRAMe:TSLot 5" ! Set the timeslot of the Every Frame trigger to 5 |