This section is only applicable to the lab applications.
The Intra Cell Handover functionality gives the user the ability to perform CS handovers procedures in the same Cell. You can choose to use the existing (and default) channel reassignment mechanism (TCH Assignment for CS) or the new Intra Cell Handover mechanism when changing the channel characteristics of a connection e.g. ARFCN, timeslot, coding scheme.
The handover type that can be implemented using the intra cell architecture include:
If the DUT fail to establish a post handover connection, the failure recovery mechanism will not return to the original channel configuration.
The GPIB command to configure the reassignment method used on the TCH is CALL:TCHannel:SIGNaling:REAssignment:TYPE
The following procedure details how to set the Intra Cell Handover parameter.
TCH Parameters
(
F8
).
3 of 3
of the
TCH Parameters
menu is displayed.
Call Signaling Parameters
(
F7
) and the Call Signaling Parameters menu appears in the center of the screen.