Last updated: December 3, 2008
This section is only applicable to the lab applications.
The Repeated SACCH functionality allows the SACCH Blocks to be repeated on both uplink and downlink to improve the robustness of the signaling link. You can choose to enable the Repeated SACCH functionality when a layer 3 message is to be sent or received in a SAPI=0 frame in the SACCH channel.
On the downlink, you can use the Repeated SACCH parameter to set the Downlink Repeated SACCH functionality, when the Repeated SACCH is set to
Continuous
, each downlink SAPI=0 SACCH Blocks are repeated without any SAPI=3 SMS blocks in between. When the Repeated SACCH is set to
On Request
, the downlink SAPI=0 SACCH Blocks are only repeated after the test set receive SRR bit in the previous uplink SACCH Layer 1 block header from DUT. (The DUT monitors SAPI=0 SACCH Blocks and if it fails to decode then it sets the SRR (SACCH Repetition Request) bit in the next uplink SACCH block.) When the Repeated SACCH is set to
Off
, the downlink SACCH Blocks are not repeated.
On Request
, the Downlink SACCH Blocks will only be repeated if the DUT has Repeated SACCH functionality implemented too.The GPIB command to enable/disable the Repeated SACCH parameter is CALL:TCHannel:(SACCH|SACChannel):REPeat[:STATe] .
The following precedure details how to set the Repeated SACCH parameter.
TCH Parameters
(
F8
).
3 of 3
of the
TCH Parameters
menu is displayed.
Call Signaling Parameters
(
F7
) and the Call Signaling Parameters menu appears in the center of the screen.
On the uplink, you can use the SACCH Repeated Order parameter to set the Uplink Repeated SACCH functionality. When the SACCH Repeated Order is set to
ON
, all downlink SACCH Blocks shall have the SRO (SACCH Repetition Order) bit set in the Layer 1 downlink block header, the DUT repeats the SAPI=0 SACCH block when the SRO in the previous downlink SACCH block is set.
The Uplink SACCH Blocks will only be repeated if the DUT has Repeated SACCH functionality implemented too.
The GPIB command to enable/disable the SACCH Repeated Order parameter is CALL:TCHannel:(SACCH|SACChannel):REPeat:ORDer .
The following precedure details how to set the SACCH Repeated Order parameter.
TCH Parameters
(
F8
).
3 of 3
of the
TCH Parameters
menu is displayed.
Call Signaling Parameters
(
F7
) and the Call Signaling Parameters menu appears in the center of the screen.For more information about Repeated SACCH, please refer to 3GPP TS 44.006 and 3GPP TS 44.006 Section 11.