How to view Measurement Reports

How to view Measurement Reports

Last updated: December 3, 2008

This section is only applicable to the lab applications.

  1. Press the Call Setup key.
  2. Press the left More key to advance the Control menu to ( 2 of 3 ).
  3. Press Measurement Reports ( F6 ).
  4. Press View ( F1 ). The Meas Reports menu is displayed on the left side of the screen. From it you can select which measurement report screen you want to view, these include: Summary Measurement Reports ( F1 ) through, SACCH Measurement Reports ( F2 ), PACCH Measurement Reports ( F3 ), and Network Control Measurement Reports ( F4 ). The Summary Measurement Reports screen is displayed by default.

    NOTE: A "----" next to a parameter indicates that the test set has not received any information from the mobile station for that parameter.