CALL:PPRocedure:ATTach

CALL:PPRocedure:ATTach

Last updated: April 27, 2013

GPIB Command Conventions

CALL:PPRocedure:ATTach:ACCept:IAReject:GMMCause

Function

GSM TA

This command is not applicable to the GSM Test Application.
GPRS TA

This command is not applicable to the GPRS Test Application.

EGPRS TA

This command is not applicable to the EGPRS Test Application.

GSM/GPRS LA

Sets the GMM Cause for Rejecting IMSI attach for non-GPRS services.

EGPRS LA
Setting

Range: 0 to 255 (decimal) See GMM Cause Information Element .

Query

Range: 0 to 255

*RST setting

111

Requirements

GSM/GPRS/ EGPRS LA

Revision: C.01 and above

Programming Example:

 
OUTPUT 714;"CALL:PPROCEDURE:ATTACH:ACCEPT:IAREJECT:GMMCAUSE 3" 
! The test set sends this GMM cause value to the MS as the reason for rejecting its attach attempt.

CALL:PPRocedure:ATTach:ACCept:IAReject:STATe

Function

GSM TA

This command is not applicable to the GSM Test Application.
GPRS TA

This command is not applicable to the GPRS Test Application.

EGPRS TA

This command is not applicable to the EGPRS Test Application.

GSM/GPRS LA

Sets/Queries IMSI attach accept state.

EGPRS LA
Setting

Range: 0| OFF | 1 | ON

Query

Range: 0 | 1

*RST setting

0

Requirements

GSM/GPRS/ EGPRS LA

Revision: C.01 and above

Programming Example:

 
OUTPUT 714;"CALL:PPROCEDURE:ATTACH:ACCEPT:IAREJECT:STATE 1" 
! The test set will now reject any attach attempt that is not for GPRS only.

CALL:PPRocedure:ATTach:ACCept:NFSupport:EMCi

Function

GSM TA

This command is not applicable to the GSM Test Application.
GPRS TA

This command is not applicable to the GPRS Test Application.

EGPRS TA

This command is not applicable to the EGPRS Test Application.

GSM/GPRS LA

Sets/Queries Emergency Bearer Services Indicator .

EGPRS LA
Setting

Range: 0 | 1

Query

Range: 0 | 1

*RST setting

0

Requirements

GSM/GPRS/ EGPRS LA

Revision: J.01.00 and above

Programming Example:

 
OUTPUT 714;"CALL:PPROCEDURE:ATTACH:ACCEPT:NFSUPPORT:EMCI 0" 
! The test set configures the emergency bearer services indicator to be 0.

CALL:PPRocedure:ATTach:ACCept:NFSupport:IMSi

Function

GSM TA

This command is not applicable to the GSM Test Application.
GPRS TA

This command is not applicable to the GPRS Test Application.

EGPRS TA

This command is not applicable to the EGPRS Test Application.

GSM/GPRS LA

Sets/Queries IMS Voice Over PS Session Indicator .

EGPRS LA
Setting

Range: 0 | 1

Query

Range: 0 | 1

*RST setting

0

Requirements

GSM/GPRS/ EGPRS LA

Revision: J.01.00 and above

Programming Example:

 
OUTPUT 714;"CALL:PPROCEDURE:ATTACH:ACCEPT:NFSUPPORT:IMSI 0" 
! The test set configures the IMS voice over PS session indicator to be 0.

CALL:PPRocedure:ATTach:IGNore[:STATe]

Function

GSM TA

This command is not applicable to the GSM Test Application.
GPRS TA

This command is not applicable to the GPRS Test Application.

EGPRS TA

This command is not applicable to the EGPRS Test Application.

GSM/GPRS LA

Sets/Queries whether or not the attach request is ignored.

EGPRS LA
Setting

Range: 0| OFF | 1 | ON

Query

Range: 0 | 1

*RST setting

0

Requirements

GSM/GPRS/ EGPRS LA

Revision: I.00.00 and above

Programming Example:

 
OUTPUT 714;"CALL:PPROCEDURE:ATTACH:IGNore 1" 
! The test set will ignore any attach attempt.

CALL:PPRocedure:ATTach:REJect:GMMCause

Function

GSM TA

This command is not applicable to the GSM Test Application.
GPRS TA

This command is not applicable to the GPRS Test Application.

EGPRS TA

This command is not applicable to the EGPRS Test Application.

GSM/GPRS LA

Sets the GMM Cause for rejecting IMSI attach.

EGPRS LA
Setting

Range: 0 to 255 (decimal) See GMM Cause Information Element .

Query

Range: 0 to 255

*RST setting

111

Requirements

GSM/GPRS/ EGPRS LA

Revision: C.01 and above

Programming Example:

 
OUTPUT 714;"CALL:PPROCEDURE:ATTACH:REJECT:GMMCAUSE 3" 
! The test set sends this GMM cause value to the MS as the reason for rejecting its attach attempt. 

CALL:PPRocedure:ATTach:REJect:STATe

Function

GSM TA

This command is not applicable to the GSM Test Application.
GPRS TA

This command is not applicable to the GPRS Test Application.

EGPRS TA

This command is not applicable to the EGPRS Test Application.

GSM/GPRS LA

Sets/Queries IMSI attach reject state.

EGPRS LA
Setting

Range: 0| OFF | 1 | ON

Query

Range: 0 | 1

*RST setting

0

Requirements

GSM/GPRS/ EGPRS LA

Revision: C.01 and above

Programming Example:

 
OUTPUT 714;"CALL:PPROCEDURE:ATTACH:REJECT:STATE 1" 
! Turns state on.  Now the test set will reject all attach attempts.