Function
|
GSM TA
|
This command is not applicable to the GSM test applications. |
GPRS TA |
This command is not applicable to the GPRS test applications. |
EGPRS TA |
This command is not applicable to the EGPRS test applications. |
GSM/GPRS LA |
This command sets the CM Service Reject cause.
|
EGPRS LA |
Setting |
Range: 0 to 255 (decimal)
|
Query
|
Range:0 to 255
|
*RST setting
|
17
|
Requirements
|
GSM/GPRS/ EGPRS LA |
Revision: J.00.00 and above
|
Programming Example:
OUTPUT 714;"CALL:PPRocedure:CMService:REJect:MMCause 7"
! The test set sends the MS the CM Service Reject cause value as "GPRS Services Not Allowed".
|