Last updated: December 3, 2008
This command is not applicable to the GSM test applications. | ||
GPRS TA |
This command sends detach request. For an explanation of the :DONE?, :OPComplete?, :SEQuential, and :WAIT commands, see Call Processing Event Synchronization . |
|
EGPRS TA | ||
GSM/GPRS LA | ||
EGPRS LA | ||
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:PPRocedure:DETach:REQuest" ! Sends a network initiated Detach Request. |
This command is not applicable to the GSM test applications. | ||
GPRS TA |
This command sets/queries the GMM Cause for the test set to send a detach request. See GMM Cause Information Element for details on settings this parameter accepts as defined in 3GPP TS 24.008 Version 6.7.0. |
|
EGPRS TA | ||
GSM/GPRS LA | ||
EGPRS LA | ||
Setting | ||
+111 | ||
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:PPRocedure:DETach:REQuest:GMMCause 96" ! The test set sends the MS this GMM Cause value as the reason for requesting a detach. |
This command is not applicable to the GSM test applications. | ||
GPRS TA |
This command sets/queries the type of detach request. See Detach Type Information Element for details on settings this parameter accepts. |
|
EGPRS TA | ||
GSM/GPRS LA | ||
EGPRS LA | ||
Setting | ||
NREQ | ||
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:PPRocedure:DETach:REQuest:TYPE REQ" ! Sets the detach type to REQ. |