This command is not applicable to the GSM Test Application. | ||
GPRS TA |
This command is not applicable to the GPRS Test Application. |
|
EGPRS TA |
This command is not applicable to the EGPRS Test Application. |
|
GSM/GPRS LA | Sets/Queries the Subscribed Reliability Class of QOS Profile 1, 2, 3 or 4 which represents Quality of Service Reliability Class that will be supplied to the MS if it requests its subscribed value. The subscribed reliability class is only applicable for pre R99 Context Request messages. See GSM 05.08 for specific values. Some values are listed below. | |
EGPRS LA | ||
Range: 0 to 7 (decimal) 0: (Undefined) 1: (Ack GTP, LLC, RLC;Protected Data) 2: (Unack GTP, ack LLC, RLC;Protected Data) 3: (Unack GTP, LLC, ack RLC;Protected Data) 4: (Unack GTP, LLC, RLC;Protected Data) 5: (Unack GTP, LLC, RLC;Unprotected Data) 6: (Undefined) 7: (Undefined) |
||
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:PPROCEDURE:QOSPROFILE2:PDPCONTEXT:AACCEPT:QOSERVICE:RCLASS:SUBSCRIBED 5" ! Sets the subscribed QoS Reliability Class of QOS Profile 2 to 5. |
This command is not applicable to the GSM Test Application. | ||
GPRS TA |
This command is not applicable to the GPRS Test Application. |
|
EGPRS TA |
This command is not applicable to the EGPRS Test Application. |
|
GSM/GPRS LA |
Sets/Queries the Override Requested Reliability Class state of QOS Profile 1, 2, 3 or 4. |
|
EGPRS LA | ||
Setting | ||
0 | ||
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:PPROCEDURE:QOSPROFILE2:PDPCONTEXT:AACCEPT:QOSERVICE:RCLASS:ENFORCE:STATE 1" ! The test set will now override the QoS requested by the MS if QOSPROFILE2 is allocated. |
This command is not applicable to the GSM Test Application. | ||
GPRS TA |
This command is not applicable to the GPRS Test Application. |
|
EGPRS TA |
This command is not applicable to the EGPRS Test Application. |
|
GSM/GPRS LA | Sets/Queries the Override Requested Reliability Class Value of QOS Profile 1, 2, 3 or 4 which represents Quality of Service Reliability Class that will be supplied to the DUT when the Override Requested Reliability Class State is set to ON. See GSM 04.08 for specific values. The values are listed below. | |
EGPRS LA | ||
Range: 0 to 7 (decimal) 0: (Undefined) 1: (Ack GTP, LLC, RLC;Protected Data) 2: (Unack GTP, ack LLC, RLC;Protected Data) 3: (Unack GTP, LLC, ack RLC;Protected Data) 4: (Unack GTP, LLC, RLC;Protected Data) 5: (Unack GTP, LLC, RLC;Unprotected Data) 6: (Undefined) 7: (Undefined) |
||
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:PPROCEDURE:QOSPROFILE2:PDPCONTEXT:AACCEPT:QOSERVICE:RCLASS:ENFORCE:Value 1" ! Set the Override Reliability Class value of QOS Profile 2 to 1. |
This command is not applicable to the GSM Test Application. | ||
GPRS TA |
This command is not applicable to the GPRS Test Application. |
|
EGPRS TA |
This command is not applicable to the EGPRS Test Application. |
|
GSM/GPRS LA | Sets/Queries the SM Cause for Rejecting PDP Context. | |
EGPRS LA | ||
Setting |
Range: 0 to 255 (decimal) See SM Cause Information Element . |
|
111 | ||
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:PPROCEDURE:PDPCONTEXT:AREJECT:SMCAUSE 37" ! The test set sends SM Cause value 37 to the MS when it rejects its PDP Context Request |
This command is not applicable to the GSM Test Application. | ||
GPRS TA |
This command is not applicable to the GPRS Test Application. |
|
EGPRS TA |
This command is not applicable to the EGPRS Test Application. |
|
GSM/GPRS LA |
Sets/Queries the PDP Context Reject state. See Activate PDP Context Reject |
|
EGPRS LA | ||
Setting | ||
0 | ||
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:PPROCEDURE:PDPCONTEXT:AREJECT:STATE 1" ! Sets the test set to reject all PDP Context Requests |
This command is not applicable to the GSM Test Application. | ||
GPRS TA |
This command is not applicable to the GPRS Test Application. |
|
EGPRS TA |
This command is not applicable to the EGPRS Test Application. |
|
GSM/GPRS LA |
Sets/Queries the Network Initiated PDP Context state. See Network Initiated PDP Context |
|
EGPRS LA | ||
Setting | ||
1 | ||
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:PPR:PDPC:NIN 1" ! Sets the Network Initiated PDP Context State to ON |
This command is not applicable to the GSM Test Application. | ||
GPRS TA |
This command is not applicable to the GPRS Test Application. |
|
EGPRS TA |
This command is not applicable to the EGPRS Test Application. |
|
GSM/GPRS LA | Sets/Queries Packet Flow Identifier (PFI) of QOS Profile 1, 2, 3 or 4 respectively. | |
EGPRS LA | ||
Setting | ||
0 | ||
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:PPROCEDURE:QOSPROFILE2:PFI 2" ! Set the PFI of QOS Profile 2 to 2 (SMS). |
This command is not applicable to the GSM Test Application. | ||
GPRS TA |
This command is not applicable to the GPRS Test Application. |
|
EGPRS TA |
This command is not applicable to the EGPRS Test Application. |
|
GSM/GPRS LA | Sets/Queries Traffic Class of QOS Profile 1, 2, 3 or 4 respectively. | |
EGPRS LA | ||
Setting | ||
INT | ||
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:PPROCEDURE:QOSPROFILE2:TCLass STR" ! Set the Traffic class of QOS Profile 2 to Streaming. |
This command is not applicable to the GSM Test Application. | ||
GPRS TA |
This command is not applicable to the GPRS Test Application. |
|
EGPRS TA |
This command is not applicable to the EGPRS Test Application. |
|
GSM/GPRS LA |
Sets/Queries the Traffic Handling Priority of QOS Profile 1, 2, 3 or 4 respectively. |
|
EGPRS LA | ||
Setting | ||
2 | ||
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:PPROCEDURE:QOSPROFILE2:THPRIORITY 1" ! Sets Traffic Handling Priority of QOS Profile 2 to 1. |