CALL:PPRocedure:PMEasurement:MPRequest

CALL:PPRocedure:PMEasurement:MPRequest

Last updated: December 3, 2008

GPIB Command Conventions

CALL:PPRocedure:PMEasurement:MPRequest:MAData

Function

GSM TA

This command is not applicable to the GSM Test Application.
GPRS TA

This command is not applicable to the GPRS Test Application.

EGPRS TA

This command is not applicable to the EGPRS Test Application.

GSM/GPRS LA Includes or excludes the optional E-OTD Measurement Assistance Data element from the Measure Position Request component.
EGPRS LA

Setting

INCLude|EXCLude

Query

INCL|EXCL

*RST setting

EXCL

Requirements

GSM/GPRS/ EGPRS LA

Revision: C.01 and above

Programming Example:

 
OUTPUT 714;"CALL:PPRocedure:PMEasurement:MPRequest:MAData INCL"

CALL:PPRocedure:PMEasurement:MPRequest:MAData:BTS[<n>]:BCHCarrier

Function

GSM TA

This command is not applicable to the GSM Test Application.
GPRS TA

This command is not applicable to the GPRS Test Application.

EGPRS TA

This command is not applicable to the EGPRS Test Application.

GSM/GPRS LA Sets the value of the BCCH Carrier field in the E-OTD Measurement Assistance Data element. This field indicates the absolute RF channel number of the BTS indicated by the [<n>] mnemonic, where n can range from 1 to 8.
The E-OTD Measurement Assistance Data element is optional. Use the CALL:PPRocedure:PMEasurement:MPRequest:MAData command to have it included.
EGPRS LA

Setting

Range: 0 to 1023
Resolution: 1

Query

Range: 0 to 1023
Resolution: 1

*RST setting

0

Requirements

GSM/GPRS/ EGPRS LA

Revision: C.01 and above

Programming Example:

 
OUTPUT 714;"CALL:PPRocedure:PMEasurement:MPRequest:MAData:BTS2:BCHCarrier 556"

CALL:PPRocedure:PMEasurement:MPRequest:MAData:BTS[<n>]:BSICode

Function

GSM TA

This command is not applicable to the GSM Test Application.
GPRS TA

This command is not applicable to the GPRS Test Application.

EGPRS TA

This command is not applicable to the EGPRS Test Application.

GSM/GPRS LA Sets the value of the BSIC field in the E-OTD Measurement Assistance Data element. This field indicates the BSIC the BTS indicated by the [<n>] mnemonic, where n can range from 1 to 8.

The E-OTD Measurement Assistance Data element is optional. Use the CALL:PPRocedure:PMEasurement:MPRequest:MAData command to have it included.
EGPRS LA

Setting

Range: 0 to 63
Resolution: 1

Query

Range: 0 to 63
Resolution: 1

*RST setting

0

Requirements

GSM/GPRS/ EGPRS LA

Revision: C.01 and above

Programming Example:

 
OUTPUT 714;"CALL:PPRocedure:PMEasurement:MPRequest:MAData:BTS2:BCICode 8"

CALL:PPRocedure:PMEasurement:MPRequest:MAData:BTS[<n>]:CASSistance

Function

GSM TA

This command is not applicable to the GSM Test Application.
GPRS TA

This command is not applicable to the GPRS Test Application.

EGPRS TA

This command is not applicable to the EGPRS Test Application.

GSM/GPRS LA Includes or excludes the optional Calculation Assistance Data fields from the E-OTD Reference BTS for Assistance Data element for the BTS indicated by the [<n>} mnemonic, where n can range from 1 to 8. You can set the value of these fields using the following commands: CALL:PPRocedure:PMEasurement:MPRequest:MAData:BTS[<n>]:CASSistance:FRTDiff CALL:PPRocedure:PMEasurement:MPRequest:MAData:BTS[<n>]:CASSistance:RNORth CALL:PPRocedure:PMEasurement:MPRequest:MAData:BTS[<n>]:CASSistance:REASt
EGPRS LA

Setting

INCLude|EXCLude

Query

INCL|EXCL

*RST setting

EXCL

Requirements

GSM/GPRS/ EGPRS LA

Revision: C.01 and above

Programming Example:

 
OUTPUT 714;"CALL:PPRocedure:PMEasurement:MPRequest:MAData:BTS2:CASSistance INCL"

CALL:PPRocedure:PMEasurement:MPRequest:MAData:BTS[<n>]:CASSistance:FRTDiff

Function

GSM TA

This command is not applicable to the GSM Test Application.
GPRS TA

This command is not applicable to the GPRS Test Application.

EGPRS TA

This command is not applicable to the EGPRS Test Application.

GSM/GPRS LA Sets the value of the optional Fine RTD field in the E-OTD Measurement Assistance Data element. This field indicates the fine RTD value between the BTS indicated by the [<n>] mnemonic (where n can range from 1 to 8) and the reference BTS.

This field is optional. Use the CALL:PPRocedure:PMEasurement:MPRequest:MAData:BTS[<n>]:CASSistance command to have it included.
EGPRS LA

Setting

Range: 0 to 255
Resolution: 1 bit

Query

Range: 0 to 255
Resolution: 1 bit

*RST setting

0

Requirements

GSM/GPRS/ EGPRS LA

Revision: C.01 and above

Programming Example:

 
OUTPUT 714;"CALL:PPRocedure:PMEasurement:MPRequest:MAData:BTS2:CASSistance:FRTDiff 220"

CALL:PPRocedure:PMEasurement:MPRequest:MAData:BTS[<n>]:CASSistance:RALTitude

Function

GSM TA

This command is not applicable to the GSM Test Application.
GPRS TA

This command is not applicable to the GPRS Test Application.

EGPRS TA

This command is not applicable to the EGPRS Test Application.

GSM/GPRS LA Includes or excludes the optional Calculation Assistance Data Relative Altitude field from the E-OTD Reference BTS for Assistance Data element for the BTS indicated by the [<n>] mnemonic, where n can range from 1 to 8. You can set the value of this field using the CALL:PPRocedure:PMEasurement:MPRequest:MAData:BTS[<n>]:CASSistance:RALTitude:VALue command.
EGPRS LA

Setting

INCLude|EXCLude

Query

INCL|EXCL

*RST setting

EXCL

Requirements

GSM/GPRS/ EGPRS LA

Revision: C.01 and above

Programming Example:

 
OUTPUT 714;"CALL:PPRocedure:PMEasurement:MPRequest:MAData:BTS2:CASSistance INCL"

CALL:PPRocedure:PMEasurement:MPRequest:MAData:BTS[<n>]:CASSistance:RALTitude:VALue

Function

GSM TA

This command is not applicable to the GSM Test Application.
GPRS TA

This command is not applicable to the GPRS Test Application.

EGPRS TA

This command is not applicable to the EGPRS Test Application.

GSM/GPRS LA Sets the value of the Relative Altitude field in the E-OTD Measurement Assistance Data element. This field indicates the altitude of the BTS indicated by the [<n>] mnemonic (where n can range from 1 to 8) relative to the reference BTS in meters.

This field is optional. Use the CALL:PPRocedure:PMEasurement:MPRequest:MAData:BTS[<n>]:CASSistance:RALTitude command to have it included. or excludes the optional E-OTD Measurement Assistance Data element from the Measure Position Request component.
EGPRS LA

Setting

Range: -4000 to 4000
Resolution: 1

Query

Range: -4000 to 4000
Resolution: 1

*RST setting

0

Requirements

GSM/GPRS/ EGPRS LA

Revision: C.01 and above

Programming Example:

 
OUTPUT 714;"CALL:PPRocedure:PMEasurement:MPRequest:MAData:BTS2:CASSistance:RALTitude:VALue 2000"

CALL:PPRocedure:PMEasurement:MPRequest:MAData:BTS[<n>]:CASSistance:REASt

Function

GSM TA

This command is not applicable to the GSM Test Application.
GPRS TA

This command is not applicable to the GPRS Test Application.

EGPRS TA

This command is not applicable to the EGPRS Test Application.

GSM/GPRS LA Sets the value of the optional Relative East field in the E-OTD Measurement Assistance Data element. This field indicates the distance between the BTS indicated by the [<n>] mnemonic (where n can range from 1 to 8) and the reference BTS in the east-west direction.

This field is optional. Use the CALL:PPRocedure:PMEasurement:MPRequest:MAData:BTS[<n>]:CASSistance command to have it included.
EGPRS LA

Setting

Range: -200000 to 200000
Resolution: 1

Query

Range: -200000 to 200000
Resolution: 1

*RST setting

0

Requirements

GSM/GPRS/ EGPRS LA

Revision: C.01 and above

Programming Example:

 
OUTPUT 714;"CALL:PPRocedure:PMEasurement:MPRequest:MAData:BTS2:CASSistance:REASt -200"

CALL:PPRocedure:PMEasurement:MPRequest:MAData:BTS[<n>]:CASSistance:RNORth

Function

GSM TA

This command is not applicable to the GSM Test Application.
GPRS TA

This command is not applicable to the GPRS Test Application.

EGPRS TA

This command is not applicable to the EGPRS Test Application.

GSM/GPRS LA Sets the value of the optional Relative North field in the E-OTD Measurement Assistance Data element. This field indicates the distance between the BTS indicated by the [<n>] mnemonic (where n can range from 1 to 8) and the reference BTS in the north-south direction.

This field is optional. Use the CALL:PPRocedure:PMEasurement:MPRequest:MAData:BTS[<n>]:CASSistance command to have it included.
EGPRS LA

Setting

Range: -200000 to 200000
Resolution: 1

Query

Range: -200000 to 200000
Resolution: 1

*RST setting

0

Requirements

GSM/GPRS/ EGPRS LA

Revision: C.01 and above

Programming Example:

 
OUTPUT 714;"CALL:PPRocedure:PMEasurement:MPRequest:MAData:BTS2:CASSistance:RNORth -22000"

CALL:PPRocedure:PMEasurement:MPRequest:MAData:BTS[<n>]:MOFFset

Function

GSM TA

This command is not applicable to the GSM Test Application.
GPRS TA

This command is not applicable to the GPRS Test Application.

EGPRS TA

This command is not applicable to the EGPRS Test Application.

GSM/GPRS LA Sets the value of the Multiframe Offset field in the E-OTD Measurement Assistance Data element. This field indicates the frame offset between the BTS indicated by the [<n>] mnemonic (where n can range from 1 to 8) and the reference BTS.

The E-OTD Measurement Assistance Data element is optional. Use the CALL:PPRocedure:PMEasurement:MPRequest:MAData command to have it included.
EGPRS LA

Setting

Range: 0 to 51
Resolution: 1

Query

Range: 0 to 51
Resolution: 1

*RST setting

0

Requirements

GSM/GPRS/ EGPRS LA

Revision: C.01 and above

Programming Example:

 
OUTPUT 714;"CALL:PPRocedure:PMEasurement:MPRequest:MAData:BTS2:MOFFset 30"

CALL:PPRocedure:PMEasurement:MPRequest:MAData:BTS:NUMBer

Function

GSM TA

This command is not applicable to the GSM Test Application.
GPRS TA

This command is not applicable to the GPRS Test Application.

EGPRS TA

This command is not applicable to the EGPRS Test Application.

GSM/GPRS LA Sets the value of the Number of BTS field in the E-OTD Measurement Assistance Data element. This field indicates how many BTS are included in this information element.
The E-OTD Measurement Assistance Data element is optional. Use the CALL:PPRocedure:PMEasurement:MPRequest:MAData command to have it included.
EGPRS LA

Setting

Range: 1 to 8
Resolution: 1

Query

Range: 1 to 8
Resolution: 1

*RST setting

1

Requirements

GSM/GPRS/ EGPRS LA

Revision: C.01 and above

Programming Example:

 
OUTPUT 714;"CALL:PPRocedure:PMEasurement:MPRequest:MAData:BTS:NUMBer 3"

CALL:PPRocedure:PMEasurement:MPRequest:MAData:BTS[<n>]:RRTDiff

Function

GSM TA

This command is not applicable to the GSM Test Application.
GPRS TA

This command is not applicable to the GPRS Test Application.

EGPRS TA

This command is not applicable to the EGPRS Test Application.

GSM/GPRS LA Sets the value of the Rough RTD field in the E-OTD Measurement Assistance Data element. This field indicates the rough RTD value between the BTS indicated by the [<n>] mnemonic (where n can range from 1 to 8) and the reference BTS.

The E-OTD Measurement Assistance Data element is optional. Use the CALL:PPRocedure:PMEasurement:MPRequest:MAData command to have it included.
EGPRS LA

Setting

Range: 0 to 1250
Resolution: 1 bit

Query

Range: 0 to 1250
Resolution: 1 bit

*RST setting

0

Requirements

GSM/GPRS/ EGPRS LA

Revision: C.01 and above

Programming Example:

 
OUTPUT 714;"CALL:PPRocedure:PMEasurement:MPRequest:MAData:BTS2:RRTDiff 120"

CALL:PPRocedure:PMEasurement:MPRequest:MAData:BTS[<n>]:TSSCheme

Function

GSM TA

This command is not applicable to the GSM Test Application.
GPRS TA

This command is not applicable to the GPRS Test Application.

EGPRS TA

This command is not applicable to the EGPRS Test Application.

GSM/GPRS LA Sets the value of the Time Slot Scheme field in the E-OTD Measurement Assistance Data element. This field indicates the type of transmission scheme used by the BTS indicated by the [<n>] mnemonic, where n can range from 1 to 8.

The E-OTD Measurement Assistance Data element is optional. Use the CALL:PPRocedure:PMEasurement:MPRequest:MAData command to have it included.
EGPRS LA

Setting

Range: 0 to 1
Resolution: 1

0: All timeslots are 156.25 bits long
1: Time slots 0 and 4 are 157 bits long, all other are 156 bits long

Query

Range: 0 to 1
Resolution: 1

*RST setting

1

Requirements

GSM/GPRS/ EGPRS LA

Revision: C.01 and above

Programming Example:

 
OUTPUT 714;"CALL:PPRocedure:PMEasurement:MPRequest:MAData:BTS2:TSSCheme 0"

CALL:PPRocedure:PMEasurement:MPRequest:PINStruction:ACCuracy

Function

GSM TA

This command is not applicable to the GSM Test Application.
GPRS TA

This command is not applicable to the GPRS Test Application.

EGPRS TA

This command is not applicable to the EGPRS Test Application.

GSM/GPRS LA Includes or excludes the optional Accuracy field from the Positioning Instructions element. You can set the value of this field using the CALL:PPRocedure:PMEasurement:MPRequest:PINStruction:ACCuracy:VALue command.
EGPRS LA

Setting

INCLude|EXCLude

Query

INCL|EXCL

*RST setting

EXCL

Requirements

GSM/GPRS/ EGPRS LA

Revision: C.01 and above

Programming Example:

 
OUTPUT 714;"CALL:PPRocedure:PMEasurement:MPRequest:PINStruction:ACCuracy INCL"

CALL:PPRocedure:PMEasurement:MPRequest:PINStruction:ACCuracy:VALue

Function

GSM TA

This command is not applicable to the GSM Test Application.
GPRS TA

This command is not applicable to the GPRS Test Application.

EGPRS TA

This command is not applicable to the EGPRS Test Application.

GSM/GPRS LA Sets the value of the Accuracy field in the Positioning Instructions element. This indicates the required accuracy of the latitude and longitude for the location estimate.
This field is optional. Use the CALL:PPRocedure:PMEasurement:MPRequest:PINStruction:ACCuracy command to have it included.
EGPRS LA

Setting

Range: 0 to 127
Resolution: 1

Query

0 to 127

*RST setting

127

Requirements

GSM/GPRS/ EGPRS LA

Revision: C.01 and above

Programming Example:

 
OUTPUT 714;"CALL:PPRocedure:PMEasurement:MPRequest:PINStruction:ACCuracy:VALue 55"

CALL:PPRocedure:PMEasurement:MPRequest:PINStruction:ECHaracter

Function

GSM TA

This command is not applicable to the GSM Test Application.
GPRS TA

This command is not applicable to the GPRS Test Application.

EGPRS TA

This command is not applicable to the EGPRS Test Application.

GSM/GPRS LA Includes or excludes the optional Environment Characterization field from the Positioning Instructions element. You can set the value of this field using the CALL:PPRocedure:PMEasurement:MPRequest:PINStruction:ECHaracter:VALue command.
EGPRS LA

Setting

INCLude|EXCLude

Query

INCL|EXCL

*RST setting

EXCL

Requirements

GSM/GPRS/ EGPRS LA

Revision: C.01 and above

Programming Example:

 
OUTPUT 714;"CALL:PPRocedure:PMEasurement:MPRequest:PINStruction:ECHaracter INCL"

CALL:PPRocedure:PMEasurement:MPRequest:PINStruction:ECHaracter:VALue

Function

GSM TA

This command is not applicable to the GSM Test Application.
GPRS TA

This command is not applicable to the GPRS Test Application.

EGPRS TA

This command is not applicable to the EGPRS Test Application.

GSM/GPRS LA Sets the value of the Environment Characterization field in the Positioning Instructions element. This field provides the MS with information about expected multipath in the current area.
This field is optional. Use the CALL:PPRocedure:PMEasurement:MPRequest:PINStruction:ECHaracter command to have it included.
EGPRS LA

Setting

Range: 0 to 3

0: Heavy multipath
1: Light multipath
2: Not Defined
3: Reserved

Query

0 to 3

*RST setting

0

Requirements

GSM/GPRS/ EGPRS LA

Revision: C.01 and above

Programming Example:

 
OUTPUT 714;"CALL:PPRocedure:PMEasurement:MPRequest:PINStruction:ECHaracter:VALue 0"

CALL:PPRocedure:PMEasurement:MPRequest:PINStruction:MSETs

Function

GSM TA

This command is not applicable to the GSM Test Application.
GPRS TA

This command is not applicable to the GPRS Test Application.

EGPRS TA

This command is not applicable to the EGPRS Test Application.

GSM/GPRS LA Sets the Multiple Sets field in the Positioning Instructions element. This indicates if the MS should send multiple E-OTD Measurement Information Sets.
EGPRS LA

Setting

0|1

0: Sending of multiple sets is allowed
1: Sending of multiple sets is not allowed

Query

0|1

*RST setting

0

Requirements

GSM/GPRS/ EGPRS LA

Revision: C.01 and above

Programming Example:

 
OUTPUT 714;"CALL:PPRocedure:PMEasurement:MPRequest:PINStruction:MSETs 1"

CALL:PPRocedure:PMEasurement:MPRequest:PINStruction:MTYPe

Function

GSM TA

This command is not applicable to the GSM Test Application.
GPRS TA

This command is not applicable to the GPRS Test Application.

EGPRS TA

This command is not applicable to the EGPRS Test Application.

GSM/GPRS LA Sets the Method Type field in the Positioning Instructions element.
EGPRS LA

Setting

Range: 0 to 3

0: MS assisted
1: MS based
2: MS based preferred, but MS assisted is allowed
3: MS assisted preferred, but MS based is allowed

Query

0 to 3

*RST setting

0

Requirements

GSM/GPRS/ EGPRS LA

Revision: C.01 and above

Programming Example:

 
OUTPUT 714;"CALL:PPRocedure:PMEasurement:MPRequest:PINStruction:MTYPe 1"

CALL:PPRocedure:PMEasurement:MPRequest:PINStruction:RTIMe

Function

GSM TA

This command is not applicable to the GSM Test Application.
GPRS TA

This command is not applicable to the GPRS Test Application.

EGPRS TA

This command is not applicable to the EGPRS Test Application.

GSM/GPRS LA Sets the Response Time field in the Positioning Instructions element. This indicates the desired time for the MS to respond to the RRLP message.
EGPRS LA

Setting

Range: 0 to 7

The response time is 2N seconds, where N is the value of the Response Time field. Therefore,
0: 1 second 4: 16 seconds
1: 2 seconds 5: 32 seconds
2: 4 seconds 6: 64 seconds
3: 8 seconds 7: 128 seconds

Query

0 to 7

*RST setting

2

Requirements

GSM/GPRS/ EGPRS LA

Revision: C.01 and above

Programming Example:

 
OUTPUT 714;"CALL:PPRocedure:PMEasurement:MPRequest:PINStruction:RTIMe 1"

CALL:PPRocedure:PMEasurement:MPRequest:RAData

Function

GSM TA

This command is not applicable to the GSM Test Application.
GPRS TA

This command is not applicable to the GPRS Test Application.

EGPRS TA

This command is not applicable to the EGPRS Test Application.

GSM/GPRS LA Includes or excludes the optional E-OTD Reference BTS for Assistance Data element from the Measure Position Request component.
EGPRS LA

Setting

INCLude|EXCLude

Query

INCL|EXCL

*RST setting

EXCL

Requirements

GSM/GPRS/ EGPRS LA

Revision: C.01 and above

Programming Example:

 
OUTPUT 714;"CALL:PPRocedure:PMEasurement:MPRequest:RAData INCL"

CALL:PPRocedure:PMEasurement:MPRequest:RAData:BTSPosition

Function

GSM TA

This command is not applicable to the GSM Test Application.
GPRS TA

This command is not applicable to the GPRS Test Application.

EGPRS TA

This command is not applicable to the EGPRS Test Application.

GSM/GPRS LA Includes or excludes the optional BTS Position field from the E-OTD Reference BTS for Assistance Data element. You can set the value of this field using the CALL:PPRocedure:PMEasurement:MPRequest:PINStruction:ECHaracter:VALue command.
EGPRS LA

Setting

INCLude|EXCLude

Query

INCL|EXCL

*RST setting

EXCL

Requirements

GSM/GPRS/ EGPRS LA

Revision: C.01 and above

Programming Example:

 
OUTPUT 714;"CALL:PPRocedure:PMEasurement:MPRequest:RAData:BTSPosition INCL"

CALL:PPRocedure:PMEasurement:MPRequest:RAData:BTSPosition:ALTitude

Function

GSM TA

This command is not applicable to the GSM Test Application.
GPRS TA

This command is not applicable to the GPRS Test Application.

EGPRS TA

This command is not applicable to the EGPRS Test Application.

GSM/GPRS LA Sets the Degrees Altitude for the BTS Position field.
The BTS Position field is optional. Use the CALL:PPRocedure:PMEasurement:MPRequest:RAData:BTSPosition command to have it included.
EGPRS LA

Setting

Range: 0 to 32767
Resolution: 1

Query

Range: 0 to 32767
Resolution: 1

*RST setting

0

Requirements

GSM/GPRS/ EGPRS LA

Revision: C.01 and above

Programming Example:

 
OUTPUT 714;"CALL:PPRocedure:PMEasurement:MPRequest:RAData:BTSPosition:ALTitude 456"

CALL:PPRocedure:PMEasurement:MPRequest:RAData:BTSPosition:ALTitude:DIRection

Function

GSM TA

This command is not applicable to the GSM Test Application.
GPRS TA

This command is not applicable to the GPRS Test Application.

EGPRS TA

This command is not applicable to the EGPRS Test Application.

GSM/GPRS LA Sets the Direction of Altitude for the BTS Position field.
The BTS Position field is optional. Use the CALL:PPRocedure:PMEasurement:MPRequest:RAData:BTSPosition command to have it included.
EGPRS LA

Setting

ABOVe|BELow

Query

ABOV|BEL

*RST setting

ABOV

Requirements

GSM/GPRS/ EGPRS LA

Revision: C.01 and above

Programming Example:

 
OUTPUT 714;"CALL:PPRocedure:PMEasurement:MPRequest:RAData:BTSPosition:ALTitude:DIRection BELow"

CALL:PPRocedure:PMEasurement:MPRequest:RAData:BTSPosition:LATitude:DEGRees

Function

GSM TA

This command is not applicable to the GSM Test Application.
GPRS TA

This command is not applicable to the GPRS Test Application.

EGPRS TA

This command is not applicable to the EGPRS Test Application.

GSM/GPRS LA Sets the Degrees Latitude for the BTS Position field.
The BTS Position field is optional. Use the CALL:PPRocedure:PMEasurement:MPRequest:RAData:BTSPosition command to have it included.
EGPRS LA

Setting

Range: 0 to 2147483647
Resolution: 1

Query

Range: 0 to 2147483647
Resolution: 1

*RST setting

0

Requirements

GSM/GPRS/ EGPRS LA

Revision: C.01 and above

Programming Example:

 
OUTPUT 714;"CALL:PPRocedure:PMEasurement:MPRequest:RAData:BTSPosition:LATitude:DEGRees 4567131"

CALL:PPRocedure:PMEasurement:MPRequest:RAData:BTSPosition:LATitude:SIGN

Function

GSM TA

This command is not applicable to the GSM Test Application.
GPRS TA

This command is not applicable to the GPRS Test Application.

EGPRS TA

This command is not applicable to the EGPRS Test Application.

GSM/GPRS LA Includes Sets the Direction of Latitude for the BTS Position field.
The BTS Position field is optional. Use the CALL:PPRocedure:PMEasurement:MPRequest:RAData:BTSPosition command to have it included. excludes the optional E-OTD Measurement Assistance Data element from the Measure Position Request component.
EGPRS LA

Setting

NORTh|SOUTh

Query

NORT|SOUT

*RST setting

NORT

Requirements

GSM/GPRS/ EGPRS LA

Revision: C.01 and above

Programming Example:

 
OUTPUT 714;"CALL:PPRocedure:PMEasurement:MPRequest:RAData:BTSPosition:LATitude:SIGN NORTh"

CALL:PPRocedure:PMEasurement:MPRequest:RAData:BTSPosition:LONGitude:DEGRees

Function

GSM TA

This command is not applicable to the GSM Test Application.
GPRS TA

This command is not applicable to the GPRS Test Application.

EGPRS TA

This command is not applicable to the EGPRS Test Application.

GSM/GPRS LA Sets the Degrees Longitude for the BTS Position field.
The BTS Position field is optional. Use the CALL:PPRocedure:PMEasurement:MPRequest:RAData:BTSPosition command to have it included.
EGPRS LA

Setting

Range: -2147483647 to 2147483647
Resolution: 1

Query

Range: -2147483647 to 2147483647
Resolution: 1

*RST setting

0

Requirements

GSM/GPRS/ EGPRS LA

Revision: C.01 and above

Programming Example:

 
OUTPUT 714;"CALL:PPRocedure:PMEasurement:MPRequest:RAData:BTSPosition:LONGitude:DEGRees 4567131"

CALL:PPRocedure:PMEasurement:MPRequest:RAData:BTSPosition:TYPe

Function

GSM TA

This command is not applicable to the GSM Test Application.
GPRS TA

This command is not applicable to the GPRS Test Application.

EGPRS TA

This command is not applicable to the EGPRS Test Application.

GSM/GPRS LA Sets the Type of Description for the BTS Position field. The type of description is either "Ellipsoid Point" or "Ellipsoid Point with Altitude".
The BTS Position field is optional. Use the CALL:PPRocedure:PMEasurement:MPRequest:RAData:BTSPosition command to have it included.
EGPRS LA

Setting

EPOint|EPALitude

EPOint: Ellipsoid Point
EPALitude: Ellipsoid Point with Altitude

Query

EPO|EPAL

*RST setting

EPO

Requirements

GSM/GPRS/ EGPRS LA

Revision: C.01 and above

Programming Example:

 
OUTPUT 714;"CALL:PPRocedure:PMEasurement:MPRequest:RAData:BTSPosition:TYPe EPAL"

CALL:PPRocedure:PMEasurement:MPRequest:REL98|RELEASE98

Function

GSM TA

This command is not applicable to the GSM Test Application.
GPRS TA

This command is not applicable to the GPRS Test Application.

EGPRS TA

This command is not applicable to the EGPRS Test Application.

GSM/GPRS LA Includes or excludes the optional Release 98 Extension element from the Measure Position Request component. You can set the value of these fields using the following commands: CALL:PPRocedure:PMEasurement:MPRequest:REL98|RELEASE98:BTS[<n>]:EOTDiff CALL:PPRocedure:PMEasurement:MPRequest:REL98|RELEASE98:BTS[<n>]:EOTDiff:UNCertainty
EGPRS LA

Setting

INCLude|EXCLude

Query

INCL|EXCL

*RST setting

EXCL

Requirements

GSM/GPRS/ EGPRS LA

Revision: C.01 and above

Programming Example:

 
OUTPUT 714;"CALL:PPRocedure:PMEasurement:MPRequest:REL98 INCL"

CALL:PPRocedure:PMEasurement:MPRequest:REL98|RELEASE98:BTS[<n>]:EOTDiff

Function

GSM TA

This command is not applicable to the GSM Test Application.
GPRS TA

This command is not applicable to the GPRS Test Application.

EGPRS TA

This command is not applicable to the EGPRS Test Application.

GSM/GPRS LA Sets the value of the Expected OTD field in the Release 98 Extension element. This field indicates the OTD value that the MS is expected to measure between the BTS indicated by the [<n>] mnemonic and the reference BTS.

The Release 98 Extension element is optional. Use the CALL:PPRocedure:PMEasurement:MPRequest:REL98|RELEASE98 command to have it included.
EGPRS LA

Setting

Range: 0 to 1250
Resolution: 1 bit

Query

Range: 0 to 1250
Resolution: 1 bit

*RST setting

0

Requirements

GSM/GPRS/ EGPRS LA

Revision: C.01 and above

Programming Example:

 
OUTPUT 714;"CALL:PPRocedure:PMEasurement:MPRequest:REL98:BTS2:EOTDiff 1010"

CALL:PPRocedure:PMEasurement:MPRequest:REL98|RELEASE98:BTS[<n>]:EOTDiff:UNCertainty

Function

GSM TA

This command is not applicable to the GSM Test Application.
GPRS TA

This command is not applicable to the GPRS Test Application.

EGPRS TA

This command is not applicable to the EGPRS Test Application.

GSM/GPRS LA Sets the value of the Uncertainty of Expected OTD field in the Release 98 Extension element. This field indicates the uncertainty in the Expected OTD value.

The Release 98 Extension element is optional. Use the CALL:PPRocedure:PMEasurement:MPRequest:REL98|RELEASE98 command to have it included.
EGPRS LA

Setting

Range: 0 to 7
Resolution: 1

Query

Range: 0 to 7
Resolution: 1

*RST setting

0

Requirements

GSM/GPRS/ EGPRS LA

Revision: C.01 and above

Programming Example:

 
OUTPUT 714;"CALL:PPRocedure:PMEasurement:MPRequest:REL98:BTS2:EOTDiff:UNCertainty 5"

CALL:PPRocedure:PMEasurement:MPRequest:SEND

Function

GSM TA

This command is not applicable to the GSM Test Application.
GPRS TA

This command is not applicable to the GPRS Test Application.

GSM/GPRS LA Sends the Measure Position Request component in an RRLP message.
EGPRS LA

Requirements

GSM/GPRS/ EGPRS LA

Revision: C.01 and above

Programming Example:

 
OUTPUT 714;"CALL:PPRocedure:PMEasurement:MPRequest:SEND"