Function
|
GSM TA
|
This command is not applicable to the GSM Test Application. |
GPRS TA |
This command is not applicable to the GPRS Test Application.
|
EGPRS TA |
This command is not applicable to the EGPRS Test Application.
|
GSM/GPRS LA |
Sets the value of the Protocol Error component. |
EGPRS LA |
Setting
|
Range: 0 to 5
Resolution: 1
0: Undefined
1: Missing Component
2: Incorrect Data
3: Missing Information Element or Component Element
4: Message Too Short
5: Unknown Reference Number |
Query
|
0 to 5 |
*RST setting
|
0 |
Requirements
|
GSM/GPRS/ EGPRS LA |
Revision: C.01 and above
|
Programming Example:
OUTPUT 714;"CALL:PPRocedure:PMEasurement:PERRor:CODE 3"
|