Last updated: January 18, 2010
This command is not applicable to the GSM Test Application. | ||
GPRS TA |
This command is not applicable to the GPRS Test Application. |
|
EGPRS TA |
This command is not applicable to the EGPRS Test Application. |
|
GSM/GPRS LA |
Queries the raw data from the last RRLP message received from a mobile station. The maximum length of the RRLP message is controlled by the RRLP Header State. See CALL:PPRocedure:PMEasurement:PIPE:HEADer[:STATe] . |
|
EGPRS LA | ||
"" | ||
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:PPRocedure:PMEasurement:PIPE:DATA:RX?" |
This command is not applicable to the GSM Test Application. | ||
GPRS TA |
This command is not applicable to the GPRS Test Application. |
|
EGPRS TA |
This command is not applicable to the EGPRS Test Application. |
|
GSM/GPRS LA | Query the received RRLP pipe message with it's associated GSM frame number. The resolution of both the transmit and receive times is one GSM frame period (4.615mS). This is an extension to the existing CALL:PPRocedure:PMEasurement:PIPE:DATA:RX? command which returns only the <string> with no frame number. See Time To First Fix (TTFF) response time | |
EGPRS LA | ||
" ", NAN | ||
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:PPRocedure:PMEasurement:PIPE:DATA:RX:TST?" |
This command is not applicable to the GSM Test Application. | ||
GPRS TA |
This command is not applicable to the GPRS Test Application. |
|
EGPRS TA |
This command is not applicable to the EGPRS Test Application. |
|
GSM/GPRS LA |
Sets or queries the string of data to be sent using the RRLP pipe. The data should be formatted as hexadecimal characters and can be up to 2000 characters long. The maximum length of the RRLP message is controlled by the RRLP Header State. See CALL:PPRocedure:PMEasurement:PIPE:HEADer[:STATe] |
|
EGPRS LA | ||
Range: 0 to 2000 ASCII formatted hexadecimal characters. | ||
"" | ||
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:PPRocedure:PMEasurement:PIPE:DATA:TX "00000000000000000000000000"" |
This command is not applicable to the GSM Test Application. | ||
GPRS TA |
This command is not applicable to the GPRS Test Application. |
|
EGPRS TA |
This command is not applicable to the EGPRS Test Application. |
|
GSM/GPRS LA | Sends the data setup using the CALL:PPRocedure:PMEasurement:PIPE:DATA:TX command to the mobile station using the RRLP pipe. This command also clears the results returned by the CALL:PPRocedure:PMEasurement:PIPE:DATA:RX:AVAilable? command. | |
EGPRS LA | ||
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:PPRocedure:PMEasurement:PIPE:SEND" |
This command is not applicable to the GSM Test Application. | ||
GPRS TA |
This command is not applicable to the GPRS Test Application. |
|
EGPRS TA |
This command is not applicable to the EGPRS Test Application. |
|
GSM/GPRS LA | This command sets/queries the Network Event at which the RRLP pipe data will be sent. Backwards compatibility is achieved by setting the default RRLP event type to `None'. See Event Based RRLP for more information | |
EGPRS LA | ||
NONe | ||
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:PPRocedure:PMEasurement:PIPE:SEND:EVENt ASS" |
This command is not applicable to the GSM Test Application. | ||
GPRS TA |
This command is not applicable to the GPRS Test Application. |
|
EGPRS TA |
This command is not applicable to the EGPRS Test Application. |
|
GSM/GPRS LA | This command sets/queries the maximum time to wait for the configured event type occur. See Event Based RRLP for more information | |
EGPRS LA | ||
300 | ||
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:PPRocedure:PMEasurement:PIPE:SEND:EVEN:TIM 10" |
This command is not applicable to the GSM Test Application. | ||
GPRS TA |
This command is not applicable to the GPRS Test Application. |
|
EGPRS TA |
This command is not applicable to the EGPRS Test Application. |
|
GSM/GPRS LA | Query the GSM frame number of the last transmitted RRLP pipe message. The resolution is 1 GSM frame (4.615ms). See Time To First Fix (TTFF) response time | |
EGPRS LA | ||
NAN | ||
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:PPRocedure:PMEasurement:PIPE:SEND:TST?" |
This command is not applicable to the GSM Test Application. | ||
GPRS TA |
This command is not applicable to the GPRS Test Application. |
|
EGPRS TA |
This command is not applicable to the EGPRS Test Application. |
|
GSM/GPRS LA | Clear the RRLP pipe message send frame number. Then the transmit timestamp is reset to NAN. See Time To First Fix (TTFF) response time | |
EGPRS LA | ||
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:PPRocedure:PMEasurement:PIPE:SEND:TST:CLE" |