Function
|
GSM TA
|
This command is not applicable to the GSM Test Application. |
GPRS TA |
This command is not applicable to the GPRS Test Application.
|
EGPRS TA |
This command is not applicable to the EGPRS Test Application.
|
GSM/GPRS LA |
Queries the status of the Measurement Position Response from the mobile station. This query returns a "0" when the a request message has been sent but an acknowledgment has not been received from the mobile station. A "1" is returned after an acknowledgment has been received and before another Measurement Position Request message is sent. |
EGPRS LA |
Query |
0 | 1
0: No results are available
1: Results are available
|
Requirements
|
GSM/GPRS/ EGPRS LA |
Revision: C.01 and above
|
Programming Example:
OUTPUT 714;"CALL:PPRocedure:PMEasurement:PRESponse:AVAilable?"
|