Last updated: December 3, 2008
This command is not applicable to the GSM Test Application. | ||
GPRS TA |
This command is not applicable to the GPRS Test Application. |
|
EGPRS TA |
This command is not applicable to the EGPRS Test Application. |
|
GSM/GPRS LA | Queries the Error Reason field of the optional Location Information Error element. If the Location Information Error element is not included, values for this field will not be available. See CALL:PPRocedure:PMEasurement:PRESponse:LIERror:INCLuded? to determine if the element is included. | |
EGPRS LA | ||
Query | ||
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:PPRocedure:PMEasurement:PRESponse:LINFormation:LIERror:REASon?" |