Last updated: December 3, 2008
This command is not applicable to the GSM Test Application. | ||
GPRS TA |
This command is not applicable to the GPRS Test Application. |
|
EGPRS TA |
This command is not applicable to the EGPRS Test Application. |
|
GSM/GPRS LA |
Queries the Reference BSIC field of the optional Reference BTS Identity element. If the Reference BTS Identity element is not included, values for this field will not be available. See
CALL:PPRocedure:PMEasurement:PRESponse:RIDentity:INCLuded?
to determine if the element is included. This query returns the BSIC for the three potential reference BTS that can be included in the Reference BTS Identity element. The values are returned the order BTS1, BTS2, BTS3. |
|
EGPRS LA | ||
Query | ||
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:PPRocedure:PMEasurement:PRESponse:RIDentity:BSICode?" |
This command is not applicable to the GSM Test Application. | ||
GPRS TA |
This command is not applicable to the GPRS Test Application. |
|
EGPRS TA |
This command is not applicable to the EGPRS Test Application. |
|
GSM/GPRS LA |
Queries the Reference BCCH Carrier field of the optional Reference BTS Identity element. If the Reference BTS Identity element is not included, values for this field will not be available. See
CALL:PPRocedure:PMEasurement:PRESponse:RIDentity:INCLuded?
to determine if the element is included. This query returns the BCCH Carrier for the three potential reference BTS that can be included in the Reference BTS Identity element. The values are returned the order BTS1, BTS2, BTS3. |
|
EGPRS LA | ||
Query | ||
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:PPRocedure:PMEasurement:PRESponse:RIDentity:CARRier?" |
This command is not applicable to the GSM Test Application. | ||
GPRS TA |
This command is not applicable to the GPRS Test Application. |
|
EGPRS TA |
This command is not applicable to the EGPRS Test Application. |
|
GSM/GPRS LA |
Queries the Reference CI field of the optional Reference BTS Identity element. If the Reference BTS Identity element is not included, values for this field will not be available. See
CALL:PPRocedure:PMEasurement:PRESponse:RIDentity:INCLuded?
to determine if the element is included. This query returns the CI for the three potential reference BTS that can be included in the Reference BTS Identity element. The values are returned the order BTS1, BTS2, BTS3. |
|
EGPRS LA | ||
Query | ||
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:PPRocedure:PMEasurement:PRESponse:RIDentity:CIDentity?" |
This command is not applicable to the GSM Test Application. | ||
GPRS TA |
This command is not applicable to the GPRS Test Application. |
|
EGPRS TA |
This command is not applicable to the EGPRS Test Application. |
|
GSM/GPRS LA |
Queries the Cell ID Type field of the optional Reference BTS Identity element. If the Reference BTS Identity element is not included, values for this field will not be available. See
CALL:PPRocedure:PMEasurement:PRESponse:RIDentity:INCLuded?
to determine if the element is included. This query returns the Cell ID Type for the three potential reference BTS that can be included in the Reference BTS Identity element. The values are returned the order BTS1, BTS2, BTS3. |
|
EGPRS LA | ||
Query | ||
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:PPRocedure:PMEasurement:PRESponse:RIDentity:CITYpe?" |
This command is not applicable to the GSM Test Application. | ||
GPRS TA |
This command is not applicable to the GPRS Test Application. |
|
EGPRS TA |
This command is not applicable to the EGPRS Test Application. |
|
GSM/GPRS LA | Queries to determine if the optional Reference BTS Identity element is included in the Measurement Position Response component from the MS. If this element is not included, none of the values in this element will be available. Therefore, CALL:PPRocedure:PMEasurement:PRESponse:RIDentity:CITYpe? , CALL:PPRocedure:PMEasurement:PRESponse:RIDentity:LACode? , CALL:PPRocedure:PMEasurement:PRESponse:RIDentity:CIDentity? , CALL:PPRocedure:PMEasurement:PRESponse:RIDentity:CARRier? , CALL:PPRocedure:PMEasurement:PRESponse:RIDentity:BSICode? , CALL:PPRocedure:PMEasurement:PRESponse:RIDentity:RINDex? and CALL:PPRocedure:PMEasurement:PRESponse:RIDentity:SIINdex? will all return NAN (Not a number). | |
EGPRS LA | ||
Query | ||
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:PPRocedure:PMEasurement:PRESponse:RIDentity:INCLuded?" |
This command is not applicable to the GSM Test Application. | ||
GPRS TA |
This command is not applicable to the GPRS Test Application. |
|
EGPRS TA |
This command is not applicable to the EGPRS Test Application. |
|
GSM/GPRS LA |
Queries the Reference LAC field of the optional Reference BTS Identity element. If the Reference BTS Identity element is not included, values for this field will not be available. See
CALL:PPRocedure:PMEasurement:PRESponse:RIDentity:INCLuded?
to determine if the element is included. This query returns the LAC for the three potential reference BTS that can be included in the Reference BTS Identity element. The values are returned the order BTS1, BTS2, BTS3. |
|
EGPRS LA | ||
Query | ||
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:PPRocedure:PMEasurement:PRESponse:RIDentity:LACode?" |
This command is not applicable to the GSM Test Application. | ||
GPRS TA |
This command is not applicable to the GPRS Test Application. |
|
EGPRS TA |
This command is not applicable to the EGPRS Test Application. |
|
GSM/GPRS LA |
Queries the Request Index field of the optional Reference BTS Identity element. If the Reference BTS Identity element is not included, values for this field will not be available. See
CALL:PPRocedure:PMEasurement:PRESponse:RIDentity:INCLuded?
to determine if the element is included. This query returns an index for each of the three potential reference BTS that can be included in the Reference BTS Identity element. The values are returned the order BTS1, BTS2, BTS3. |
|
EGPRS LA | ||
Query | ||
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:PPRocedure:PMEasurement:PRESponse:RIDentity:RINDex?" |
This command is not applicable to the GSM Test Application. | ||
GPRS TA |
This command is not applicable to the GPRS Test Application. |
|
EGPRS TA |
This command is not applicable to the EGPRS Test Application. |
|
GSM/GPRS LA |
Queries the System Info Index field of the optional Reference BTS Identity element. If the Reference BTS Identity element is not included, values for this field will not be available. See
CALL:PPRocedure:PMEasurement:PRESponse:RIDentity:INCLuded?
to determine if the element is included. This query returns an index for each of the three potential reference BTS that can be included in the Reference BTS Identity element. The values are returned the order BTS1, BTS2, BTS3. |
|
EGPRS LA | ||
Query | ||
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:PPRocedure:PMEasurement:PRESponse:RIDentity:SIINDex?" |