Last updated: December 3, 2008
Function |
This query returns the Repeated SACCH Frame Error Rate measurement results. The integrity indicator, number of samples counted, frame erasure ratio, and frame erasure count are returned. |
|
EGPRS LA | ||
GSM TA | ||
This command is not applicable to the GPRS Test Application. | ||
This command is not applicable to the EGPRS Test Application. | ||
|
||
Requirements | GSM/GPRS/ EGPRS LA |
Function |
This query returns the integrity indicator value for the last Repeated SACCH Frame Error Rate measurement performed. Zero indicates a normal result. See Integrity Indicator for descriptions of non-zero integrity indicators. |
|
EGPRS LA | ||
GSM TA | ||
This command is not applicable to the GPRS Test Application. | ||
This command is not applicable to the EGPRS Test Application. | ||
Range: See Integrity Indicator . |
||
Requirements | GSM/GPRS/ EGPRS LA |
Function | ||
EGPRS LA | ||
GSM TA | ||
This command is not applicable to the GPRS Test Application. | ||
This command is not applicable to the EGPRS Test Application. | ||
Requirements | GSM/GPRS/ EGPRS LA |