Function |
GSM/GPRS LA
|
This command sets/queries the number of samples to be taken by the Repeated SACCH Frame Erasure Error (FER) measurement. Each sample corresponds to a single SACCH block or a SACCH block and its requested repeat blocks.
|
EGPRS LA |
GSM TA |
This command is not applicable to the GSM Test Application.
|
GPRS TA
|
This command is not applicable to the GPRS Test Application. |
EGPRS TA
|
This command is not applicable to the EGPRS Test Application. |
Setting |
Range: 1 to 999999
Resolution: 1
|
Query
|
Range: 1 to 999999
Resolution: 1
|
*RST Setting |
1000
|
Requirements |
GSM/GPRS/ EGPRS LA |
Revision: F.00.37 and above
|
Programming Example
OUTPUT 714;"SETup:SFERate:SAMPles 55000"
! Sets the number of samples to measure to 55000.
|