CALL:MORiginated

CALL:MORiginated

Last updated: May 19, 2009

GPIB Command Conventions

CALL:MORiginated:ALERting:DURation

Function GSM TA

This command is not applicable to the GSM Test Applications.

GPRS TA

This command is not applicable to the GPRS Test Applications.

EGPRS TA

This command is not applicable to the EGPRS Test Applications.

GSM/GPRS LA

This command sets/queries the length of time that the test set holds a Mobile Originated voice call in the Alerting state before completing (or ending) the call connection. See Alerting Duration for more information.

EGPRS LA

Setting

Range: 0 to 600 (s)

Resolution: 1

Query

Range: 0|600

Resolution: 1

*RST Setting

0
Requirements GSM/GPRS/ EGPRS LA

Revision: G.00.00 and above

Programming Example

 
OUTPUT 714;"CALL:MORiginated:ALERting:DURation 0" 
! The incoming Mobile Originated voice call will be connected immediately.

CALL:MORiginated:CALL:RELease[:STATe]

Function GSM TA

This command is not applicable to the GSM Test Applications.

GPRS TA

This command is not applicable to the GPRS Test Applications.

EGPRS TA

This command is not applicable to the EGPRS Test Applications.

GSM/GPRS LA

This command sets/queries whether an incoming Mobile Originated voice call is connected or released. See Call Release State for more information.

EGPRS LA

Setting

Range: 1|ON|0|OFF

Query

Range: 0|1

*RST Setting

0|OFF
Requirements GSM/GPRS/ EGPRS LA

Revision: G.00.00 and above

Programming Example

 
OUTPUT 714;"CALL:MORiginated:CALL:RELease OFF" 
! The incoming Mobiel Originated voice call will be connected.