Last updated: December 3, 2008
Sets/queries the Network Color Code for the active (that is the selected) format. See Configuring the Broadcast Channel (BCH) . This can only be set when the Cell Operating Mode is set to Off (see CALL:OPERating:MODE ). |
||
EGPRS TA |
||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:CELL:NCCODE:SELECTED 2" |
Sets/queries the Network Color Code. See Configuring the Broadcast Channel (BCH) . This can only be set when the Cell Operating Mode is set to Off (see CALL:OPERating:MODE ). |
||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:CELL:NCCODE 2" |