CALL:PMNCode

CALL:PMNCode

Last updated: December 3, 2008

GPIB Command Conventions

CALL[:CELL]:PMNCode[:SVALue]

Function

GSM TA

This command sets/queries the 3 digit mobile network code. This command is used for the PCS band only. This command sets the PMNCode state to ON. This can only be set when the Call Operating Mode is set to Off (see CALL:OPERating:MODE ).

GPRS TA

EGPRS LA

GSM/GPRS LA

EGPRS LA

Setting

Range: 0 to 999

Resolution: 1

Query

Range: 0 to 999

Resolution: 1

*RST Setting

1

Requirements GSM/GPRS/
EGPRS TA

Revision: A.01 and above

GSM/GPRS/ EGPRS LA

Revision: C.01 and above

Programming Example

 
OUTPUT 714;"CALL:CELL:PMNCODE:SVALUE 798" 
! Sets the value to 798 and the state to ON. Only used for PCS 1900 band. 

CALL[:CELL]:PMNCode:VALue

Function

GSM TA

This command sets/queries the 3 digit mobile network code value. This command is used for PCS band only.

GPRS TA

EGPRS LA

GSM/GPRS LA

EGPRS LA

Setting

Range: 0 to 999

Resolution: 1

Query

Range: 0 to 999

Resolution: 1

*RST Setting

1

Requirements GSM/GPRS/
EGPRS TA

Revision: A.01 and above

GSM/GPRS/ EGPRS LA

Revision: C.01 and above

Programming Example

 
OUTPUT 714;"CALL:CELL:PMNCODE:VALUE 798" 
! Sets the 3 digit MNCode for PCS 1900 to 798.

CALL[:CELL]:PMNCode:STATe

Function

GSM TA

This command sets/queries the MNC state in the active (that is the selected) format. This command is used for the PCS band only. Setting it to ON configures the BCCH to use the 3 digit MNC. Note, this command can only be used when the Cell Operating Mode is OFF.

If the test set is in active cell operating mode, this command cannot be set unless the Call Operating Mode is OFF.

GPRS TA

EGPRS LA

GSM/GPRS LA

EGPRS LA

Setting

Range: 0 | OFF | 1 | ON

Query

Range: 0 | 1

*RST Setting

0 | OFF
Requirements GSM/GPRS/
EGPRS TA

Revision: A.01 and above

GSM/GPRS/ EGPRS LA

Revision: C.01 and above

Programming Example

 
OUTPUT 714;"CALL:CELL:PMNCode:STATe ON" 
! Enables the 3 digit MNCode for PCS 1900.