Last updated: November 25, 2010
This command is not applicable to the GSM Test Application. | ||
This command is not applicable to the GPRS Test Application. | ||
This command is not applicable to the EGPRS Test Application. | ||
This command sets/queries the deferred DTM (Dual Transfer Mode) traffic channel for the band selected. The optional [SELected] keyword in this command specifies that the channel being set/queried applies to the current DTM band. See DTM Traffic Channel for more information. |
||
Setting |
|
|
Query |
|
|
*RST setting |
PGSM, EGSM and RGSM bands: 30, DCS and PCS bands: 698, GSM450: 280, GSM480: 320, GSM750: 460, GSM850: 160, TGSM810: 400. |
|
Requirements | GSM/GPRS/ EGPRS LA | |
OUTPUT 714;"CALL:SETup:DTMode:ARFCn 512" ! Sets the deferred DTM ARFCN of the selected band to 512, if 512 is valid for the selected band. |
This command is not applicable to the GSM Test Application. | ||
This command is not applicable to the GPRS Test Application. | ||
This command is not applicable to the EGPRS Test Application. | ||
This command sets/queries the deferred DTM band, therefore constraining the range of DTM ARFCNs. See DTM Traffic Band for more information. |
||
Setting | Range: PGSM | EGSM | GSM450 | GSM480 | GSM750 | GSM850 | DCS | PCS | RGSM| TGSM810 | |
Query | Range: PGSM | EGSM | GSM450 | GSM480 | GSM750 | GSM850 | DCS | PCS | RGSM| TGSM810 | |
*RST setting | PGSM | |
Requirements | GSM/GPRS/ EGPRS LA | |
OUTPUT 714;"CALL:SETup:DTMode:BAND DCS" ! Sets the deferred DTM band to DCS. |
This command is not applicable to the GSM Test Application. | ||
This command is not applicable to the GPRS Test Application. | ||
This command is not applicable to the EGPRS Test Application. | ||
This command sets/queries the deferred DTM coding scheme for both GPRS uplink and downlink. See DTM Coding Schemes for more information. |
||
Setting | Range: CS1 | CS2 | CS3 | CS4 | |
Query | Range: CS1 | CS2 | CS3 | CS4 | |
*RST setting | CS4 | |
Requirements | GSM/GPRS/ EGPRS LA | |
OUTPUT 714;"CALL:SETup:DTMode:CSCHeme CS1" ! Sets the deferred DTM coding scheme to CS1. |
This command is not applicable to the GSM Test Application. | ||
This command is not applicable to the GPRS Test Application. | ||
This command is not applicable to the EGPRS Test Application. | ||
This command is not applicable to the EGPRS Lab Application. | ||
GSM/GPRS LA |
This command sets/queries the deferred DTM coding scheme for GPRS downlink. When ETSI B connection is used, the coding scheme on the downlink must be the same as the uplink. See DTM Coding Schemes for more information. |
|
Setting | Range: CS1 | CS2 | CS3 | CS4 | |
Query | Range: CS1 | CS2 | CS3 | CS4 | |
*RST setting | CS4 | |
Requirements | GSM/GPRS LA | |
OUTPUT 714;"CALL:SETup:DTMode:CSCHeme:DOWNlink CS1" ! Sets the deferred downlink DTM coding scheme to CS1. |
This command is not applicable to the GSM Test Application. | ||
This command is not applicable to the GPRS Test Application. | ||
This command is not applicable to the EGPRS Test Application. | ||
This command is not applicable to the EGPRS Lab Application. | ||
GSM/GPRS LA |
This command sets/queries the deferred DTM coding scheme for GPRS uplink. See DTM Coding Schemes for more information. |
|
Setting | Range: CS1 | CS2 | CS3 | CS4 | |
Query | Range: CS1 | CS2 | CS3 | CS4 | |
*RST setting | CS4 | |
Requirements | GSM/GPRS LA | |
OUTPUT 714;"CALL:SETup:DTMode:CSCHeme:UPLink CS1" ! Sets the deferred uplink DTM coding scheme to CS1. |
This command is not applicable to the GSM Test Application. | ||
This command is not applicable to the GPRS Test Application. | ||
This command is not applicable to the EGPRS Test Application. | ||
This command sets/queries the deferred DTM Circuit Switched Half Rate Sub-channel. See DTM CS Half Rate Sub Channel for more information. |
||
Setting | Range: 0 | 1 | |
Query | Range: 0 | 1 | |
*RST setting | 0 | |
Requirements | GSM/GPRS/ EGPRS LA | |
OUTPUT 714;"CALL:SETup:DTMode:CSWitched:HRSPeech:SCHannel 1" ! Sets the deferred DTM CS Half Rate Sub-channel to ON. |
This command is not applicable to the GSM Test Application. | ||
This command is not applicable to the GPRS Test Application. | ||
This command is not applicable to the EGPRS Test Application. | ||
This command sets/queries the deferred DTM circuit switched timeslot position within the selected multislot configuration. See DTM CS Timeslot Position for more information. |
||
Setting | ||
Query | ||
*RST setting | Depends on the currently selected multislot configuration. See DTM CS Timeslot Position | |
Requirements | GSM/GPRS/ EGPRS LA | |
OUTPUT 714;"CALL:SETup:DTMode:CSWitched:TSLot 3" ! Sets the deferred circuit switched timeslot position to 3. |
This command is not applicable to the GSM Test Application. | ||
This command is not applicable to the GPRS Test Application. | ||
This command is not applicable to the EGPRS Test Application. | ||
This command enables/queries the deferred DTM Frequency Hopping state for GPRS or EGPRS. See DTM Frequency Hopping for more information. |
||
Setting | Range: 0 | OFF | 1 | ON | |
Query | Range: 0 | 1 | |
*RST setting | 0 |OFF | |
Requirements | GSM/GPRS/ EGPRS LA | |
OUTPUT 714;"CALL:SETup:DTMode:FHOPping ON" ! Enables deferred DTM Frequency Hopping. |
This command is not applicable to the GSM Test Application. | ||
GPRS TA |
This command is not applicable to the GPRS Test Application. |
|
EGPRS TA |
This command is not applicable to the EGPRS Test Application. |
|
GSM/GPRS LA | This command sets/queries the deferred DTM gamma value for any uplink burst in the selected band. The range of gamma 0 to 31 represents 0 to 62 dB in 2 dB steps. See MS Output Power for more information. | |
EGPRS LA | ||
13 | ||
Requirements | GSM/GPRS/ EGPRS LA | |
OUTPUT 714;CALL:SETup:DTMode:MS:GAMMa:BURSt2 7 ! Sets the deferred DTM gamma parameter of the 2rd uplink burst in the selected band to 7. |
This command is not applicable to the GSM Test Application. | ||
This command is not applicable to the GPRS Test Application. | ||
This command is not applicable to the EGPRS Test Application. | ||
This command sets/queries the deferred DTM packet switched MS transmit power level for any burst in the selected band. Burst one is assumed if no burst is specified. The optional [SELected] keyword in this command specifies that the channel being set/queried applies to the current DTM band. See DTM MS Tx Levels for more information. |
||
PGSM, EGSM, RGSM, GSM450, GSM480, GSM750, GSM850, and TGSM810 bands: 15, |
||
Requirements | GSM/GPRS/ EGPRS LA | |
OUTPUT 714;"CALL:SETup:DTMode:MS:TXLevel:BURSt 10" ! Sets the deferred DTM MS Transmit power level of burst one in the selected band to 10. |
This command is not applicable to the GSM Test Application. | ||
This command is not applicable to the GPRS Test Application. | ||
This command is not applicable to the EGPRS Test Application. | ||
This command sets/queries the deferred DTM multislot configuration. See DTM Multislot Configuration for more information. The actual timeslots used in each configuration are fixed as in the list below. Multislot Configuration Downlink Timeslots Used Uplink Timeslots Used
D1U1 3 3 |
||
Range: D1U1 |D1U2 |D1U3 |D1U4 |D1U5 |D1U6 |D2U1 | D2U2 |D2U3 |D2U4 |D2U5 |D3U1 | D3U2 |D3U3 |D3U4 |D4U1 |D4U2 |D4U3 |D5U1 |D5U2 |D6U1 | ||
Range: D1U1 |D1U2 |D1U3 |D1U4 |D1U5 |D1U6 |D2U1 | D2U2 |D2U3 |D2U4 |D2U5 |D3U1 | D3U2 |D3U3 |D3U4 |D4U1 |D4U2 |D4U3 |D5U1 |D5U2 |D6U1 | ||
D2U2 | ||
Requirements | GSM/GPRS/ EGPRS LA | |
OUTPUT 714;"CALL:SETup:DTMode:MSLot:CONFig D2U2" ! Sets the deferred DTM multislot configuration to be 2 downlink and 2 uplink timeslots. |
This command is not applicable to the GSM Test Application. | ||
This command is not applicable to the GPRS Test Application. | ||
This command is not applicable to the EGPRS Test Application. | ||
This command sets/queries the customized DTM multislot configuration. See Flexible Timeslot for more information. The command form accepts two string parameters with each contains a maximum of 8 characters. The first string represents the timeslot usage of TS0 to TS7 of the downlink timeslots and the second string represents the timeslot usage of TS0 to TS7 of the uplink timslots. Each timeslot of the uplink and downlink can be configured to one of the three values:
If less than 8 characters in each string are specified in a parameter, the remaining higher numbered timeslots are assumed to be OFF. See DTM Multislot Configuration for more information. |
||
Range: -, ,x,X,0 |p,P,1 |t,T | ||
Range: - |P |T | ||
--PT----,--PT---- | ||
Requirements | GSM/GPRS/ EGPRS LA | |
OUTPUT 714;"CALL:SETup:DTMode:MSLot:CONFig:CUSTom:TSLots --PT----, --PT----" ! Sets the DTM custom multislot configuration to be 2 downlink and 2 uplink timeslots. Timeslot 2 are ! configured as PDCH and Timeslot 3 are configured as TCH in both uplink and downlink. |
This command is not applicable to the GSM Test Application. | ||
This command is not applicable to the GPRS Test Application. | ||
This command is not applicable to the EGPRS Test Application. | ||
This command sets/queries the deferred DTM power reduction reference level. (ETSI refers to this as P0) See DTM Power Reduction Reference for more information. |
||
EGPRS LA | ||
Setting |
Range: 0 to 30 dB Resolution: 2 dB |
|
Query |
Range: 0 to 30 dB Resolution: 2 dB |
|
*RST setting | 0 dB | |
Requirements | GSM/GPRS/ EGPRS LA | |
OUTPUT 714;"CALL:SETup:DTMode:PZERo:LEVel 30" ! Sets the deferred DTM power reduction reference level (p0) to 30 dB. |
This command is not applicable to the GSM Test Application. | ||
This command is not applicable to the GPRS Test Application. | ||
GSM/GPRS LA | This command is not applicable to the GSM/GPRS Lab Application. | |
EGPRS TA | This command is not applicable to the EGPRS Test Application. | |
Sets/Queries the deferred TTI mode that the TBFs will be operated in the DTM operation. See TTI Mode Configuration | ||
Setting | ||
Query | BTTI | RTTI | |
*RST setting | BTTI | |
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:SETup:DTMode:TTI:MODE BTTI" ! Sets the deferred TTI mode to BTTI in the DTM operation. |
This command is not applicable to the GSM Test Application. | ||
GPRS TA | This command is not applicable to the GPRS Test Application. | |
This command is not applicable to the EGPRS Test Application. | ||
This command sets/queries the deferred DTM uplink state flag (USF). The USF allows multiple mobile stations to share over-the-air resources. See DTM Uplink State Flag for more information. |
||
0 | ||
Requirements | GSM/GPRS/ EGPRS LA | |
OUTPUT 714;"CALL:SETup:DTMode:USFLag 2" ! Sets the deferred DTM USF to 2. |
This command is not applicable to GSM. | ||
This command sets/queries the deferred PDTCH ARFCN for the band specified using the command CALL:SETup:(PDTCH|PDTChannel):BAND . Deferred parameters are applied when a channel change is executed using the CALL:HANDover command (see CALL:HANDover|HANDoff[:IMMediate] ). The ARFCN range varies with the selected PDTCH band. The correspondence between ARFCN and frequency differs for each band and that a single ARFCN specifies a separate frequency for uplink and downlink. The PDTCH ARFCN selects the ARFCN for all the PDTCHs which you can configure. The PDTCH ARFCN is a frequency banded parameter. Refer to Frequency Banded Parameters for a detailed description of the implications of being a banded parameter. |
||
Setting |
|
|
Query |
|
|
*RST setting |
PGSM, EGSM and RGSM bands: 30, DCS and PCS bands: 698, GSM450 band: 280, GSM480 band: 320, GSM750 band: 460, GSM850 band: 160, TGSM810 band: 400 |
|
GSM/GPRS/ EGPRS TA |
||
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:SETup:PDTCh 515" ! Sets the ARFCN to 515 if it is appropriate in the current band. |
This command is not applicable to GSM. | ||
This command sets/queries the deferred GSM band. Deferred parameters are applied when a channel change is executed using the CALL:HANDover command (see CALL:HANDover|HANDoff[:IMMediate] ). |
||
Setting |
Range: DCS | EGSM | GSM450 | GSM480 | GSM750 | GSM850 |PCS |PGSM |RGSM | TGSM810 |
|
Query |
Range: DCS | EGSM | GSM450 | GSM480 | GSM750 | GSM850 |PCS |PGSM |RGSM| TGSM810 |
|
*RST setting | PGSM | |
GSM/GPRS/ EGPRS TA |
||
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:SETup:PDTCH:BAND DCS" ! Sets the deferred band to DCS |
This command is not applicable to GSM TA. | ||
This command sets/queries the deferred PDTCH coding scheme for both GPRS uplink and downlink. Deferred parameters are applied when a channel change is executed using the CALL:HANDover command (see CALL:HANDover|HANDoff[:IMMediate] ). When a Coding Scheme change is executed, all measurements and BLER reports are stopped before the change is made, and re-started after the change has taken effect. |
||
Setting | Range: CS1 | CS2| CS3 | CS4 | |
Query | Range: CS1 | CS2 | CS3 | CS4 | |
*RST setting | CS4 | |
GSM/GPRS/ EGPRS TA |
||
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:SETup:PDTCH:CSCHeme CS4" ! Sets the PDTCH deferred coding scheme to CS4 |
This command is not applicable to GSM/GPRS Test Application. | ||
This command sets/queries the deferred downlink PDTCH coding scheme. Deferred parameters are applied when a channel change is executed using the CALL:HANDover command (see CALL:HANDover|HANDoff[:IMMediate] ). When a Coding Scheme change is executed, all measurements and BLER reports are stopped before the change is made, and re-started after the change has taken effect. When ETSI B connection is used, the coding scheme on the downlink must be the same as the uplink. |
||
Setting | Range: CS1 | CS2| CS3 | CS4 | |
Query | Range: CS1 | CS2 | CS3 | CS4 | |
*RST setting | CS4 | |
GSM/GPRS LA | ||
OUTPUT 714;"CALL:SETup:PDTCH:CSCHeme:DOWNlink CS4" ! Sets the downlink PDTCH deferred coding scheme to CS4 |
This command is not applicable to GSM/GPRS Test Application. | ||
This command sets/queries the deferred uplink PDTCH coding scheme. Deferred parameters are applied when a channel change is executed using the CALL:HANDover command (see CALL:HANDover|HANDoff[:IMMediate] ). When a Coding Scheme change is executed, all measurements and BLER reports are stopped before the change is made, and re-started after the change has taken effect. |
||
Setting | Range: CS1 | CS2| CS3 | CS4 | |
Query | Range: CS1 | CS2 | CS3 | CS4 | |
*RST setting | CS4 | |
GSM/GPRS LA | ||
OUTPUT 714;"CALL:SETup:PDTCH:CSCHeme:UPLink CS4" ! Sets the uplink PDTCH deferred coding scheme to CS4 |
This command is not applicable to the GSM Test Application. | ||
GPRS TA | This command is not applicable to the GPRS Test Application. | |
This command is not applicable to the EGPRS Test Application. | ||
This command is not applicable to the GSM/GPRS Lab Application. | ||
This command sets/queries the deferred downlink EGPRS Level of a TBF in Dual Transfer Mode. EGPRS level is used to group certain subsets of Modulation Coding Scheme choices. The different EGPRS Level available are EGPRS and EGPRS-2A. See Downlink EGPRS Level for more information. |
||
EGPRS | ||
Requirements | GSM/GPRS/ EGPRS LA | |
OUTPUT 714;"CALL:SETup:PDTCH:DTMode:EGPRS:LEVel:DOWNlink EGPRS2A" ! Sets the deferred downlink EGPRS level to EGPRS-2A in Dual Transfer Mode. |
This command is not applicable to the GSM Test Application. | ||
GPRS TA | This command is not applicable to the GPRS Test Application. | |
This command is not applicable to the EGPRS Test Application. | ||
This command is not applicable to the GSM/GPRS Lab Application. | ||
This command sets/queries the deferred uplink EGPRS Level of a TBF in Dual Transfer Mode. EGPRS level is used to group certain subsets of Modulation Coding Scheme choices. The different EGPRS Level available are EGPRS and EGPRS-2A. See Uplink EGPRS Level for more information. |
||
EGPRS | ||
Requirements | GSM/GPRS/ EGPRS LA | |
OUTPUT 714;"CALL:SETup:PDTCH:DTMode:EGPRS:LEVel:UPLink EGPRS2A" ! Sets the deferred uplink EGPRS level to EGPRS-2A in Dual Transfer Mode. |
This command is not applicable to the GSM Test Application. | ||
GPRS TA | This command is not applicable to the GPRS Test Application. | |
This command is not applicable to the EGPRS Test Application. | ||
This command is not applicable to the GSM/GPRS Lab Application. | ||
This command sets/queries the deferred downlink EGPRS Level of a TBF. EGPRS level is used to group certain subsets of Modulation Coding Scheme choices. The different EGPRS Level available are EGPRS and EGPRS-2A. See Downlink EGPRS Level for more information. |
||
EGPRS | ||
Requirements | GSM/GPRS/ EGPRS TA | |
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:SETup:PDTCH:EGPRS:LEVel:DOWNlink EGPRS2A" ! Sets the deferred downlink EGPRS level to EGPRS-2A. |
This command is not applicable to the GSM Test Application. | ||
GPRS TA | This command is not applicable to the GPRS Test Application. | |
This command is not applicable to the GSM/GPRS Lab Application. | ||
This command sets/queries the deferred uplink EGPRS Level of a TBF. EGPRS level is used to group certain subsets of Modulation Coding Scheme choices. The different EGPRS Level available are EGPRS and EGPRS-2A. See Uplink EGPRS Level for more information. |
||
EGPRS | ||
Requirements | GSM/GPRS/ EGPRS TA | |
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:SETup:PDTCH:EGPRS:LEVel:UPLink EGPRS2A" ! Sets the deferred uplink EGPRS level to EGPRS-2A. |
This command is not applicable to the GSM Test Application. | ||
GPRS TA |
This command is not applicable to the GPRS Test Application. |
|
GSM/GPRS LA | This command is not applicable to the GSM/GPRS Lab Application. | |
EGPRS TA | This command sets/queries the deferred FANR state for PS connections. See Fast Ack/Nack Reporting for more information. | |
EGPRS LA | ||
Range: 0 | OFF | 1 | ON |
||
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:SETup:PDTCH:FANReporting ON" ! Turns the deferred FANR On. OUTPUT 714;"CALL:SETup:PDTCH:FANReporting?" ! Returns "On" if the deferred FANR has been turn on. |
This command is not applicable to the GSM Test Application. | ||
GPRS TA |
This command is not applicable to the GPRS Test Application. |
|
GSM/GPRS LA | This command is not applicable to the GSM/GPRS Lab Application. | |
EGPRS TA | This command sets/queries the deferred Event-based FANR state for PS connections. See Fast Ack/Nack Reporting for more information. | |
EGPRS LA | ||
Range: 0 | OFF | 1 | ON |
||
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:SETup:PDTCH:FANReporting:EVENt ON" ! Turns the deferred Event-based FANR On. OUTPUT 714;"CALL:SETup:PDTCH:FANReporting:EVENt?" ! Returns "On" if the deferred Event-based FANR has been turn on. |
This command is not applicable to the GSM TA. | ||
This command is not applicable to the GPRS TA. | ||
This command is not applicable to the GSM/GPRS LA. | ||
This command sets/queries the deferred modulation coding scheme used for transmission on the downlink and uplink in Active Cell operating mode. Deferred parameters are applied when a channel change is executed using the CALL:HANDover command (see CALL:HANDover|HANDoff[:IMMediate] ). |
||
Setting | ||
Query | ||
*RST setting | MCS4,MCS4 | |
GSM/GPRS/ EGPRS TA |
Revision: A.12 with a required feature license adds DAS5 to DAS12 Revision: A.13 with a required feature license adds UAS7 to UAS11 |
|
Revision: H.00.00 and above adds DAS5 to DAS12 Revision: H.01 with a required feature license adds UAS7 to UAS11 |
||
OUTPUT 714;"CALL:SETup:PDTCH:MCSCheme MCS2, MCS2" ! Sets the PDTCH deferred modulation coding scheme for the downlink and uplink to MCS2. |
This command is not applicable to the GSM Test Application. | ||
GPRS TA |
This command is not applicable to the GPRS Test Application. |
|
EGPRS TA |
This command is not applicable to the EGPRS Test Application. |
|
GSM/GPRS LA | This command sets/queries the deferred gamma value for any uplink burst in the selected band. The range of gamma 0 to 31 represents 0 to 62 dB in 2 dB steps. See MS Output Power for more information. | |
EGPRS LA | ||
13 | ||
GSM/GPRS/ EGPRS TA | Revision: A.12 and above | |
GSM/GPRS/ EGPRS LA | Revision: F.00.37 and above | |
OUTPUT 714;CALL:SETup:PDTCH:MS:GAMMa:BURSt3 11 ! Sets the deferred gamma parameter of the 3rd uplink burst in the selected band to 11. |
This command is not applicable to GSM. | ||
This command sets/queries the deferred mobile station transmit power level for the deferred PDTCH band. The transmit power is set individually for each uplink burst. Depending on the "Multislot Configuration" setting, there is one to four uplink bursts (burst 1, burst 2, burst 3, burst 4) - burst 1 is in the first uplink slot specified, not timeslot 1, burst 2 is in the second slot specified, not timeslot 2, etc. Deferred parameters are applied when a channel change is executed using the CALL:HANDover command (see CALL:HANDover|HANDoff[:IMMediate] ). The immediate setting for the mobile station transmit power level for a PDTCH band is CALL:(PDTCH|PDTChannel):MS:TXLevel[:SELected]:BURSt<[1]|2|3|4|5> . The mobile station transmit power level is a frequency banded parameter. Refer to Frequency Banded Parameters for a detailed description of the implications of being a banded parameter. The mobile station transmit power level is a bursted parameter. Refer to Bursted Parameters for a detailed description of being a bursted parameter. |
||
EGPRS LA | ||
Setting | ||
Query | ||
*RST setting |
PGSM, EGSM RGSM, GSM450, GSM480, GSM750, GSM850, TGSM810 bands:15, |
|
GSM/GPRS/ EGPRS TA |
Revision A.04 adds Burst 3 and Burst 4. |
|
GSM/GPRS/ EGPRS LA |
Revision D.01 adds Burst 3 and Burst 4. |
|
OUTPUT 714;"CALL:SETup:PDTCH:MS:TXLevel:BURSt2 13" ! Sets the deferred mobile station TX level for the 2nd uplink burst in the currently selected band. |
This command sets/queries the deferred number of downlink and uplink PDTCHs. These deferred PDTCHs are only applied when the Execute Channel Change action is initiated using CALL:HANDover|HANDoff[:IMMediate] . The effect this command has on the number of uplink and downlink timeslots depends on the Data Connection Type:
The actual timeslots used in each configuration are fixed as follows: Multislot Configuration Downlink Timeslots Used Uplink Timeslots Used
D1U1 3 3 When the Multislot Configuration is set to D1U1, D2U1, D3U1, D4U1 or D5U1 the measurement burst is set to 1. When a multislot configuration change is executed, all measurements are stopped before the change is made, and restarted after the change has taken effect.
|
|||
Range: D1U1 |D1U2 |D1U3 |D1U4 |D1U5 |D1U6 |D2U1 | D2U2 |D2U3 |D2U4 |D2U5 |D3U1 | D3U2 |D3U3 |D3U4 |D4U1 |D4U2 |D4U3 |D5U1 |D5U2 |D6U1 "D<n>U<m>" corresponds to "Downlink<n>Uplink<m>", where <n> indicates the number of downlink timeslots and <m> represents the number of uplink timeslots. |
|||
Range: D1U1 |D1U2 |D1U3 |D1U4 |D1U5 |D1U6 |D2U1 | D2U2 |D2U3 |D2U4 |D2U5 |D3U1 | D3U2 |D3U3 |D3U4 |D4U1 |D4U2 |D4U3 |D5U1 |D5U2 |D6U1 | |||
D2U1 | |||
GPRS/EGPRS TA |
Revision A.04 adds D1U2, D1U3, D1U4, and D2U3 |
||
GSM/GPRS/ EGPRS LA |
Revision D01 adds D1U2, D1U3, D1U4, and D2U3 |
||
OUTPUT 714;"CALL:SETup:PDTCH:MSLot:CONFig D2U2" ! Sets the number of downlink timeslots to 2 and uplink timeslots to 2. |
This command is not applicable to the GSM Test Application. | ||
This command is not applicable to the GPRS Test Application. | ||
This command is not applicable to the EGPRS Test Application. | ||
This command sets/queries the customized DTM multislot configuration. See Flexible Timeslot for more information. The command form accepts two string parameters with each contains a maximum of 8 characters. The first string represents the timeslot usage of TS0 to TS7 of the downlink timeslots and the second string represents the timeslot usage of TS0 to TS7 of the uplink timeslots. Each timeslot of the uplink and downlink can be configured to one of the three values:
If less than 8 characters in each string are specified in a parameter, the remaining higher numbered timeslots are assumed to be OFF. See DTM Multislot Configuration for more information. |
||
Range: -, ,x,X,0 |p,P,1 |t,T | ||
Range: - |P |T | ||
--PT----,--PT---- | ||
Requirements | GSM/GPRS/ EGPRS LA | |
OUTPUT 714;"CALL:SETup:PDTCH:MSLot:CONFig:CUSTom:TSLots --PT----, --PT----" ! Sets the DTM custom multislot configuration to be 2 downlink and 2 uplink timeslots. Timeslot 2 are ! configured as PDCH and Timeslot 3 are configured as TCH in both uplink and downlink. |
This command is not applicable to GSM. | ||
This command sets/queries the deferred Power Reduction reference level to be used for connections. Deferred parameters are applied when the Execute Channel Change action is initiated using CALL:HANDover|HANDoff[:IMMediate] . When Data Connection Type "ETSI Type A" is used, there is no downlink PDTCH and therefore changing this parameter has no effect other than remembering the new value until the Data Connection Type "ETSI Type B" or "BLER" is used. |
||
GSM/GPRS LA | ||
EGPRS LA | ||
Setting |
Range: 0 to 30 dB Resolution: 2 dB |
|
Query |
Range: 0 to 30 dB Resolution: 2 dB |
|
*RST setting | 0 dB | |
GSM/GPRS/ EGPRS TA |
||
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:SETup:PDTCH:PZERo:LEVel 15 dB" ! Sets the deferred Power Reduction reference level to 15 dB. |
This command is not applicable to the GSM Test Application. | ||
This command is not applicable to the GPRS Test Application. | ||
GSM/GPRS LA | This command is not applicable to the GSM/GPRS Lab Application. | |
EGPRS TA | Sets/Queries the deferred TTI mode that the TBFs will be operated. See TTI Mode Configuration | |
Setting | ||
Query | BTTI | RTTI | |
*RST setting | BTTI | |
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:SETup:PDTCH:TTI:MODE BTTI" ! Sets the deferred TTI mode to BTTI. |
This command is not applicable to the GSM Test Application. | ||
This command is not applicable to the GPRS Test Application. | ||
This command is not applicable to the EGPRS Test Application | ||
This command is not applicable to the GSM/GPRS Lab Application. | ||
This command sets/quires the deferred burst state with respect to configuration of different USF to be assigned and allocated to the mobile for each PDCH or PDCH-pair depending on whether the USF Mode is BTTI or RTTI respectively. See USF by Burst . | ||
Setting | ||
Query | Range: 0 | OFF | 1 | ON | |
*RST setting | 1 | ON | |
Requirements | GSM/GPRS/ EGPRS LA | |
OUTPUT 714;"CALL:SETup:PDTCH:USFlag:BURSt1:STATe ON" ! Sets the deferred burst 1 state in terms of USF by burst to ON. |
This command is not applicable to the GSM Test Application. | ||
This command is not applicable to the GPRS Test Application. | ||
This command is not applicable to the EGPRS Test Application | ||
This command is not applicable to the GSM/GPRS Lab Application. | ||
This command sets/quires the deferred USF value with respect to configuration of different USF to be assigned and allocated to the mobile for each PDCH or PDCH-pair depending on whether the USF Mode is BTTI or RTTI respectively. See USF by Burst . | ||
Setting | ||
Query | Range: 0 to 7 | |
*RST setting | 0 | |
Requirements | GSM/GPRS/ EGPRS LA | |
OUTPUT 714;"CALL:SETup:PDTCH:USFlag:BURSt1:VALue 1" ! Sets the deferred burst 1 USF vaule to 1. |
This command is not applicable to the GSM Test Application. | ||
This command is not applicable to the GPRS Test Application. | ||
This command is not applicable to the EGPRS Test Application | ||
This command is not applicable to the GSM/GPRS Lab Application. | ||
This command sets/quires the deferred burst state&value with respect to configuration of different USF to be assigned and allocated to the mobile for each PDCH or PDCH-pair depending on whether the USF Mode is BTTI or RTTI respectively. See USF by Burst . | ||
Setting | ||
Query | Range: 0 to 7 | |
*RST setting | 0 | |
Requirements | GSM/GPRS/ EGPRS LA | |
OUTPUT 714;"CALL:SETup:PDTCH:USFlag:BURSt 2 " ! Sets the deferred burst 1 value to 2 and state to ON. |
This command is not applicable to GSM TA. | ||
This command is not applicable to GPRS TA. | ||
This command is not applicable to GSM/GPRS LA. | ||
EGPRS TA |
This command sets/queries the deferred PDTCH2 ARFCN for the band specified using the command CALL:SETup:(PDTCH|PDTChannel):BAND . Deferred parameters are applied when a channel change is executed using the CALL:HANDover command (see CALL:HANDover|HANDoff[:IMMediate] ). The ARFCN range varies with the selected PDTCH2 band. The correspondence between ARFCN and frequency differs for each band and that a single ARFCN2 specifies a separate frequency for uplink and downlink. The PDTCH2 ARFCN and PDTCH1 ARFCN can NOT be the same, refer to Constrains on PDTCH Configuration for a detailed description. The PDTCH2 ARFCN is a frequency banded parameter. Refer to Frequency Banded Parameters for a detailed description of the implications of being a banded parameter. |
|
Setting |
|
|
Query |
|
|
*RST setting |
PGSM, EGSM and RGSM bands: 20, DCS and PCS bands: 512, GSM450 band: 270, GSM480 band: 310, GSM750 band: 450, GSM850 band: 150, TGSM810 band: 380 |
|
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:SETup:PDTC2:ARFCN 515" ! Sets the ARFCN to 515 if it is appropriate in the current band. |
This command is not applicable to the GSM Test Application. | |||
This command is not applicable to the GPRS Test Application. |
|||
This command is not applicable to the GSM/ GPRS Lab Application. |
|||
EGPRS TA |
This command is not applicable to the EGPRS Test Application. |
||
This command sets/queries the deferred number of downlink and uplink PDTCH2s. These deferred PDTCH2s are only applied when the Execute Channel Change action is initiated using CALL:HANDover|HANDoff[:IMMediate] . The effect this command has on the number of uplink and downlink timeslots depends on the Data Connection Type:
The actual timeslots used in each configuration are fixed as follows: Multislot Configuration Downlink Timeslots Used Uplink Timeslots Used
D1U1 3 3 When the Multislot Configuration is set to D1U1, D2U1, D3U1, D4U1 or D5U1 the measurement burst is set to 1. When a multislot configuration change is executed, all measurements are stopped before the change is made, and restarted after the change has taken effect.
|
|||
Range: D1U1 | D1U2 |D1U3 |D1U4 |D1U5 |D1U6|D2U1 | D2U2 |D2U3 | D2U4 |D2U5|D3U1 | D3U2 | D3U3 |D3U4| D4U1 | D4U2 |D4U3| D5U1|D5U2|D6U1|CUSTom | |||
Range: D1U1 | D1U2 |D1U3 |D1U4 |D1U5 |D1U6|D2U1 | D2U2 |D2U3 | D2U4 |D2U5|D3U1 | D3U2 | D3U3 |D3U4| D4U1 | D4U2 |D4U3| D5U1|D5U2|D6U1|CUSTom | |||
D2U1 | |||
Requirements | EGPRS LA | ||
OUTPUT 714;"CALL:SET:(PDTC2|PDTCH2|PDTChannel2):MSLot:CONFig D2U1" ! Sets the multislot configuration to be 2 downlink PDTCHs and 1 uplink PDTCH. |
This command is not applicable to the GSM Test Application. | ||
This command is not applicable to the GPRS Test Application. | ||
This command is not applicable to the EGPRS Test Application. | ||
This command is not applicable to the GSM/EGPRS Lab Application | ||
This command sets/queries the customized multislot configuration. See Flexible Timeslot for more information. The command form accepts two string parameters with each contains a maximum of 8 characters. The first string represents the timeslot usage of TS0 to TS7 of the downlink timeslots and the second string represents the timeslot usage of TS0 to TS7 of the uplink timeslots. Each timeslot of the uplink and downlink can be configured to one of the three values:
If less than 8 characters in each string are specified in a parameter, the remaining higher numbered timeslots are assumed to be OFF. |
||
Range: -, ,x,X,0 |p,P,1 | ||
Range: - |P | ||
--PP----,--P----- | ||
Requirements | GSM/GPRS/ EGPRS LA | |
OUTPUT 714;"CALL:SET:(PDTC2|PDTCH2|PDTChannel2):MSLot:CONFig:CUSTom:TSLots --PP----,--P-----" ! Sets the custom multislot configuration to be 2 downlink PDTCHs and 1 uplink PDTCH. Timeslot 2 and 3 ! are configured to PDCH in the downlink and Timeslot 2 is configured to PDCH in the uplink. |
This command is not applicable to the GSM Test Application. | ||
This command is not applicable to the GPRS Test Application. |
||
This command is not applicable to the GSM/GPRS Lab Application. |
||
EGPRS TA |
This command is not applicable to the EGPRS Test Application. |
|
EGPRS LA |
This command sets/queries the power reduction reference level (ETSI refers to this as P0) for the downlink PDTCH carrier 2 power control as part of executing a deferred handover in Dual Transfer Mode. For further information see Downlink Dual Carrier . |
|
Setting |
Range: 0 to 30 dB Resolution: 2 dB |
|
Query |
Range: 0 to 30 dB Resolution: 2 dB |
|
*RST setting | 0 dB | |
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:SETup:PDTC2:DTM:PZERo:LEVel 30" ! Sets the power reduction reference level (P0) to 30 dB for DTM mode. |
Sets/queries the channel number of downlink and uplink TCH for the band already selected. See Configuring the Traffic Channel (TCH) Parameters . TCH ARFCN may be set and queried when the CALL:STATUS:STATE is idle or connected, see CALL:STATus[:STATe][:VOICe]? . |
||
This command is not applicable to GPRS. | ||
This command is not applicable to the EGPRS test application. | ||
|
||
|
||
PGSM, EGSM and RGSM bands: 30, DCS and PCS bands: 698, GSM450: 280, GSM480: 320, GSM750: 460, GSM850: 160, TGSM810: 400. |
||
GSM/GPRS/ EGPRS TA |
||
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:SETup:TCH 515" ! Sets the ARFCN to 515 if it is appropriate in the current band. |
Sets/queries which GSM band the BS Emulator should use for the TCH. The test set may be queried for the current TCH band when the CALL:STATUS:STATE is idle or connected, see CALL:STATus[:STATe][:VOICe]? . The test set uses this command to perform a channel assignment, see How the Test Set Performs a Dualband Handover when the MS will support the band and the CALL:STATUS:STATE is CONNected. |
||
This command is not applicable to GPRS. | ||
This command is not applicable to the EGPRS test application. | ||
Range: DCS | EGSM | GSM450 | GSM480 | GSM750 | GSM850 |PCS |PGSM |RGSM| TGSM810 |
||
Range: DCS | EGSM | GSM450 | GSM480 | GSM750 | GSM850 |PCS |PGSM |RGSM| TGSM810 |
||
See Traffic Band Parameter . |
||
GSM/GPRS/ EGPRS TA |
||
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:SETup:TCH:BAND DCS" ! Sets the deferred band to DCS |
Please use CALL:SETup:TCHannel:CMODe:LSPeech:CHANnel instead. This command sets/queries which channel mode the mobile station should use for speech data. This setting is either full rate speech (FRSPeech), enhanced full rate speech (EFRSpeech) or half rate speech (HRSPeech). See Programming a Channel Mode Change . |
||
This command is not applicable to GPRS. | ||
This command is not applicable to the EGPRS test application. | ||
FRSPeech | ||
GSM/GPRS/ EGPRS TA |
||
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:SETup:TCH:CMODe EFRSpeech" ! Sets the TCH coding mode to EFRSpeech |
This command selects the mobile station uplink power control level for the band already selected. See Frequency Banded Parameters . |
||
This command is not applicable to the EGPRS test application. | ||
The default TX Level depends on the band (the default band is PGSM): |
||
GSM/GPRS/ EGPRS TA |
||
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:SETup:TCH:MS:TXLevel 19" ! Sets the deferred mobile station TX level for the currently selected band. |