Last updated: December 3, 2008
GSM TA |
Queries the bit error measurement. Query returns integrity indicator, bits tested, bit error ratio, and bit error count. (A similar query, FETCh:BERRor:FULL? , returns the same results but for all bit types simultaneously.) See Bit Error Measurement . |
|
This command is not applicable to GPRS. | ||
|
||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA |
GSM TA |
Queries the number of bits actually tested. This query only returns the result of the bit type set using the SETup:BERRor[:TYPE] command. The number of bits actually tested will exceed the number requested because the test set rounds up the number requested to the nearest number that results in an integral number of speech frames. One speech frame is 132 bits. The test set measures complete a speech frame and it is queried for bits. See Bit Error Measurement |
|
GPRS TA | ||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA |
GSM TA |
Queries the number of bits which have been tested. This query allows you to select the bit type you want to query; either Type Ia, Type Ib or Type II. See Bit Error Measurement |
|
EGPRS TA | ||
Range for Type Ia: 0 to 999,000 and 9.91 E+37 (NAN) Range for Type Ib: 0 to 2,637,369 and 9.91 E+37 (NAN) |
||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA |
GSM TA |
Queries the number of bits that were in error during the last bit error test. See Bit Error Measurement |
|
EGPRS TA | ||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA |
Queries the number of bad cyclic redundancy checks (CRCs) for a non-residual measurement type, loopback type B test. See Bit Error Measurement The mobile station re-transmits the CRC it received from the test set on the uplink. A bad CRC occurs when the CRC transmitted by the test set does not match what is received back from the mobile station. |
||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA |
GSM TA |
Queries the number of frames erased during a residual measurement type, looback type A test. |
|
EGPRS TA | ||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA |
GSM TA |
Queries the number of bits in error. This query allows you to select the bit type you want to query; either Type Ia, Type Ib or Type II. See Bit Error Measurement |
|
EGPRS TA | ||
Range for Type Ia: 0 to 999,000 and 9.91 E+37 (NAN) Range for Type Ib: 0 to 2,637,369 and 9.91 E+37 (NAN) |
||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA |
Queries the delay (in speech frames) that the test set used during the last bit error measurement to correlate uplink information bits with downlink information bits. This value is displayed in the Loopback Delay field. This value can be determined automatically, or manually set by the user. See SETup:BERRor:MANual:DELay and SETup:BERRor:LDControl:AUTO . Refer also to the Bit Error Measurement for a description of loopback delay and how it is used in the bit error measurement. |
||
EGPRS TA | ||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA |
Queries the bit error measurement. Returns Integrity Indicator see Integrity Indicator , Bits Tested, Bit Error Ratio and Bit Error Count for Type Ia, Type Ib and Type II bits. (A similar query, FETCh:BERRor[:ALL]? , returns the same results but only for the bit type previously set using the SETup:BERRor[:TYPE] command.) See Bit Error Measurement |
||
EGPRS TA | ||
|
||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA |
GSM TA |
Queries the intermediate count of bits tested (measurement progress report). See Measurement Progress Report |
|
EGPRS TA | ||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA |
GSM TA |
Returns the integrity indicator value for the last bit error measurement performed. Zero indicates a normal result. See Integrity Indicator for descriptions of non-zero integrity indicators. |
|
Range: See Integrity Indicator . |
||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA |
GSM TA |
Queries the ratio of bits in error to the number of bits tested during the last bit error test and returns it as a percentage. See Bit Error Measurement |
|
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA |
GSM TA |
Queries the ratio of bad cyclic redundancy checks (CRCs) to the total number of CRCs received for a non-residual measurement type, looback type B test and returns it as a percentage. See Bit Error Measurement The mobile station re-transmits the CRC it received from the test set on the uplink. A bad CRC occurs when the CRC transmitted by the test set does not match what is received back from the mobile station. |
|
EGPRS TA | ||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA |
GSM TA |
Queries the ratio of erased frames to the total number of frames received for a residual measurement type, looback type A test and returns them as a percentage. See Bit Error Measurement |
|
EGPRS TA | ||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA |
GSM TA |
Queries the number of bits in error to the number of bits tested. This query allows you to select the bit type you want to query; either Type Ia, Type Ib or Type II. The result is returned as a percentage. See Bit Error Measurement |
|
EGPRS TA | ||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA |