Last updated: December 3, 2008
Queries the EDGE Dynamic Power measurement results. Query returns N integrity indicators and N average TX power levels (where N is the number measurement results present in the specified range). Each of the ranges can return measurement results, that is, integrity and power measurements, for up to 100 burst. Therefore if you have set up to measure 250 bursts you must query range 1, range 2 and range 3 to obtain all your results. If a range contains no measurement results, a single integrity value of `1' and a single power value of NAN are returned. |
||
GSM/GPRS LA | ||
Integrity indicators for each individual burst
|
||
Requirements |
GSM/GPRS/ EGPRS TA |
Revision A.05 makes the EDP Measurement available in all TAs. |
GSM/GPRS/ EGPRS LA |
Revision D.02 makes the EDP Measurement available in all LAs. |
|
OUTPUT 714;"FETCh:EDPower?" ! Queries the Dynamic Power measurement results for the first 100 bursts. |
Returns N integrity indicators (where N is the number of measurement results present in the specified range). Each of the ranges can query up to 100 bursts. For example, if you want to obtain the measurements for 160 bursts you must query range 1 and range 2 to obtain all the integrity indicators. Range 1 will contain the maximum of 100 measurement results and Range 2 contains the remaining 60 measurement results. If a range contains no measurement results, a single value of `1' is returned. |
||
Range: See Integrity Indicator . |
||
Requirements |
GSM/GPRS/ EGPRS TA |
Revision A.05 makes the EDP Measurement available in all TAs. |
GSM/GPRS/ EGPRS LA |
Revision D.02 makes the EDP Measurement available in all LAs. |
|
OUTPUT 714;"FETCh:EDPower:INTegrity:RANGe3?" ! Queries the integrity results for bursts 201 through 300. |
Queries the average TX power levels for the EDGE Dynamic Power measurement. Returns N average power levels (where N is the number of measurement results present in the specified range). To set the number of bursts you want to measure, see SETup:EDPower:COUNt:NUMBer . Each of the ranges can query up to 100 bursts. Therefore if you have set up to measure 400 bursts you must use range 1, range 2, range 3 and range 4 to obtain all your TX power level results. If a range contains no measurement results, a single NAN value is returned. |
||
GSM/GPRS LA | ||
Requirements |
GSM/GPRS/ EGPRS TA |
Revision A.05 makes the EDP Measurement available in all TAs. |
GSM/GPRS/ EGPRS LA |
Revision D.02 makes the EDP Measurement available in all LAs. |
|
OUTPUT 714;"FETCh:EDPower:POWer:RANGe2?" ! Queries the average TX power for bursts 101 through 200. |