Last updated: December 3, 2008
GSM TA |
Queries the fast bit error measurement. Query returns integrity indicator, bits tested, bit error ratio, and bit error count. Bit error ratio is displayed in the Fast Bit Error field. The other values returned by this query are not available on the front panel display. |
|
|
||
GSM/GPRS/ EGPRS TA |
||
GSM/GPRS/ EGPRS LA |
GSM TA |
Queries the total number of information bits tested during the last fast bit error measurement. See SETup:FBERror:COUNt |
|
GSM/GPRS/ EGPRS TA |
||
GSM/GPRS/ EGPRS LA |
GSM TA |
Queries the number of information bits that were deemed errors during the last fast bit error test. |
|
GSM/GPRS/ EGPRS TA |
||
GSM/GPRS/ EGPRS LA |
Queries the delay (in TDMA frames) the test set used during the last fast bit error measurement to correlate uplink information bits with downlink information bits. This value is displayed in the TDMA Frame Delay field. This value can be determined automatically, or set by the user. See SETup:FBERror:MANual:DELay and SETup:FBERror:LDControl:AUTO for setting this value manually. Refer also to the Fast Bit Error Measurement Description for a description of frame delay and how it is used in the fast bit error measurement. |
||
GSM/GPRS/ EGPRS TA |
||
GSM/GPRS/ EGPRS LA |
GSM TA |
Queries the intermediate count (measurement progress report) of bits tested |
|
GSM/GPRS/ EGPRS TA |
||
GSM/GPRS/ EGPRS LA |
GSM |
Returns the integrity indicator value for the last fast bit error measurement performed. Zero indicates a normal result. See Integrity Indicator for descriptions of non-zero integrity indicators. |
|
Range: See Integrity Indicator . |
||
GSM/GPRS/ EGPRS TA |
||
GSM/GPRS/ EGPRS LA |
GSM TA |
Queries the ratio of bits deemed bad to total bits tested during the last fast bit error measurement performed. |
|
GSM/GPRS/ EGPRS TA |
||
GSM/GPRS/ EGPRS LA |