FETCh:IFERror

FETCh:IFERror

Last updated: December 3, 2008

GPIB Command Conventions

FETCh:IFERror[:ALL]?

Function

GSM TA

This command is not applicable to the GSM TA.

GPRS TA

This command is not applicable to the GPRS TA.

EGPRS TA

This command is not applicable to the EGPRS TA.

GSM/GPRS LA

Queries, in the following order: integrity, speech frames measured, frame error ratio, and frame error count.

EGPRS LA

Query

Integrity indicator

Number of speech frames tested

  • Range: 1 to 900000 or 9.91e+37 (NAN)
  • Resolution: 1

Frame Error Ratio

  • Range: 0 to 100 or 9.91e+37 (NAN)
  • Resolution: .001

Frame Error Count

  • Range: 0 to 900000 or 9.91e+37 (NAN)
  • Resolution: 1
Requirements

GSM/GPRS/ EGPRS LA

Revision: D.01 and above

GSM/GPRS/ EGPRS TA

Revision: A.09 and above with required feature license.

Programming Example

 
OUTPUT 714;"FETCh:IFERror?" 
! Queries for values in the following order: integrity, speech frames tested, frame error ratio, 
! frame error count.

FETCh:IFERror:COUNt?

Function

GSM TA

This command is not applicable to the GSM TA.

GPRS TA

This command is not applicable to the GPRS TA.

EGPRS TA

This command is not applicable to the EGPRS TA.

GSM/GPRS LA

Queries the frame error count.

EGPRS LA

Query

Range: 1 to 900000 or 9.91e+37 (NAN)

Resolution: 1

Requirements

GSM/GPRS/ EGPRS LA

Revision: D.01 and above

GSM/GPRS/ EGPRS TA

Revision: A.09 and above with required feature license.

Programming Example

 
OUTPUT 714;"FETCh:IFERror:COUNt?" 
! Queries the frame error count.

FETCh:IFERror:DELay?

Function

GSM TA

This command is not applicable to the GSM TA.

GPRS TA

This command is not applicable to the GPRS TA.

EGPRS TA

This command is not applicable to the EGPRS TA.

GSM/GPRS LA

Queries the number of speech frames that were necessary for the test set to synchronize the uplink with the downlink.

EGPRS LA

Requirements

GSM/GPRS/ EGPRS LA

Revision: D.01 and above

GSM/GPRS/ EGPRS TA

Revision: A.09 and above with required feature license.

Programming Example

 
OUTPUT 714;"FETCh:IFERror:DELay?" 
! Queries the number of speech frames that were necessary for the test set to synchronize 
! the uplink with the downlink.

FETCh:IFERror:ICOunt?

Function

GSM TA

This command is not applicable to the GSM TA.

GPRS TA

This command is not applicable to the GPRS TA.

EGPRS TA

This command is not applicable to the EGPRS TA.

GSM/GPRS LA

Queries the measurement progress by returning the number of frames measured of the total to be measured.

EGPRS LA

Query

Range: 1 to 900000 or 9.91e+37 (NAN)

Resolution: 1

Requirements

GSM/GPRS/ EGPRS LA

Revision: D.01 and above

GSM/GPRS/ EGPRS TA

Revision: A.09 and above with required feature license.

Programming Example

 
OUTPUT 714;"FETCh:IFERror:ICOunt?" 
! Queries the measurement progress.

FETCh:IFERror:INTegrity?

Function

GSM TA

This command is not applicable to the GSM TA.

GPRS TA

This command is not applicable to the GPRS TA.

EGPRS TA

This command is not applicable to the EGPRS TA.

GSM/GPRS LA

Queries the integrity indicator value for each burst.

EGPRS LA

Query

Range: See Integrity Indicator .

Resolution: 1

Requirements

GSM/GPRS/ EGPRS LA

Revision: D.01 and above

GSM/GPRS/ EGPRS TA

Revision: A.09 and above with required feature license.

Programming Example

 
OUTPUT 714;"FETCh:IFERror:INTegrity?" 
! Queries the measurement integrity indicator value.

FETCh:IFERror:RATio?

Function

GSM TA

This command is not applicable to the GSM TA.

GPRS TA

This command is not applicable to the GPRS TA.

EGPRS TA

This command is not applicable to the EGPRS TA.

GSM/GPRS LA Queries the frame error ratio.

EGPRS LA

Query

Range: 0 to 100 or 9.91e+37 (NAN)

Resolution: .001

Requirements

GSM/GPRS/ EGPRS LA

Revision: D.01 and above

GSM/GPRS/ EGPRS TA

Revision: A.09 and above with required feature license.

Programming Example

 
OUTPUT 714;"FETCh:IFERror:RATio?" 
! Queries for the frame error ratio.

FETCh:IFERror:SFRames?

Function

GSM TA

This command is not applicable to the GSM TA.

GPRS TA

This command is not applicable to the GPRS TA.

EGPRS TA

This command is not applicable to the EGPRS TA.

GSM/GPRS LA

Queries the number of speech frames measured.

EGPRS LA

Query

Range: 1 to 900000 or 9.91e+37 (NAN)

Resolution: 1

Requirements

GSM/GPRS/ EGPRS LA

Revision: D.01 and above

GSM/GPRS/ EGPRS TA

Revision: A.09 and above with required feature license.

Programming Example

 
OUTPUT 714;"FETCh:IFERror:SFRames?" 
! Queries for the number of frames measured.