Last updated: January 18, 2010
GSM TA |
Queries (initiates and fetches) one analog audio measurement as a sequential operation. Returns an integrity indicator (see Integrity Indicator ), average analog audio level, average SINAD, average distortion and the average audio frequency. Values are returned in a comma-separated list. Returns Integrity Indicator, see Integrity Indicator and analog audio (average). The FETCh command should be used to obtain other measurement results. See FETCh:AAUDio . |
|
Query |
|
|
GSM/GPRS/ EGPRS TA |
||
GSM/GPRS/ EGPRS LA |
GSM TA |
Queries (initiates and fetches) one RX bit error measurement as a sequential operation. Returns Integrity Indicator see Integrity Indicator , Bits Tested, Bit Error Ratio and Bit Error Count, for the bit type set using SETup:BERRor[:TYPE] . (A similar query, READ:BERRor:FULL? , returns the same results but for all residual, or all non-residual bit types simultaneously.) The FETCh command should be used to obtain other measurement results. See FETCh:BERRor . |
|
Query |
|
|
GSM/GPRS/ EGPRS TA |
||
GSM/GPRS/ EGPRS LA |
GSM TA |
Queries (initiates and fetches) one RX bit error measurement as a sequential operation. Either all of the residual or non-residual results are returned, depending on the type of bit error measurement set using SETup:BERRor[:TYPE] . Returns Integrity Indicator (see Integrity Indicator ), Bits Tested, Bit Error Ratio and Bit Error Count for Type Ia, Type Ib and Type II. (A similar query, READ:BERRor[:ALL]? , returns the same results but only for the bit type previously set using SETup:BERRor[:TYPE] .) The FETCh command should be used to obtain other measurement results. See FETCh:BERRor . |
|
|
||
GSM/GPRS/ EGPRS TA |
||
GSM/GPRS/ EGPRS LA |
GSM TA | ||
Queries (initiates and fetches) one block error measurement as a sequential operation. Returns Integrity Indicator (see Integrity Indicator ), Blocks Tested, Block Error Ratio, and Block Error Count. The FETCh command should be used to obtain other measurement results. See FETCh:BLERror . |
||
|
||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA |
GSM TA | ||
Queries the block error measurement results for all the bursts. The total integrity indicator and the block error ratio for burst 1 to 8 are returned. Note, the block error ratio for burst 6, 7 and 8 are always NAN. . This query can only be used when the BLER measurement method is Polling. See Block Error Measurement for more information about the BLER measurement methods. |
||
|
||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA | ||
Programming Example
OUTPUT 714;"READ:BLER:BURS:ALL?"
|
GSM TA | ||
This command is not applicable to GPRS TA. | ||
This command is not applicable to GSM/GPRS LA. | ||
EGPRS TA |
Queries the block error measurement results for all the bursts on Carrier 2. The total integrity indicator and the block error ratio for burst 1 to 8 are returned. This query can only be used when the BLER measurement method is Polling. See Block Error Measurement for more information about the BLER measurement methods. |
|
|
||
Requirements | GSM/GPRS/ EGPRS LA | |
Programming Example
OUTPUT 714;"READ:BLER:PDTC2 BURS:ALL?"
|
Queries (initiates and fetches) one bad frame indication measurement as a sequential operation. Returns Integrity Indicator see Integrity Indicator , Number of Samples Counted, Number of Undetected Bad Frames, Number of SIDs Reported as Bad Frames, and the Number of SIDs Sent. The FETCh command should be used to obtain other measurement results. See FETCh:<BFINdication|BFI> . |
||
GSM TA | This command is not applicable to the GSM Test Application. | |
EGPRS TA | ||
Query |
|
|
Requirements | GSM/GPRS/ EGPRS LA |
GSM TA |
Queries (initiates and fetches) one decoded audio (uplink speech level) measurement as a sequential operation. Returns Integrity Indicator see Integrity Indicator and decoded audio (average). The FETCh command should be used to obtain other measurement results. See FETCh:DAUDio . |
|
|
||
GSM/GPRS/ EGPRS TA |
||
GSM/GPRS/ EGPRS LA |
GSM TA | Queries the Dynamic Power measurement results. Query returns N integrity indicators and N average TX power levels (where N is the number of bursts measured). To set the number of bursts you want to measure, use SETup:DPOWer:COUNt:NUMBer[:SELected] . The maximum number of results that can be returned is 99. Measurement result 100 and above must be retrieved using the FETCh command. | |
Integrity indicators for each individual burst
|
||
GSM/GPRS/ EGPRS TA |
||
GSM/GPRS/ EGPRS LA |
GSM TA | Queries the EDGE Dynamic Power measurement results. Query returns N integrity indicators and N average TX power levels (where N is the number of measurement results present in the specified range). To set the number of bursts you want to measure, use SETup:EDPower:COUNt:NUMBer . | |
Integrity indicators for each individual burst
|
||
GSM/GPRS/ EGPRS TA |
Revision A.05 makes the EDP Measurement available in all TAs. |
|
GSM/GPRS/ EGPRS LA |
Revision D.02 makes the EDP Measurement available in all LAs. |
GSM TA | ||
Queries (initiates and fetches) the 8PSK multislot modulation accuracy measurement results as a sequential operation. Queries integrity indicator, RMS error vector magnitude (EVM), peak EVM, 95th percentile EVM, frequency error, origin offset suppression, RMS phase error, peak phase error, RMS magnitude error, peak magnitude error, amplitude droop, IQ imbalance. |
||
|
||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA |
GSM TA | ||
Queries (initiates and fetches) the ETSI specified 8PSK multislot modulation accuracy results. The query returns integrity indicator, RMS error vector magnitude (EVM), peak EVM, 95th percentile EVM, frequency error, and origin offset suppression. |
||
|
||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA |
GSM TA | ||
Queries (initiates and fetches) one EGPRS TX power measurement as a sequential operation. Returns Integrity Indicator (see Integrity Indicator ), average burst power, and average estimated carrier power. When the selected modulation format is set to GMSK, Burst Power and Carrier Power measurements are equivalent so both results return the same value. |
||
|
||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA |
GSM |
Queries (initiates and fetches) one fast bit error measurement as a sequential operation. Returns Integrity Indicator see Integrity Indicator , Bits Tested, Bit Error Ratio, and Fast Bit Error Count using mobile station burst-by-burst looback (type C loopback). The FETCh command should be used to obtain other measurement results. See FETCh:BERRor . |
|
GSM/GPRS LA | ||
|
||
GSM/GPRS/ EGPRS TA |
||
GSM/GPRS/ EGPRS LA |
GSM/GPRS LA |
Queries (initiates and fetches) one frame erasure rate on FACCH full rate speech measurement as a sequential operation. Returns Integrity Indicator see Integrity Indicator , Samples, Frame Erasure Ratio, and Count of Retransmissions. The FETCh command should be used to obtain other measurement results. See FETCh:FFERate . |
|
This command is not applicable to the GPRS Test Application. |
||
This command is not applicable to the EGPRS Test Application. |
||
|
||
GSM/GPRS/ EGPRS LA |
GSM TA |
Initiates and fetches a frequency stability measurement as a sequential operation. Measurement results are returned in the following order: integrity, worst-case frequency error, average frequency. |
|
Initiates and fetches a frequency stability measurement as a sequential operation. Measurement results are returned in the following order: integrity, worst-case frequency error, average frequency. |
||
Query |
|
|
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA |
GSM TA | ||
Queries (initiates and fetches) one bit error measurement as a sequential operation. Returns Integrity Indicator see Integrity Indicator , Bits Tested, Bit Error Ratio, and Bit Error Count. The FETCh command should be used to obtain other measurement results. See FETCh:GBERror . |
||
|
||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA |
GSM TA | ||
GPRS TA | ||
EGPRS TA | ||
Queries (initiates and fetches) one bit error measurement as a sequential operation. Returns the results in the following order: integrity, speech frames measured, frame error ratio, and frame error count. |
||
|
||
Requirements | GSM/GPRS/ EGPRS LA |
GSM TA |
Queries (initiates and fetches) the I/Q Tuning measurement results. Query returns the integrity indicator and the relative power level at the following offset frequencies: carrier frequency, 䕧.7083 kHz, 𫏯.417 kHz, 𫐳.125 kHz, 𫑶.833 kHz. The spur measurement result is also returned. The FETCh command should be used to return other measurement results. See FETCh:IQTuning . |
|
Signal level relative to the desired signal at 9 different frequencies |
||
GSM/GPRS/ EGPRS TA |
||
GSM/GPRS/ EGPRS LA |
GSM TA |
Queries (initiates and fetches) the Multi-Tone Audio measurement results. Query returns the integrity indicator and a comma separated list of RMS audio levels for the 20 audio tones. The FETCh command should be used to return other measurement results. See FETCh:MTAudio[:ALL]? . |
|
This command is not applicable to GPRS. | ||
|
||
GSM/GPRS/ EGPRS TA |
||
GSM/GPRS/ EGPRS LA |
GSM TA |
Queries (initiates and fetches) one output RF spectrum measurement as a sequential operation. Returns Integrity Indicator see Integrity Indicator , TX Power, Output RF Spectrum due to Switching (Max), 30 kHz Bandwidth Power, and Output RF Spectrum due to Modulation (Average). The FETCh command should be used to obtain other measurement results. See FETCh:ORFSpectrum . |
|
|
||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA |
GSM TA |
This command initiates the Phase and Amplitude versus Time measurement and fetches the results when the measurement is complete.
This query is only applicable when the waveform type is
If the waveform type is The values returned by this query are a single integrity result for the measurement followed by a comma separated list of up to 512 measured power values, followed by a comma separated list of up to 512 measured phase values, followed by a comma separated list of up to 512 frequency error results. The first measured power value is the absolute power level and all subsequent power values are relative to the absolute power. The first phase value is 0° and all subsequent values are phase values relative to the 0° reference. The first frequency value is the absolute frequency, and all subsequent values are relative to the absolute frequency. |
|
GSM/GPRS LA | ||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA |
GSM TA |
Queries (initiates and fetches) one Phase and Frequency Error measurement as a sequential operation. Returns Integrity Indicator see Integrity Indicator , RMS Phase Error (Max), Peak Phase Error (Max), Frequency Error (Worst). The FETCh command should be used to obtain other measurement results. See FETCh:PFERror . Worst frequency error (negative or positive) is the value furthest from zero. |
|
GSM/GPRS LA | ||
|
||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA |
GSM |
Queries (initiates and fetches) one Phase and Frequency Error measurement as a sequential operation. Returns Integrity Indicator see Integrity Indicator , RMS Phase Error pass/fail indicator, Peak Phase Error pass/fail indicator, Frequency Error pass/fail indicator, and the number of measurements taken. The number of measurements taken may be of interest to you if you are using the confidence level feature. For more information on using confidence levels refer to Confidence Levels . The FETCh command should be used to obtain other measurement results. See FETCh:PFERror . Worst frequency error (negative or positive) is the value furthest from zero. |
|
RMS phase error pass/fail indicator Peak phase error pass/fail indicator |
||
GSM/GPRS/ EGPRS TA |
||
GSM/GPRS/ EGPRS LA |
GSM TA |
Queries (initiates and fetches) one power versus time measurement as a sequential operation. Returns Integrity Indicator see Integrity Indicator , Mask pass/fail, power versus time transmit power and up to 12 power versus time offset (max) results. The FETCh command should be used to obtain other measurement results. See FETCh:PVTime . |
|
This command is not applicable to the GPRS Test Application. | ||
This command is not applicable to the GPRS Test Application. | ||
|
||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA |
GSM TA | This command is not applicable for GSM. | |
Queries (initiates and fetches) one power versus time measurement as a sequential operation for the burst in the multislot configuration that you specify. Returns Integrity Indicator see Integrity Indicator , Mask pass/fail, power versus time transmit power and up to 12 power versus time offset (max) results. The FETCh command should be used to obtain other measurement results. See FETCh:PVTime . |
||
|
||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA |
GSM TA | ||
This command is not applicable to GPRS TA. | ||
This command is not applicable to the GSM/GPRS LA. | ||
Queries (initiates and fetches) one bit error measurement as a sequential operation. Returns Integrity Indicator see Integrity Indicator , Bits Tested, Bit Error Ratio, and Bit Error Count. The FETCh command should be used to obtain other measurement results. See FETCh:SBERror . |
||
|
||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA |
GSM/GPRS LA |
Queries (initiates and fetches) one Repeated SACCH Frame Erasure Rate (FER) measurement as a sequential operation. Returns Integrity Indicator see Integrity Indicator , Samples, Frame Erasure Ratio, and Frame Erasure Count. The FETCh command should be used to obtain other measurement results. See FETCh:SFERate[:ALL]? . |
|
This command is not applicable to the GPRS Test Application. |
||
This command is not applicable to the EGPRS Test Application. |
||
|
||
GSM/GPRS/ EGPRS LA |
GSM TA |
Queries (initiates and fetches) one TX power measurement as a sequential operation. Returns Integrity Indicator see Integrity Indicator and transmit power (average). The FETCh command should be used to obtain other measurement results. See FETCh:TXPower . |
|
This command is not applicable to the EGPRS Test Application. |
||
|
||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA |