This command is not applicable to GSM TA. | ||
This command is not applicable to GPRS TA. | ||
This command is not applicable to GSM/GPRS LA. | ||
EGPRS TA |
This command sets/queries the group count, that is the number of bursts at each power level, for each ramp segment. For the command form, if the number of parameters sent exceeds the current number of ramp segments, the additional values are stored but are only used in a measurement if the number of ramp segments is increased. If the group size is set to a value greater than the number of bursts in a ramp segment, the group size will truncate the group size to the number of bursts in the ramp segment. The query form of this command returns one value per ramp segment. The number of ramp segments is specified by the command SETup:EDPower:COUNt:RSEGment . The total number of bursts to be measured over all ramp segments can be obtained with the query SETup:EDPower:COUNt:TOTal? . |
|
Setting | ||
*RST Setting | 1 | |
GSM/GPRS/EGPRS TA |
Revision A.05 makes the EDP Measurement available in all TAs. |
|
GSM/GPRS/EGPRS LA |
Revision D.02 makes the EDP Measurement available in all LAs. |
|
|
This command is not applicable to GSM TA. | ||
This command is not applicable to GPRS TA. | ||
This command is not applicable to GSM/GPRS LA. | ||
EGPRS TA |
This command sets/queries the number of bursts to be measured for each ramp segment. For the command syntax, if the number of parameters sent exceeds the current number of ramp segments, the additional values are stored but are only used in a measurement if the number of ramp segments is increased The total number of bursts to be measured over all ramp segments can be obtained with the query SETup:EDPower:COUNt:TOTal? . |
|
Setting | ||
*RST Setting | 25 | |
GSM/GPRS/EGPRS TA |
Revision A.05 makes the EDP Measurement available in all TAs. |
|
GSM/GPRS/EGPRS LA |
Revision D.02 makes the EDP Measurement available in all LAs. |
|
OUTPUT 714; "SETup:EDPower:COUNt:RSEGment 4" ! Sets number of ramp segments to 4. OUTPUT 714; "SETup:EDPower:COUNt:NUMBer 25, 50, 75, 100, 125, 150" ! Specifies the burst count for 6 ramp segments, only the first 4 will be used. OUTPUT 714; "SETup:EDPower:COUNt:NUMBer?" ! Query returns one value per ramp segment (25, 50, 75, 100). OUTPUT 714; "SETup:EDPower:COUNt:TOTal?" ! Query returns the total number of bursts for the whole measurement (250). OUTPUT 714; "SETup:EDPower:COUNt:RSEGment 6" ! Increases number of ramp segments to 6. OUTPUT 714; "SETup:EDPower:COUNt:NUMBer?" ! Query now returns all six values (25, 50, 75, 100, 125, 150). OUTPUT 714; "SETup:EDPower:COUNt:TOTal?" ! Query returns the total number of bursts for the whole measurement (525). |
This command is not applicable to GSM TA. | ||
This command is not applicable to GPRS TA. | ||
This command is not applicable to GSM/GPRS LA. | ||
EGPRS TA |
This command queries the total number of bursts to be measured by the EDGE Dynamic Power measurement. The value returned will be the sum of the burst counts specified for each ramp segment. For more information see SETup:EDPower:COUNt:NUMBer . |
|
*RST Setting | 25 | |
GSM/GPRS/EGPRS TA |
Revision A.05 makes the EDP Measurement available in all TAs. |
|
GSM/GPRS/EGPRS LA |
Revision D.02 makes the EDP Measurement available in all LAs. |
|
OUTPUT 714;"SETup:EDPower:COUNt:TOTal?" ! Queries the total number of bursts to be measured for the whole measurement. This value ! is the sum of values returned by SET:EDP:COUN:NUMB? |
This command sets/queries the EDGE Dynamic Power Measurement Expected Maximum Time Interval value in seconds and sets the Expected Maximum Time Interval State to ON for the active format. This combines the commands SETup:EDPower:EMTInterval:STATe and SETup:EDPower:EMTInterval:TIME . | ||
Setting | ||
*RST Setting | ||
GSM/GPRS/ EGPRS TA |
||
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"SETup:EDPower:EMTInterval:STIMe 0.1" ! Sets the EDPOW Expected Maximum Time Interval State to ON and sets the value to 0.1s. |
This command sets/queries the EDGE Dynamic Power Measurement Expected Maximum Time Interval State. When this parameter is set to ON, the EDPOW Measurement will stop waiting and return measurement results if the time between the input bursts is over the value specified by the Expected Maximum Time Interval Value parameter.See SETup:EDPower:EMTInterval:TIME for information on how to set the Expected Maximum Time Interval Value. |
||
Setting | ||
*RST Setting | 0|OFF | |
GSM/GPRS/ EGPRS TA |
||
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"SETup:EDPower:EMTInterval:STATe ON" ! Sets the EDPOW Expected Maximum Time Interval State to ON. |
This command sets/queries the EDGE Dynamic Power Measurement Expected Maximum Time Interval value between the measured bursts when the EDPOW Expected Maximum Time Interval State is set to ON. See SETup:EDPower:EMTInterval:STATe for information on how to set the Expected Maximum Time Interval State. | ||
Setting | ||
*RST Setting | ||
GSM/GPRS/ EGPRS TA |
||
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"SETup:EDPower:EMTInterval:TIME 0.1" |
This command is not applicable to GSM TA. | ||
This command is not applicable to GPRS TA. | ||
This command is not applicable to GSM/GPRS LA. | ||
EGPRS TA |
This command sets/queries whether or not the expected power for the first burst in each ramp segment should be derived automatically by the test set. When this command is set to 1 or ON, the same expected power setting is used for the first burst in all ramp segments. The value used for the expected power depends on the state of the Expected Power Control. To set the state of the test set's expected power see RFANalyzer:CONTrol:POWer:AUTO . If the Expected Power Control parameter is set to Auto, the MS TX Level Burst 1 setting is used, see CALL:(PDTCH|PDTChannel):MS:TXLevel[:SELected]:BURSt<[1]|2|3|4|5> . If the Expected Power Control parameter is set to Manual, the expected power that is used is the power level setting for burst 1 that the test set's receiver is expecting to see. To set the power level that the test set's receiver is expecting see RFANalyzer:MANual:POWer:BURSt<[1]|2|3|4|5|6|7> . When the initial power state is set to OFF, the initial power values set by the Initial Power Values parameter, SETup:EDPower:INITial:POWer , are used for the expected value in each ramp segment. |
|
Setting | Range: 0 | OFF | 1 | ON | |
Range: 0 | 1 | ||
*RST Setting | 1 (ON) | |
GSM/GPRS/ EGPRS TA |
Revision A.05 makes the EDP Measurement available in all TAs. |
|
GSM/GPRS/ EGPRS LA |
Revision D.02 makes the EDP Measurement available in all LAs. |
|
OUTPUT 714;"SETup:EDPower:INITial:POWer:AUTO ON" ! Specifies that the expected power for the first burst in each ramp segment should be derived ! automatically from the base station emulator. |