Last updated: December 3, 2008
GSM TA | ||
GPRS TA | ||
EGPRS TA | ||
This command combines SETup:IFERror:TIMeout:TIME and SETup:IFERror:TIMeout:STATe . This command sets both the state of the In-Band Frame Error (IFER) measurement timeout to ON and the time for the measurement to time out. The units (S|MS|US|NS) are optional, if none are specified, the the default is S. Only the timeout time is queried with this command. |
||
10 seconds | ||
Requirements | GSM/GPRS/ EGPRS LA | |
Revision: A.09 and above with required feature license. |
||
OUTPUT 714;"SETup:IFERror:TIMeout 5" ! Sets the state of the timeout to ON and the measurement timeout time to 5 seconds. |