This command sets/queries the number of I/Q Tuning multi-measurements the test set makes in the active (that is the selected) format. The multi-measurement count state must be on. See I/Q Tuning Measurement Description . | ||
Setting | ||
*RST Setting |
The *RST value of this command depends on the format that is currently active. For example, if the GSM format is currently active, the *RST value for this command is the same value as the equivalent command containing the :GSM format identifier. |
|
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"SETUP:IQTUNING:COUNT:NUMBER:SELECTED 30" ! Sets the number of multi-measurements. |
This command sets/queries the number of I/Q Tuning multi-measurements the test set makes in the GSM format whether or not that format is active. The multi-measurement count state must be on. See I/Q Tuning Measurement Description . | ||
Setting | ||
*RST Setting | 10 | |
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"SETUP:IQTUNING:COUNT:NUMBER:GSM 30" ! Sets the number of multi-measurements. |