Queries the test set to determine the fastest measurement filter type based on the currently installed hardware and test set configuration. The possible measurement filter types are The command to set the measurement filter type is SETup:ORFSpectrum:FILTer:TYPE . For more information on how the hardware affects the measurement filter type, see: |
||
GSM/GPRS LA |
||
Setting | ||
*RST Setting | ANAL | |
Requirements | ||
Revision: D.03 and above | ||
OUTPUT 714;"SETup:ORFSpectrum:AUTO:FILTer:TYPe?" ! Queries the ORFS modulation measurement filter type that would give the fastest measurement results. |
This command sets/queries the fast measurement state, which determines whether or not the ORFS due to modulation measurement is performed exactly as defined in the ETSI standards. When set to On, the measurement is performed on both the front and back sections of the burst. With this setting, the test set can provide two modulation measurements per burst, effectively doubling measurement throughput. When set to Off, the measurement is only performed on the latter section of the burst as defined in the ETSI GSM standards.
When the ORFS measurement filter type (
SETup:ORFSpectrum:FILTer:TYPE
) is set to |
||
Setting | ||
*RST Setting | 1 | ON | |
Requirements | ||
OUTPUT 714;"SETUP:ORFSPECTRUM:FAST OFF" ! Sets the ORFS modulation measurement to be performed exactly as defined in the ETSI standards. |
Sets/Queries the filter type. The possible measurement filter options are Analog, Digital, and AUTO. The analog and digital measurement filter types each include ORFS due to modulation and ORFS due to switching. When set to AUTO, the test set automatically selects the filter type that will result in the fastest measurement speed based on the test set's hardware specification and the current test set configuration. The filter type chosen by the test set can be queried using the command SETup:ORFSpectrum:AUTO:FILTer:TYPE? . See also Output RF Spectrum Measurement Description for more information regarding the measurement filter type and other information on the ORFS measurement. |
||
GSM/GPRS LA |
||
Setting | ||
*RST Setting | ANAL | |
Requirements | ||
Revision: D.03 and above | ||
OUTPUT 714;"SETup:ORFSpectrum:FILTer:TYPe AUTO" ! Allows the test set to determine which measurement type was the fastest. ! The measurement filter type that is used is what the test set returns from the query ! SETup:ORFSpectrum:AUTO:FILTer:TYPE? |
This command queries the total number of measurements made each time an ORFS measurement is initiated. This number will vary depending on the number of offsets and number of multi-measurements that you choose. The total number of measurements is calculated using the following formula: See Output RF Spectrum Measurement Description for a description of modulation and switching offsets. |
||
Requirements | ||
This query returns the number of enabled reference points for the ORFS Modulation Absolute custom mask you specify. |
||
GSM/GPRS LA |
||
EGPRS LA |
||
*RST Setting | 0 | |
Requirements | ||
This command sets/queries the number of ORFS due to modulation multi-measurements the test set will make when the multi-measurement count state is on. See Output RF Spectrum Measurement Description . | ||
GSM/GPRS LA |
||
Setting | ||
*RST Setting | 20 | |
Requirements | ||
OUTPUT 714;"SETUP:ORFSPECTRUM:MODULATION:COUNT:NUMBER 75" ! Sets the multi-measurement count number for ORFS due to modulation measurements to 75. |
This command sets/queries the list of ORFS due to modulation frequency offsets. Each offset listed in the command is turned on by default. If no frequency offsets (null list) are sent, the output RF spectrum due to modulation measurement will not be made. The units (GHZ|MHZ|KHZ|HZ) are optional, if no units are specified than units default to HZ. see Output RF Spectrum Measurement Description . | ||
GSM/GPRS LA |
||
Setting |
Range: 0 to 22 comma-separated values ranging from -1.8 MHz to -10 Hz, and +10 Hz to +1.8 MHz |
|
Range: 0 to 22 comma-separated values ranging from -1.8 MHz to -10 Hz, and +10 Hz to +1.8 MHz |
||
*RST Setting | ||
Requirements | ||
OUTPUT 714;"SETUP:ORFSPECTRUM:MODULATION:FREQUENCY:OFFSET 400 KHZ, 700 KHZ" ! Turns on the first two ORFS due to modulation measurement offsets and sets ! them to 400 kHz and 700 kHz offsets. All other offsets are in the off state. OUTPUT 714;"SETUP:ORFSPECTRUM:MODULATION:FREQUENCY:OFFSET 700 KHZ" ! Turns on the first ORFS due to modulation measurement offset and sets it to A 700 kHz ! offset. All other offsets are in the off state. OUTPUT 714;"SETUP:ORFSPECTRUM:MODULATION:FREQUENCY:OFFSET" ! Turns all offsets for ORFS due to modulation measurement to the off state. |
This command turns on or off all of the frequency offsets for the ORFS Modulation measurement. |
||||
GSM/GPRS LA |
||||
Setting | ||||
*RST Setting | ||||
Requirements | ||||
This command queries the number of frequency offsets currently on during an ORFS due to modulation measurement in the active (that is the selected) format. See Output RF Spectrum Measurement Description . |
||
GSM/GPRS LA |
||
Requirements | ||
This query returns the number of enabled reference points for the ORFS Modulation Relative custom mask you specify. |
||
GSM/GPRS LA |
||
EGPRS LA |
||
*RST Setting | 0 | |
Requirements | ||
This command sets/queries the ORFS due to switching multi-measurement count value. See Output RF Spectrum Measurement Description . | ||
GSM/GPRS LA |
||
EGPRS LA | ||
Setting | ||
*RST Setting | 10 | |
Requirements | ||
OUTPUT 714;"SETUP:ORFSPECTRUM:SWITCHING:COUNT:NUMBER 15" ! Sets the multi-measurement count number for ORFS due to switching to 15. |
This command sets/queries the list of ORFS due to switching frequency offsets in the active (that is the selected) format. Each offset listed in the command is turned on by default. If no frequency offsets (null list) are sent, the output RF spectrum due to switching measurement will not be made. The units (GHZ|MHZ|KHZ|HZ) are optional, if no units are specified than units default to HZ. See Output RF Spectrum Measurement Description . | ||
GSM/GPRS LA |
||
Setting |
Range: 0 to 8 comma-separated values ranging from -1.8 MHz to -10 Hz, and +10 Hz to +1.8 MHz |
|
Range: 0 to 8 comma-separated values ranging from -1.8 MHz to -10 Hz, and +10 Hz to +1.8 MHz |
||
*RST Setting | ||
Requirements | ||
OUTPUT 714;"SETUP:ORFSPECTRUM:SWITCHING:FREQUENCY:OFFSET 400 KHZ, 700 KHZ" ! Turns on the first two ORFS due to switching measurement offsets and sets them ! to 400 kHz and 700 kHz offsets. All other offsets are in the off state. OUTPUT 714;"SETUP:ORFSPECTRUM:SWITCHING:FREQUENCY:OFFSET 700 KHZ" ! Turns on the first ORFS due to switching measurement offset and sets it to 700 kHz ! offsets. All other offsets are in the off state. OUTPUT 714;"SETUP:ORFSPECTRUM:SWITCHING:FREQUENCY:OFFSET" ! Turns all of the ORFS due to switching measurements offsets to off. |
This command turns on or off all of the frequency offsets for the ORFS Switching measurement. |
||||
GSM/GPRS LA |
||||
Setting | ||||
*RST Setting | ||||
Requirements | ||||
This command queries the number of frequency offsets currently on during an ORFS due to switching measurement. See Output RF Spectrum Measurement Description . | ||
GSM/GPRS LA |
||
Requirements | ||
This query returns the number of enabled reference points for the ORFS Switching Absolute custom mask. |
||
GSM/GPRS LA |
||
EGPRS LA |
||
*RST Setting | 0 | |
Requirements | ||
This command sets/queries the frequency that the time domain trace is made on. the frequency is either equal to that of the carrier or an offset towards the carrier. You can use SETup:ORFSpectrum:SWITching:FREQuency[:OFFSet] to set the offset value. | ||
GPRS TA | ||
GSM/GPRS LA |
||
Setting |
Range: CARRier|OFFSet1|OFFSet2|OFFSet3|OFFSet4|OFFSet5|OFFSet6| OFFSet7|OFFSet8|CARRier |
|
Range: CARR|OFFS1|OFFS2|OFFS3|OFFS4|OFFS5|OFFS6| OFFS7|OFFS8 | ||
*RST Setting | CARRier | |
Requirements | ||
OUTPUT 714;"SETup:ORFSpectrum:SWITching:TIME:DOMain:FREQuency:OFFSet:INDex OFFSet1" ! Sets the Frequency Offset Index to OFFSet1. |
This command selects/queries the timeout value in seconds that will be used for ORFS measurements when the SETup:ORFSpectrum:TIMeout:STATe is ON. The units (S | MS) are optional. Units default to S if units are not specified. | ||
GPRS TA | ||
GSM/GPRS LA |
||
Setting | ||
*RST Setting | ||
Requirements | ||
OUTPUT 714;"SETUP:ORFSPECTRUM:TIMEOUT:TIME 15" ! Sets the timeout value to 15 seconds. |
This command selects/queries the ORFS measurement timeout state. |
||
GSM/GPRS LA |
||
Setting | ||
*RST Setting | 0 | OFF | |
Requirements | ||
OUTPUT 714;"SETUP:ORFSPECTRUM:TIMEOUT:STATE ON" ! Sets timeout state to on. |
This command selects/queries the trigger source for ORFS measurements. See Output RF Spectrum Measurement Description . | ||
EGPRS LA | ||
Setting | ||
*RST Setting | ||
Requirements | ||
OUTPUT 714;"SETUP:ORFSPECTRUM:TRIGGER:SOURCE AUTO" ! Sets the trigger source to automatic. |