SETup:GPESuality

SETup:GPESuality

Last updated: November 25, 2010

GPIB Command Conventions

SETup:GPESquality:CONTinuous

Function

GSM TA This command is not applicable to the GSM Test Application.

GPRS TA

This command is not applicable to the GPRS Test Application.

EGPRS TA

This command is not applicable to the EGPRS Test Application.

GSM/GPRS LA

Sets/queries the trigger arm state for the PESQ measurement.

EGPRS LA

Setting

1|ON|0|OFF

Query

1|0

*RST setting

0|OFF

Requirements

GSM/GPRS/ EGPRS TA

Revision: A.12 and above with a required feature license

GSM/GPRS/
EGPRS LA

Revision: H.00.00 and above with a required feature license

Programming Example

 
OUTPUT 714;"SETup:GPESquality:CONTinuous OFF"
!Sets measurement to single trigger mode..

SETup:GPESquality:INPut:VOLTage[:EXPected]

Function

GSM TA This command is not applicable to the GSM Test Application.

GPRS TA

This command is not applicable to the GPRS Test Application.

EGPRS TA

This command is not applicable to the EGPRS Test Application.

GSM/GPRS LA

Sets/queries the Expected Audio In Peak Voltage that is applied at the test set's AUDIO IN connector for the PESQ measurement. The units (V|mV|uV) are optional. If no units are specified, then units default to V.

EGPRS LA

Setting

Range: 0.001 to 2.0 V

Resolution: 1 mV

Query

Range: 0.001 to 2.0 V

*RST setting

2.0 V

Requirements

GSM/GPRS/ EGPRS TA

Revision: A.12 and above with a required feature license

GSM/GPRS/
EGPRS LA

Revision: H.00.00 and above with a required feature license

Programming Example

 
OUTPUT 714;"SETup:GPESquality:INPut:VOLTage 2"
!Sets the PESQ Expected Audio In Peak Voltage to 2 V.

SETup:GPESquality:MEASurement:MODE

Function

GSM TA This command is not applicable to the GSM Test Application.

GPRS TA

This command is not applicable to the GPRS Test Application.

EGPRS TA

This command is not applicable to the EGPRS Test Application.

GSM/GPRS LA

Sets/queries the Expected Audio In Peak Voltage that is applied at the test set's AUDIO IN connector for the PESQ measurement. The units (V|mV|uV) are optional. If no units are specified, then units default to V.

EGPRS LA

Setting

UPLink | DOWNlink | BOTH

Query

UPL| DOWN | BOTH

*RST setting

BOTH

Requirements

GSM/GPRS/ EGPRS TA

Revision: A.12 and above with a required feature license

GSM/GPRS/
EGPRS LA

Revision: H.00.00 and above with a required feature license

Programming Example

 
OUTPUT 714;"SETup:GPESquality:MEASurement:MODE UPL"
!Sets the PESQ measurement mode to Uplink audio.

SETup:GPESquality:OUTPut:VOLTage[:MAXimum]

Function

GSM TA This command is not applicable to the GSM Test Application.

GPRS TA

This command is not applicable to the GPRS Test Application.

EGPRS TA

This command is not applicable to the EGPRS Test Application.

GSM/GPRS LA

Sets/queries the Expected Audio In Peak Voltage that is applied at the test set's AUDIO IN connector for the PESQ measurement. The units (V|mV|uV) are optional. If no units are specified, then units default to V.

EGPRS LA

Setting

Range: 0.0 to 5.0 V

Resolution: 0.1 mV

Query

Range: 0.0 to 5.0 V

Resolution: 0.1 mV

*RST setting

0.0 V

Requirements

GSM/GPRS/ EGPRS TA

Revision: A.12 and above with a required feature license

GSM/GPRS/
EGPRS LA

Revision: H.00.00 and above with a required feature license

Programming Example

 
OUTPUT 714;"SETup:GPESquality:OUTPut:VOLTage 0.0"
!Sets the PESQ Maximum Audio Out Peak voltage.

SETup:GPESquality:SPEech

Function

GSM TA This command is not applicable to the GSM Test Application.

GPRS TA

This command is not applicable to the GPRS Test Application.

EGPRS TA

This command is not applicable to the EGPRS Test Application.

GSM/GPRS LA

Sets/queries the speech source of the PESQ measurement.

EGPRS LA

Setting

MALE | FEMale

Query

MALE | FEM

*RST setting

MALE

Requirements

GSM/GPRS/ EGPRS TA

Revision: A.12 and above with a required feature license

GSM/GPRS/
EGPRS LA

Revision: H.00.00 and above with a required feature license

Programming Example

 
OUTPUT 714;"SETup:GPESquality:SPEech MALE"
!Sets the PESQ speech source to Male.

SETup:GPESquality:TIMeout[:STIMe]

Function

GSM TA This command is not applicable to the GSM Test Application.

GPRS TA

This command is not applicable to the GPRS Test Application.

EGPRS TA

This command is not applicable to the EGPRS Test Application.

GSM/GPRS LA

The setting form of this command performs two functions: (1) sets the PESQ measurements' time-out STATe to 1 (ON) and, (2) sets the PESQ measurements' time-out value.

The query form returns the PESQ measurements' time-out value.

EGPRS LA

Setting

Range: 0.1 to 999.9 seconds

Resolution: 0.1 second

Query

Range: 0.1 to 999.9

*RST setting

10 seconds, ON

Requirements

GSM/GPRS/ EGPRS TA

Revision: A.12 and above with a required feature license

GSM/GPRS/
EGPRS LA

Revision: H.00.00 and above with a required feature license

Programming Example

 
OUTPUT 714;"SETup:GPESquality:TIMeout 5 s"
!Sets timeout state to ON and sets the timeout time to 5 seconds.

SETup:GPESquality:TIMeout:STATe

Function

GSM TA This command is not applicable to the GSM Test Application.

GPRS TA

This command is not applicable to the GPRS Test Application.

EGPRS TA

This command is not applicable to the EGPRS Test Application.

GSM/GPRS LA

Sets/queries the PESQ measurements's time-out state.

EGPRS LA

Setting

Range: 1|ON|0|OFF

Query

Range: 1|0

*RST setting

0|OFF

Requirements

GSM/GPRS/ EGPRS TA

Revision: A.12 and above with a required feature license

GSM/GPRS/
EGPRS LA

Revision: H.00.00 and above with a required feature license

Programming Example

 
OUTPUT 714;"SETup:GPESquality:TIMeout:STATe ON"
!Sets the timeout state to ON.

SETup:GPESquality:TIMeout:TIME

Function

GSM TA This command is not applicable to the GSM Test Application.

GPRS TA

This command is not applicable to the GPRS Test Application.

EGPRS TA

This command is not applicable to the EGPRS Test Application.

GSM/GPRS LA

Sets/queries the PESQ measurements' time-out setting to be used when the time-out state is set to ON.

EGPRS LA

Setting

Range: 0.1 to 999.9 seconds

Resolution: 0.1 second

Query

Range: 0.1 to 999.9

*RST setting

10 S

Requirements

GSM/GPRS/ EGPRS TA

Revision: A.12 and above with a required feature license

GSM/GPRS/
EGPRS LA

Revision: H.00.00 and above with a required feature license

Programming Example

 
OUTPUT 714;"SETup:GPESquality:TIMeout:TIME 5 s"
!Sets the timeout time to five seconds.