SYSTem:MEASurement

SYSTem:MEASurement

Last updated: December 3, 2008

GPIB Command Conventions

SYSTem:MEASurement:RESet

Function

GSM TA

Sets all measurements to abort, if the trigger arm is set to continuous the measurements will begin a new measurement cycle. See Trigger Arm (Single or Continuous) Description .

Any measurement results are cleared and the Integrity Indicator is set to 1 (No_Result_Available). See Integrity Indicator .

GPRS TA
EGPRS TA

GSM/GPRS LA

EGPRS LA

Setting GSM TA





These results are set to their default values:

  • RACH Count
  • Page Count
  • Missing Burst Count
  • Corrupted Burst Count
  • Channel Decoder Error Count
  • MS TX Level Reported
  • TCH Timing Advance Reported
  • RX Level
  • RX Qual

GSM/GPRS LA

GPRS TA

These results are set to their default values:

  • Block Error Rate (BLER)
  • Blocks Tested

EGPRS LA

Requirements

GSM/GPRS/
EGPRS TA

Revision: A.01 and above

GSM/GPRS/
EGPRS LA

Revision: C.01 and above

Programming Example

 
OUTPUT 714;"SYSTEM:MEASUREMENT:RESET" 
! Resets current measurements.