Last updated: September 2, 2009
Various calibration routines must be run periodically to ensure measurement accuracy, source accuracy and allow the most robust demodulation of the device-under-test's signal. This document describes the various calibrations available in the test set and when they should be performed.
This section indicates when the test set calibrations should be performed. Procedures are given for test sets that include Option 003: Flexible Radio Link and test sets that do not. Refer to Calibration Descriptions for details about the calibrations and how to perform them.
If any of the following calibrations fail, ensure that you have followed the Calibration Process Requirements and have performed the calibrations in the order prescribed by Recommended Calibration Intervals . If the calibration still fails, contact your local Keysight Sales Representative for assistance.
When performed from a GSM/GPRS/EGPRS or AMPS/136 application or format, the
First IQ Modulator
calibration sends a signal from the Baseband Generator 1 module to the RF Source 1 module to optimize the phase accuracy of RF Source 1 as a function of frequency. The optimization data is then stored in the test set and accessed whenever the RF Source frequency is set. The
Second IQ Modulator
calibration performs a similar procedure for RF Source 2 (RF Source 2 is only present if the test set includes option 002: RF Source 2).
When performed from a W-CDMA/HSPA, cdma2000/IS-95/AMPS or 1xEV-DO application or format (which require option 003: Flexible Radio Link), the IQ calibrations perform the same phase optimizations explained above. Additionally, a signal is sent from the Flexible Radio Link Subsystem to the RF sources to calibrate phase accuracy for those alternative paths as well. This additional calibration data is written to the same calibration data file as above, but in a different area of the calibration table.
The IQ calibrations ensure that the test set accurately generates IQ-modulated signals. If the test set's IQ modulators have not been properly calibrated, the test set's output power (when producing an IQ-modulated signal) will be inaccurate, which may result in degraded receiver test results.
If you perform the IQ calibrations from a W-CDMA/HSPA, cdma2000/IS-95/AMPS or 1xEV-DO application or format, you do not need to perform them from any other application or format. However, note that if you perform the IQ calibrations from a GSM/GPRS/EGPRS or AMPS/136 application/format, you must still perform them once from a W-CDMA/HSPA, cdma2000/IS-95/AMPS or 1xEV-DO application or format.
The IQ calibrations do not need to be run frequently. See Recommended Calibration Intervals .
To initiate the IQ calibrations from the front panel, press
SYSTEM CONFIG
, press the right
More
(
1 of 2
) key, select
Service
(
F7
), then select
Cal. first IQ Modulator
or
Cal. second IQ Modulator
. To initiate the IQ calibrations from a remote program, use the
CALibration:IQ[1]|2?
queries.
This calibration is only applicable to W-CDMA/HSPA, cdma2000/IS-95/AMPS, and 1xEV-DO applications and formats. This calibration is only required when using the test set to generate an
AM
or
DSB-SC
test signal (select (
F9
)
Test Signal
when in
CW Operating Mode
). These test signals are used for calibrating Zero Intermediate Frequency (Zero IF) devices which utilize Qualcomm's radioOne architecture.
You do not have to perform the
Burst Mod Offset 1
calibration for each application/format in your test set; performing it from one application/format provides calibration data to all relevant applications and formats.
The
Burst Mod Offset 1
calibration does not need to be run frequently. See
Recommended Calibration Intervals
.
The
Burst Mod Offset 1
calibration calibrates the noise and signal level of RF Source 1 (as a function of frequency) to most accurately produce the
AM
and
DSB-SC
test signals required for Zero IF device calibration. The calibration is performed by generating the modulated test signals and adjusting RF Source 1 to optimize gain and minimize the noise floor. The optimization data is then stored in the test set and accessed whenever the RF Source frequency is set.
To initiate the
Burst Mod Offset 1
calibration from the front panel, press
SYSTEM CONFIG
, press the right
More
(
1 of 2
) key, select
Service
(
F7
), then select
Cal. Burst Mod Offset 1
. To initiate the
Burst Mod Offset 1
calibration from a remote program, use the
CALibration:BMOFfset?
query.
The
Burst Mod Offset 1
calibration takes less than 1 minute to execute.
The
Thermal Power Null Adjustment
is only applicable to the cdma2000/IS-95/AMPS, 1xEV-DO and W-CDMA/HSPA applications/formats.
The Thermal Power Detector is calibrated at the factory and temperature controlled for stability. However, it is still possible for the auto-null circuit within the detector to drift over time. The
Thermal Power Null Adjustment
re-centers the auto-null circuit to provide optimum accuracy for the affected measurements.
You only need to perform the
Thermal Power Null Adjustment
once to re-center the auto-null circuit (you do not have to perform it from each application/format in your test set).
Thermal Power Null Adjustment
feature. Any applications that do not include the
Thermal Power Null Adjustment
feature (in the
Utilities
menu of the
System Config
screen) do not use the re-centering data and thus do not achieve the accuracy optimization that results from re-centering the auto-null circuit. You must upgrade those applications if you wish to achieve the accuracy optimization that results from running the
Thermal Power Null Adjustment
.
The
Thermal Power Null Adjustment
does not need to be run frequently. See
Recommended Calibration Intervals
.
This adjustment affects the
Thermal Power
(W-CDMA/HSPA) measurement, as well as all measurements that are calibrated by the
Digital Average Power Calibration
(cdma2000/IS-95/AMPS, 1xEV-DO) and
Calibrate Measurements
(W-CDMA/HSPA) routine.
To initiate the
Thermal Power Null Adjustment
from the front panel, press
SYSTEM CONFIG
, press the right
More
(
1 of 2
) key, and select
Thermal Power Null Adjust
(
F9
). To initiate the
Thermal Power Null Adjustment
from a remote program, use the
SYSTem:INSTrument:THERmal:POWer:NULL:ADJust?
query.
The
Thermal Power Null Adjustment
takes between 30 seconds and 3 minutes.
The
Thermal Power Null Adjustment
can also be used to help verify your test set. See "Verifying the Test Set" in the Related Topics below.
The
Digital Average Power
calibration is only applicable to the cdma2000/IS-95/AMPS and 1xEV-DO applications/formats.
You do not have to perform the
Digital Average Power
calibration for each application/format in your test set; performing it from one application/format provides calibration data to all relevant applications and formats.
The
Digital Average Power
calibration does not need to be run frequently. See
Recommended Calibration Intervals
.
Digital Average Power
calibration is complete in order to complete the calibration (the calibration data is not available to the test set until it has been restarted).
The
Digital Average Power
calibration generates calibration data for the Fast Power Detector for use by cdma2000/IS-95/AMPS and 1xEV-DO applications and formats. This calibration improves the accuracy of the Fast Power Detector when used to measure IS-95 and reverse RC-1 and RC-2 signals.
The calibration generates a CW signal at a given power level, measures it using the Fast Power Detector, generates a CDMA-modulated signal at the same power level, measures it using the Fast Power Detector and notes the difference. The calibration then generates a CW signal at a given power level, measures it using the Thermal Power Detector, generates a CDMA-modulated signal at the same power level, measures it using the Thermal Power Detector and notes the difference. Calibration data is then created by comparing these results. This is repeated for several power levels.
The
Digital Average Power
calibration provides calibration data for the following measurements:
To initiate the
Digital Average Power
calibration from the front panel, press
Measurement selection
, select
Digital Average Power
, then select
Calibrate Digital Avg Pwr
(F4)
. To initiate the
Digital Average Power
calibration from a remote program, use the
CALibration:DAPower?
query.
The
Digital Average Power
calibration takes approximately 9 minutes to execute.
Performing the
Spectrum Monitor
calibration from one application/format does not provide calibration data to all relevant applications and formats. The calibration data files are shared as follows:
Spectrum Monitor
calibration data file.
Spectrum Monitor
calibration data file.
Spectrum Monitor
calibration data file.
Thus, if you perform the
Spectrum Monitor
calibration from a 1xEV-DO application/format, you do not need to perform it from a cdma2000/IS-95/AMPS application/format. However you do still need to perform it from a W-CDMA/HSPA application/format and then again from either a GSM/GPRS/EGPRS or AMPS/136 application/format.
The
Spectrum Monitor
calibration should be run monthly, or whenever the test set's operating environment changes. See
Recommended Calibration Intervals
.
Performing the
Spectrum Monitor
calibration from a cdma2000/IS-95/AMPS or 1xEV-DO application/format executes the same routine as performing the
Channel Power Calibration
.
Performing the
Spectrum Monitor
calibration from a W-CDMA/HSPA application/format executes the same routine as performing the
Calibrate Measurements
routine.
Performing the
Spectrum Monitor
calibration from a GSM/GPRS/EGPRS or AMPS/136 application/format calibrates the IF signal path in the Measurement Downconverter, using a CW signal.
To initiate the
Spectrum Monitor
calibration from the front panel, press
Instrument selection
, select
Spectrum Monitor
, select
Trigger Setup
(
F4
), then select
Calibrate Measurement
(
F11
). To initiate the
Spectrum Monitor
calibration from a remote program, use the
CALibration:SMONitor?
query.
The
Spectrum Monitor
calibration takes between 45 seconds and 3 minutes to execute, depending upon which application/format it is executed from.
The
Channel Power
calibration is applicable to the cdma2000/IS-95/AMPS and 1xEV-DO applications/formats.
You do not have to perform the
Channel Power
calibration for each application/format in your test set; performing it from one application/format provides calibration data to all relevant applications and formats.
The
Channel Power
calibration should be run monthly, or whenever the test set's operating environment changes. See
Recommended Calibration Intervals
.
The
Channel Power
calibration calibrates the signal paths through the Measurement Downconverter and Demod Downconverter using both a CW signal and a modulated signal. The calibration is performed by comparing measured signals through the MDC and DDC to measurements made using the Fast Power Detector (which is calibrated at the factory and temperature controlled for stability). During the
Calibrate Measurements
calibration, the internal temperature of the test set is measured and stored with the calibration data. If the internal temperature of the test set drifts by more than +/- 10 C since the last calibration, measurements utilizing this calibration will return integrity indicator 19 (
Uncalibrated Due to Temperature
).
The
Channel Power
calibration provides calibration data for the following measurements:
Performing the
Channel Power
calibration executes the same routine as performing the
Spectrum Monitor Calibration
from a cdma2000/IS-95/AMPS or 1xEV-DO application/format.
To initiate the
Channel Power
calibration from the front panel, initiate any of the measurements listed above and select
Calibrate Channel Power
(F4)
. To initiate the
Channel Power
calibration from a remote program, use the
CALibration:CPOWer?
query.
The
Channel Power
calibration takes approximately 2 minutes to execute.
The
Calibrate Measurements
routine is only applicable to W-CDMA/HSPA applications/formats.
The
Calibrate Measurements
routine should be run monthly, or whenever the test set's operating environment changes. See
Recommended Calibration Intervals
.
The
Calibrate Measurements
routine calibrates the signal paths through the Measurement Downconverter and Demod Downconverter using both a CW signal and a modulated signal. The calibration is performed by comparing measured signals through the MDC and DDC to measurements made using the Fast Power Detector (for CW signals) and the Thermal Power Detector (for modulated signals). Both of these detectors are calibrated at the factory and temperature controlled for stability. During the
Calibrate Measurements
calibration, the internal temperature of the test set is measured and stored with the calibration data. If the internal temperature of the test set drifts by more than +/- 10 C since the last calibration, measurements utilizing this calibration will return integrity indicator 19 (
Uncalibrated Due to Temperature
).
The
Calibrate Measurements
routine provides calibration data for the following measurements:
Performing the
Calibrate Measurements
routine executes the same routine as performing the
Spectrum Monitor Calibration
from a W-CDMA/HSPA application/format.
To initiate the
Calibrate Measurements
routine from the front panel, initiate any of the measurements listed above and select
Calibrate Measurements
(F4)
. To initiate the
Calibrate Measurements
routine from a remote program, use the
CALibration:MEASurements?
query.
The
Calibrate Measurements
routine takes approximately 3 minutes to execute.